Experimenting with Inductors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Inductors
  • More
  • Cancel
Experimenting with Inductors
Blog Experimenting with inductors blog Part 1: Introduction to Fourier Series
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
  • Author Author: rsjawale24
  • Date Created: 29 Jan 2020 5:04 PM Date Created
  • Views 1818 views
  • Likes 11 likes
  • Comments 6 comments
  • experimenting with inductors
  • signal processing
  • inductors
  • filter design
Related
Recommended

Experimenting with inductors blog Part 1: Introduction to Fourier Series

rsjawale24
rsjawale24
29 Jan 2020

Hi there!

This is the first part of my blog in Experimenting with Inductors. Here's a short introduction of me and what I do.

I'm a MS by Research Scholar from India working on Radio frequency antennas. I have been working on electronics since last 7-8 years when I picked up interest in Radio Frequency circuits. I decided to pursue my masters in RF.

Apart from Antennas, I have also worked on Embedded systems, Analog and RF circuits, SDRs and some general electronics projects.

 

I have entered the Experimenting with Inductors challenge to showcase a very beautiful and fundamental topic studied by every electrical engineer i.e. Fourier Series.

When I say Fourier series the first thing that comes in mind is a series of trigonometric functions!

Yes, it is math but do you know that you can prove or verify the Fourier series experimentally using inductors?(Well, not just inductors but some other passive components)

I have always believe that engineering education should be a bit fun by practically verifying the theories learnt in class.

 

Introduction to Fourier Series

We all have studied Fourier series at some point of time in our engineering studies. It says that any periodic signal can be represented as a sum of harmonics of sines and cosines.

In other words, every periodic signal consists of harmonics of sines/cosines. Does this mean we can extract sine from a square wave or a ramp?

Yes, we can!

Let's take a look at the formula for Fourier series

image

Where a0, an and bn are the fourier coefficients which needs to be solved using integrals. I won't go into much of math here. I will directly show the results.

 

Now let's take an example of Fourier series representation of a periodic square wave

Assuming a even symmetric square wave, for even signals, bn= 0 as bn is the coefficient of sin(nx) which is an odd signal.

The Fourier series expansion is

image

which shows that a even square wave can be represented as the sum of infinite harmonics of cosines. In other words, a square wave can be made by adding infinite cosines.

 

Experiment to prove Fourier series

 

Above, we saw that a square wave is made up of infinite cosines. Is it possible to extract a cosine wave from a square wave?

Yes, it is. But how?

 

Firstly, as we can see each cosine wave in the square wave has a different frequency (harmonics) which means we will need a frequency selective circuit that can separate these harmonics.

A filter is one such frequency selective circuit which can allow or stop a certain frequency or a band or frequencies depending upon type of filter.

 

So, in my experiment I plan to use a LC filter using Inductors from the Kemet Kit which I received for the Experimenting with inductors challenge.

 

A single LC filter provides two poles which means it provides a roll off of -40dB/dec at the cutoff frequency. I will be using a LC low pass filter with a cutoff frequency equal to the fundamental frequency of the square wave which we want to separate into cosines.

The low pass filter will filter out the fundamental frequency from the square wave.

Similarly, for the harmonics, a LC band pass filter will be used to separate the various harmonics of cosines from the square wave.

 

 

I will cover the pole-zero diagram, filter design details, calculations and circuits in the next part of the blog.

Till then, if you have any queries please post them below. image

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 6 years ago +4
    It is nice to see some theory being converted into practical implementations. This is often a missing step. Dubbie
  • jc2048
    jc2048 over 6 years ago +4
    Good starting blog - a nice mix of theory and practical work. I'll be interested to see if you can get the cut-off where you want it and how good a sinewave you get out of it. Have you had a chance to…
  • rsjawale24
    rsjawale24 over 6 years ago in reply to jc2048 +3
    Hi Jon, I'm glad that you liked it. My whole motive behind this was to give a practical understanding of theoretical concepts. Yes, I got to use the LCR meter and it's awesome. I will post about it in…
  • rsjawale24
    rsjawale24 over 6 years ago in reply to dubbie

    Hi Dubbie,

    Glad that you liked it. image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rsjawale24
    rsjawale24 over 6 years ago in reply to jc2048

    Hi Jon,

    I'm glad that you liked it. My whole motive behind this was to give a practical understanding of theoretical concepts. image
    Yes, I got to use the LCR meter and it's awesome. I will post about it in the next part of the blog.

     

    However, to answer you questions, the L and C are calculated at a fixed frequency and current/voltage (depends of L or C calculation) and you cannot change it.
    But overall, it is a pretty great instrument as it has L,C,R, Diode, continuity and transistor (hfe) measurements.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rsjawale24
    rsjawale24 over 6 years ago in reply to shabaz

    Hi!
    Thanks for that! image
    I didn't use HTML. I used the equation editor available in the text editor here.

    I guess it has some problem. I will edit the blog.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago

    Hi Rushiraj,

     

    Great start! I had a suggestion, to make it more readable, maybe it's better to include any math stuff as inline images, instead of HTML.

    The reason is, it's coming out small and with strange symbols (at least on Chrome on desktop and on mobile). This is what it looks like for me (but smaller text) - the A looks like a weird Angstrom hehe :

    image

    If you do it (say) in Word and then paste in an image, it will work on all browsers, and be a nice size:

    image

    No-one can use the text-based version through copy-paste into (say) a calculator anyway, so there's no disadvantage to using graphic files for this I think!

    Plus then people won't need to zoom : )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 6 years ago

    Good starting blog - a nice mix of theory and practical work. I'll be interested to see if you can get the cut-off where you want it and how good a sinewave you get out of it.

     

    Have you had a chance to use the LC meter that was included with the kit? What's it like? Does it tell you the frequency at which the test was done or, even better, allow you some choice in the matter?

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
>