Experimenting with Industrial Automation
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Industrial Automation
  • More
  • Cancel
Experimenting with Industrial Automation
Blog Experimenting with Industrial Automation - Water Tunnel Controller Upgrade - Blog1 - Unboxing
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rsc
  • Date Created: 17 Jan 2024 5:33 PM Date Created
  • Views 853 views
  • Likes 11 likes
  • Comments 3 comments
  • plc
  • industrial automation
  • Water Tunnel
Related
Recommended

Experimenting with Industrial Automation - Water Tunnel Controller Upgrade - Blog1 - Unboxing

rsc
rsc
17 Jan 2024

Unboxing the kit:

The kit arrived today.

The kit

The kit parts

I downloaded all of the part documents and the control software.

The first thing I'll do is wire the components up on a board using some DIN rail

so I can try out the PLC software and make sure all the components are working.

The Plan:

The overall plan is to replace the Direct Logic PLC on our water tunnel with the Schneider

Electric PLC and add some remote control switches for motor On/Off and E-Stop.

This is the current control box with the Direct Logic PLC down at the bottom 

DirectLogic PLC

The water flowmeter monitor and E-Stop are currently located on the side of the water tunnel.

Flowmeter Monitor

The water tunnel takes up half of the lab, and there are only controls on one side, so

it will be nice to have controls the are a bit more portable.

Here's a picture of the water tunnel operating in PIV mode with the laser on.  There are particles

in the water that are lit up by the laser and then a camera and software capture the images to map the 

flow around the target.

Flume 

Here's a picture of an instrumented propeller in the water tunnel testing the torque

at various flow rates.

flume2

  • Sign in to reply

Top Comments

  • dougw
    dougw over 2 years ago +1
    Wow, I don't think that would fit in my basement.. Interesting application.
Parents
  • dougw
    dougw over 2 years ago

    Wow, I don't think that would fit in my basement..Relaxed

    Interesting application.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rsc
    rsc over 2 years ago in reply to dougw

    You would need some very large doorways, and a floor that could hold 30,000 lbs

    Wink

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rsc
    rsc over 2 years ago in reply to dougw

    You would need some very large doorways, and a floor that could hold 30,000 lbs

    Wink