Experimenting with Industrial Automation
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Industrial Automation
  • More
  • Cancel
Experimenting with Industrial Automation
Blog The Academic Approach: Expansion Module on Modicon M251 - 2
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: pandoramc
  • Date Created: 14 Feb 2024 4:47 PM Date Created
  • Views 861 views
  • Likes 5 likes
  • Comments 0 comments
  • experimenting with industrial automation
  • schneider electric
  • M251
Related
Recommended

The Academic Approach: Expansion Module on Modicon M251 - 2

pandoramc
pandoramc
14 Feb 2024

The Modicon M251 has powerful features to connect each element of automation and control remote actuators or take information from remote sensors. In other hand, this does not mean that is local control is not allowed. The device takes advantages of expansion port to connect other devices like I/O since the Modicon M251 has not integrated this kind of systems like the M241. Each side of the module has labels that can be removed in order to integrate new features to the module.

Main Label

If you remove this label, you will be able to view a special connector for expansion modules which shares data and power according to the kind of module. This time I used the TM3DM24R, which is a Digital Input/Output Module, to use the new features to integrate the ladder logic in a local way.

Connectors

To integrate, you only need the power supply, the TM3DM24R connected with the M251 by the expansion port and an Ethernet wire to upload the latest program. The software required to design the logic is the EcoStruxure Machine Expert and I used an external Button to implement a toggle switch. According to the wiring manual, the TM3DM24R module could be used in positive logic or negative logic but for this test I used the positive logic. Don't worry about the logic with I/O since the three blocks available has isolated references to implement the better combination of logic.

{gallery}Integration

image

IMAGE TITLE: TM3DM24R/G wiring diagram

Assembly

IMAGE TITLE: Kit Assembly for test

Integration of the Button

IMAGE TITLE: Integration

To have a better perception about I made a video that is below. There are a description of the implementation and test of an oscillator using Set/Rest elements and turn on delayed timers using ladder logic.