Experimenting with Industrial Automation
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Industrial Automation
  • More
  • Cancel
Experimenting with Industrial Automation
Blog The Academic Approach: Summary
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: pandoramc
  • Date Created: 25 Mar 2024 3:49 PM Date Created
  • Views 512 views
  • Likes 5 likes
  • Comments 0 comments
  • experimenting with industrial automation
  • design challenge
  • conveyor
  • schneider electric
  • winners
  • Harmony Hub
Related
Recommended

The Academic Approach: Summary

pandoramc
pandoramc
25 Mar 2024

Table of Contents

  • Input/Outputs
  • Interfaces
  • Software
  • Application
  • Conclusions

Input/Outputs

Although the M251 does not have Inputs/Outputs like other series of the PLCs, the device has expansion connectors to improve the capabilities. In this learning path, there was the opportunity to use the TM3DM24R, which is an I/O module. There is an interesting feature in this module, the terminals can be configured with positive logic or negative logic, since the common terminals are not internally connected. On the other hand, to test the operation I implemented a toggle button to turn on and turn off a load each time the button is pressed and released.

{gallery}I/O

image

Expansion Connectors

image

Positive logic connection

image

Negative logic connection

image

Button connected to expansion module

image

Toggle function synthetized with a SR Flip-Flop

Interfaces

The M251 is really impressive device because all the communication can be centralized and managed in the PLC itself. This is possible because there are two Ethernet connections and a configurable Serial Line. In the chosen architecture, the serial line is dedicated to the Harmony Hub, since the ZBRN2 model has a ModBus protocol through an RS485 serial port. This brings a remote interaction between the buttons and indicators, and avoids the use of other expansion modules. The Ethernet ports were used for the PLC programming and the data exchange with the HMI. Despite its size, the HMI is a powerful tool to interact locally or remote if the Network infrastructure allows that. An interesting feature of the HMI is the red edge coloring when a variable does not exist or the communication fails

{gallery}Interfaces

image

Assembly of visual receiver and a button for the Harmony Hub interaction

image

Remote placement of the Harmony Hub wireless receiver

image

Data exchange with the ST6200

image

HMI Interaction with the M251 device

image

Variable connection failure

Software

The software is amazing, it is intuitive and we can do a proof-of-concept really quickly. You just have to look at the licensing modes. Despite the Machine Expert has 42 days to test the software for free, you can register yourself on the Schneider Electric website to get a limited license to test and program the PLC. We will lose the simulation benefits to test our applications before the programming, but you are able to use the PLC after this road test. To recover this cabability, you must acquire a license from an SE dealer. Other features may be limited, but for a small scale application the available could be sufficient. On the other hand, if there is not a valid license for the Operator Terminal package, you will not be able to download your program to the HMI, here you MUST get a valid license.

{gallery}Software

image

Limited License effects

image

Machine Expert Architecture for the proof-of-concept

image

HMI Project Architecture

Application

Despite the prototype limitations of the first proposal, it is feasible to understand our weakness and select other elements that can improve the system behavior. An example is changing the acrylic structure for a metal sheet to achieve a better structure that resists the forces involved in the transmission line. The designed roller did not have a treatment to improve the coefficient of friction and the forces could break the acrylic, consequently, the new proposal has this new material.

{gallery}App

image

Roller design with 3D printer

image

New tensor system

image

Last roller assembly with the transport belt

Conclusions

The whole system has interesting features and approaches since the connected industry (IIoT) is an importMachine-human interaction must evolve, and the HMI provided has the flexibility to configure the machine operation according to work conditionsant area of application today. The Harmony Hub, in cooperation with the M251, offers a new way to connect the industrial facilities, and provide security for the device connectivity. Thanks to rscasny
 for the support and all the participants for sharing their concerns about the devices in order to solve them.

I added the Toogle function like a Youtube short below