Experimenting with Single Pair Ethernet
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Single Pair Ethernet
  • More
  • Cancel
Experimenting with Single Pair Ethernet
Forum SPE face-off
  • News
  • Projects
  • Forum
  • Enroll
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Experimenting with Single Pair Ethernet to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 35 subscribers
  • Views 1129 views
  • Users 0 members are here
  • single pair ethernet
  • podl
  • DP83TD510E
  • spe
Related

SPE face-off

wolfgangfriedrich
wolfgangfriedrich 8 months ago

Even before the Single Pair Ethernet design challenge started, I was pondering about making a SPE solution available for whoever is interested. Looking at the feature list, the cable length of 10baseT1L stood out more than e.g. 1Gbit over 40 meter on a single pair. So I started researching chip sets and landed on the TI solutions instead of ADI. And the chip of choice is the TI DP83TD510E.

This is not a competitive entry into the design challenge, I just want to share my work in progress. My idea is to build a simple board that works as an Ethernet extension: plug it into a network hub on one end and have 10Mb of Ethernet data rate at the other end which can be really far away. This is plenty for sensor data or even streaming audio, not so much for a NAS or other high speed data connections. 
The first step is going to be a one-board design that can be used on both ends as a media converter from regular Ethernet to SPE. As a compliant interface it would also be possible to replace the far end with a ADI or Microchip device. Low power is a design goal but there will be lower power options available, I am thinking of the SPE to SPI chip ADIN1110. Also the selected microcontroller is not famous for its low power, but something I am comfortable working with, the RP2040.

The board is equipped with an expansion connector breaking out a set of signals that might be sufficient for a Power over Dataline (PoDL) add on board, but this is just a concept for now without a design yet. Another thought I had during a shower recently, power input for the PoDL section could be done as a USB-C PD sink device. Or even better, in the meantime there are chips available that can act as a sink or source, so I could extend the single board for both ends to a PD source to power the SPE far end device and provide additional power output. But that is step 42, I am at step 3 right now. 

 The schematic is finished enough to share and I have started putting components on a board. Layout progress will be shared when I have something to show for.

Edit: I had to remove the schematic as it was still full of errors. It should not be out in the wild in this form and I will update when I am confident in a better version.

Edit2: Added new schematic, which is much more complete. Added config resistors and changedMII to RMII connect. 
 
 Please enjoy and I am very open to suggestions or even better, to pointing out any blatant mistakes I have made. 

  • Sign in to reply
  • Cancel

Top Replies

  • BigG
    BigG 8 months ago +1
    Thanks for sharing. Last year I was tinkering at best but then lost interest as I don't really have a problem to solve. I had started with LAN8651 10BASE-T1S daisy chain. I even did up a design (a learn…
  • wolfgangfriedrich
    wolfgangfriedrich 8 months ago in reply to JWx +1
    They are mostly series termination and debug friendliness. And if I remove some of them I should be able to run this interface as RMII. They eval board is wired for RMII, which makes it a good resource…
  • kmikemoo
    kmikemoo 8 months ago +1
    Nice!!! I love the vision. I do like the PoDL thought. That would make this setup amazing. Great work.
Parents
  • BigG
    BigG 8 months ago

    As you have included an RP2040 in your design, I am not sure if you are aware there's a rmii library available. It's something I came across last time I looked at SPE. I believe it uses PIO.

    https://github.com/rscott2049/pico-rmii-ethernet_nce

    https://github.com/sandeepmistry/pico-rmii-ethernet

    From the readme's I gather sandeepmistry's library achieves 50Mbit data rate and rscott2049 just about gets 100Mbit. Pretty impressive and certainly faster than SPI.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx 8 months ago in reply to BigG

    this is a software implementation of MAC - impressive, but I wonder how much resources are left for the user after it is running: "Leverages the Raspberry Pi RP2040 MCU's PIO, DMA, and dual core capabilities to create a Ethernet MAC stack in software!" 

    I think that some versions of ESP32 have a hardware MAC onboard that can be used to interface such a PHY (in the first iteration of preparation for this challenge I have even asked for ADIN1100 chip for such a project)  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG 8 months ago in reply to JWx

    Yes, the new ESP32-P4 has a hardware MAC onboard. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG 8 months ago in reply to JWx

    Yes, the new ESP32-P4 has a hardware MAC onboard. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • JWx
    JWx 8 months ago in reply to BigG

    according to this, original ESP32 (included in ESP32-WROOM-32, ESP32-DevKitC)  also had onboard MAC

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG 8 months ago in reply to JWx

    Indeed so. Although I believe the ESP32-WROOM-32 module is not recommended for new designs even if still available.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx 8 months ago in reply to BigG

    it may be - it is pretty old today...