Experimenting with Thermal Switches
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Thermal Switches
  • More
  • Cancel
Experimenting with Thermal Switches
Challenge Blog Experiment with thermal switches :- thermal switches to maintain the temperature of an electroplating solution
  • Challenge Blog
  • Forum
  • Documents
  • Files
  • RoadTests
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: manojroy123
  • Date Created: 2 Feb 2022 10:50 AM Date Created
  • Views 4175 views
  • Likes 8 likes
  • Comments 3 comments
  • Experimenting with Thermal Switches.
Related
Recommended

Experiment with thermal switches :- thermal switches to maintain the temperature of an electroplating solution

manojroy123
manojroy123
2 Feb 2022

Experimenting with Thermal Switches

thermal switches to maintain the temperature of an electroplating solution:-

About Myself: -

I run a business of manufacturing electronics goods for consumers and for trainees’ engineers. A lot of time I prototype double sided PCB in my premises. For plating the PCB holes. I had to build an electroplating setup bath. It is very difficult to judge weather the holes are plated or not if they are not shiny.

Problem: -

Surface plating finish of any metal heavely depends on current density and temperature of the plating solution as shown in the figure bellow.

Figure 1:-

image

Most factory machine comes with the temperature controller for the machine. But over her, we are trying to build an inexpensive copper plating  machine for personal use. We are using a plastic contianer to store and the Copper sulphate pentahydrate as plating electrolyte. This where the problem arises, We want to build an inexpensive machine that takes less time to build. We even have to consider melting temperature of plastic container.

Solution: -

To maintain temperature of copper sulfate and current density based on figure 1. We are building a temperature switch controller to set the temperature of the solution to 60'c. Circuit schematic of the controller is given in figure 2

image

Over here the power resistor and the thermal switch  is sealed and dipped in the copper sulfate solution to heat the solution and to maintain the temperature of the solution.

  • Sign in to reply
Parents
  • javagoza
    javagoza over 4 years ago

    I like the idea of the project but I don't understand the schematics. I understand that the Thermal Reed Switch is normally closed until it reaches 60 C and the resistance and switch are in parallel, with the resistance of the switch being 150 mOhms MAX (Contact Resistance)  how can this work?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • manojroy123
    manojroy123 over 4 years ago in reply to javagoza

    a lot of assumption is made before the experiment is done. Please consider those values as assumptions. True value will be reveled while we do the experiment

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • manojroy123
    manojroy123 over 4 years ago in reply to javagoza

    a lot of assumption is made before the experiment is done. Please consider those values as assumptions. True value will be reveled while we do the experiment