Experimenting with Vibration Sensors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Vibration Sensors
  • More
  • Cancel
Experimenting with Vibration Sensors
Blog Experimenting with Vibration Sensors - Machinery Safety Blog #5
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
  • Author Author: dwinhold
  • Date Created: 13 Dec 2020 1:32 AM Date Created
  • Views 818 views
  • Likes 4 likes
  • Comments 0 comments
  • experimenting_with_vibration_sensors
  • dwinhold
  • kemet vibration sensor
Related
Recommended

Experimenting with Vibration Sensors - Machinery Safety Blog #5

dwinhold
dwinhold
13 Dec 2020

Vibration Sensor Demo

 

Below is Arduino code for testing the KEMET vibration sensors sensitivity. I also attached a video of the code running with the sensor attached to a small fan. In the video you can see when I run the fan it picks up the slight vibration (I couldn't even feel). I have an LCD display attached to show the readouts.

 

Below is the code for vibration sensor test reading:

 

#include <LiquidCrystal.h>

const int rs = 12, en = 11, d4 = 5, d5 = 4, d6 = 3, d7 = 2;
LiquidCrystal lcd(rs, en, d4, d5, d6, d7);

int vib = A0; //Vibration sensor pin
int data; //Sensor reading
int average = 0; //Average reading
int averageA = 0;
int averageB = 0;
int x = 0; //Loop count
int tread = 0; //Temporary read
int hread = 0; //Highest reading


void setup(){
  lcd.clear();
  lcd.begin(16, 2); //Set screen size
  lcd.setCursor(0,0); //Start print location
  lcd.print("KEMET Vibration");
  lcd.setCursor(0,1); //Start print location
  lcd.print("Sensor - VSBV20");
  delay(5000); //5 second delay
  pinMode(vib, INPUT); //initialize vib sensor as INPUT
  Serial.begin(9600); //begin the serial monitor at 9600 baud
  lcd.clear();
    do{ //Calibrate loop to get average vibration
      x = x + 1;
      averageA = analogRead(vib);
      averageB = averageB + averageA;
      Serial.println("Calibrating");
      lcd.setCursor(0,0);
      lcd.print("Calibrating");
      lcd.setCursor(0,1);
      lcd.print("XXXXXXXXXXXXXXX " + x);   
      delay(500);   
      } while (x < 15);
    average = averageB/15;
    delay(1000);
}

void loop(){

    data=analogRead(vib);
    Serial.println(data);
    tread = data;
    x = x + 1;
    
     // Set highest reading 
     if(hread < tread) { 
      hread = tread;
     }

      lcd.clear();
      lcd.setCursor(0,0);
      lcd.print("Ca=");
      lcd.setCursor(3,0);
      lcd.print(average); //Display average vibration
      lcd.setCursor(8,0);
      lcd.print("CR=");
      lcd.setCursor(11,0);
      lcd.print(data); //Displays current vibrations
      lcd.setCursor(8,1);
      lcd.print("HR=");
      lcd.setCursor(11,1);
      lcd.print(hread); //Displays highest vibration reading
      delay(100);

  }

 

 

Below is the code for my project:

 

#include <LiquidCrystal.h>

const int rs = 12, en = 11, d4 = 5, d5 = 4, d6 = 3, d7 = 2;
LiquidCrystal lcd(rs, en, d4, d5, d6, d7);

int vib = A0; //Vibration sensor pin
int safelt1 = 8; //Assign warning LED
int safelt2 = 9; //Assign warning LED
int warnlt1 = 10; //Assign warning LED
int warnlt2 = 13; //Assign warning LED
int shutdwnlt = 14; //Assign warning LED
int shutdwnsw = 7; //Assign shutdown switch
int data; //Sensor reading
int average = 0; //Average reading
int averageA = 0;
int averageB = 0;
int x = 0; //Loop count
int tread = 0; //Temporary read
int hread = 0; //Highest reading


void setup(){
  pinMode(shutdwnsw, OUTPUT);
  digitalWrite(shutdwnsw, LOW);
  lcd.clear();
  lcd.begin(16, 2);
  lcd.setCursor(0,0); //Start print location
  lcd.print("KEMET Vibration");
  lcd.setCursor(0,1); //Start print location
  lcd.print("Sensor - VSBV20");
  delay(2500);
  pinMode(vib, INPUT); //initialize vib sensor as INPUT
  Serial.begin(9600); //begin the serial monitor at 9600 baud
  lcd.clear();
    do{ //Calibrate average vibration
      x = x + 1;
      averageA = analogRead(vib);
      averageB = averageB + averageA;
      Serial.println("Calibrating");
      lcd.setCursor(0,0);
      lcd.print("Calibrating");
      lcd.setCursor(0,1);
      lcd.print("XXXXXXXXXXXXXXX " + x);   
      delay(500);   
      } while (x < 15);
    average = averageB/15;
    delay(1000);

}

void loop(){

    data=analogRead(vib);
    Serial.println(data);
    digitalWrite(safelt1, HIGH);
    tread = data;
    
     // Set highest reading 
     if(hread < tread) { 
      hread = tread;
     }
    
    if(data <= (average*1.05)){ 
      lcd.clear();
      digitalWrite(safelt2, LOW);
      digitalWrite(warnlt1, LOW);
      digitalWrite(warnlt2, LOW);
      digitalWrite(shutdwnlt, LOW);
      Serial.println("Within Limits");
      lcd.setCursor(0,0);
      lcd.print("Ave=");
      lcd.setCursor(4,0);
      lcd.print(average);
      lcd.setCursor(10,1);
      lcd.print("HR=");
      lcd.setCursor(13,1);
      lcd.print(hread);
      lcd.setCursor(0,1);
      lcd.print("--------");
      lcd.setCursor(10,0);
      lcd.print("CR=");
      lcd.setCursor(13,0);
      lcd.print(data);

    }
    
    else if(data <= (average*1.1)){
      lcd.clear();
      digitalWrite(warnlt1, LOW);
      digitalWrite(warnlt2, LOW);
      digitalWrite(shutdwnlt, LOW);
      Serial.println("Within Limits High");
      lcd.setCursor(0,0);
      lcd.print("Ave=");
      lcd.setCursor(4,0);
      lcd.print(average);
      lcd.setCursor(10,1);
      lcd.print("HR=");
      lcd.setCursor(13,1);
      lcd.print(hread);
      lcd.setCursor(0,1);
      lcd.print("XX------");
      lcd.setCursor(10,0);
      lcd.print("CR=");
      lcd.setCursor(13,0);
      lcd.print(data);
      digitalWrite(safelt2, HIGH);
    }
    
    else if(data <= (average*1.2)){
      lcd.clear();
      digitalWrite(safelt2, LOW);
      digitalWrite(warnlt1, LOW);
      digitalWrite(warnlt2, LOW);
      digitalWrite(shutdwnlt, LOW);
      Serial.println("Warning Limits");
      lcd.setCursor(0,0);
      lcd.print("Ave=");
      lcd.setCursor(4,0);
      lcd.print(average);
      lcd.setCursor(10,1);
      lcd.print("HR=");
      lcd.setCursor(13,1);
      lcd.print(hread);
      lcd.setCursor(0,1);
      lcd.print("XXXX----");
      lcd.setCursor(10,0);
      lcd.print("CR=");
      lcd.setCursor(13,0);
      lcd.print(data);
      digitalWrite(safelt2, HIGH);
      digitalWrite(warnlt1, HIGH);
    }
    
    else if(data <= (average*1.35)){
      lcd.clear();
      digitalWrite(safelt2, LOW);
      digitalWrite(warnlt1, LOW);
      digitalWrite(warnlt2, LOW);
      digitalWrite(shutdwnlt, LOW);
      Serial.println("Warning Limits High");
      lcd.setCursor(0,0);
      lcd.print("Ave=");
      lcd.setCursor(4,0);
      lcd.print(average);
      lcd.setCursor(10,1);
      lcd.print("HR=");
      lcd.setCursor(13,1);
      lcd.print(hread);
      lcd.setCursor(0,1);
      lcd.print("XXXXXX--");
      lcd.setCursor(10,0);
      lcd.print("CR=");
      lcd.setCursor(13,0);
      lcd.print(data);
      digitalWrite(safelt2, HIGH);
      digitalWrite(warnlt1, HIGH);
      digitalWrite(warnlt2, HIGH);
}

    else if(data <= (average*1.5)){
      lcd.clear();
      digitalWrite(safelt2, LOW);
      digitalWrite(warnlt1, LOW);
      digitalWrite(warnlt2, LOW);
      digitalWrite(shutdwnlt, LOW);
      Serial.println("Shut Down Required");
      lcd.setCursor(0,0);
      lcd.print("Ave=");
      lcd.setCursor(4,0);
      lcd.print(average);
      lcd.setCursor(10,1);
      lcd.print("HR=");
      lcd.setCursor(13,1);
      lcd.print(hread);
      lcd.setCursor(0,1);
      lcd.print("XXXXXXXX");
      lcd.setCursor(10,0);
      lcd.print("CR=");
      lcd.setCursor(13,0);
      lcd.print(data);
      digitalWrite(safelt2, HIGH);
      digitalWrite(warnlt1, HIGH);
      digitalWrite(warnlt2, HIGH);
      digitalWrite(shutdwnlt, HIGH);
}


  else if(data > (average*1.5)){
      Serial.println("Shutting Down");
      lcd.clear();
      digitalWrite(safelt2, HIGH);
      digitalWrite(warnlt1, HIGH);
      digitalWrite(warnlt2, HIGH);
      digitalWrite(shutdwnlt, HIGH);
      digitalWrite(shutdwnsw, HIGH);
      lcd.setCursor(1,0);
      lcd.print("Limit Exceeded");
      lcd.setCursor(8,1);
      lcd.print("Max=");
      lcd.setCursor(12,1);
      lcd.print(data);
      delay(5000);
      lcd.clear();
      lcd.setCursor(0,0);
      lcd.print("Press Button to");
      lcd.setCursor(0,1);  
      lcd.print("Reset Sensor");
        while(0 == 0); // Causes infinate loop
        {}
  }
     
   delay(100);
}

 

I know the code is a bit messy and can be cut down, but for now it does the job. I will upload a couple of videos of it working in the field.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Thank you for checking out my blog,

 

Dale W