Experimenting with Vibration Sensors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Vibration Sensors
  • More
  • Cancel
Experimenting with Vibration Sensors
Forum L2CAP with BLE and STM32
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 3 subscribers
  • Views 2683 views
  • Users 0 members are here
  • ble
  • l2cap
  • stm32
  • bluenrg
Related

L2CAP with BLE and STM32

yosoufe
yosoufe over 5 years ago

Hi

 

It has been few weeks that I am trying to learn about Bluetooth low energy (BLE). This is the first time I code for bluetooth and I spent a lot on learning the basics. I managed to get my python script to communicate with the Nucleo board via the BLE expansion board. It seems the BLE is not designed for relatively large data. Every packet is like around 20 bytes of data. I read about L2CAP which seems it can increase the throughput. But I do not find an example or any code to use the BLE and L2CAP. L2CAP is marked as supported in the BLE exansion board but I do not know how to activate it and how it works.

 

My purpose is to be able to send the ADC measurements over BLE to the PC and do the rest of calculation on PC. It has been impossible to have a good speed of data transfer for this purpose. For example when I send 250 bytes from nucleo board to PC without L2CAP, it takes more than 1 seconds. The alternative is to do calculations on the nucleo board and use the BLE just as a notification.

 

If you know about the L2CAP and BLE please help me. I do not find anyway to send data using L2CAP with the bluenrg library as a server. bluenrg library has few functions to receive L2CAP stuff or sending as a client, but I could not find anything to initiate the communication over the L2CAP as server.

 

Thanks

Yousof

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 5 years ago

    Hi Yousof,

     

    I have not used the particular hardware or software that you mention, however generally it is not expected to be necessary to code at the L2CAP level. The software stack for BLE for your processor/environment, or firmware inside the RF function inside the chip, will do all that. You normally only have access at a higher level API, which will interact at GAP and GATT level, if not an even higher level friendlier abstraction.

    When you make the API calls that will cause interaction at these higher levels, and the BLE software stack will automatically convert the high level instructions into the low level L2CAP layer.

    It is easiest to imagine it like I2C communication where you normally send bytes to your i2c_write function call, and do not need to toggle the SDA/SCL lines individually.

    The high level API will translate down internally in the stack to the low layer, and will then be handled accordingly over the air.

     

    If you're actually not interested in using the supplied BLE stack and just want to transmit raw bytes and handle your own error detection, retransmits, your own channel selection etc., then the chip may have a 'raw' mode, but then that is not BLE, the stack is too complex to code, and such a raw mode will not work with a PC expecting BLE communications.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 5 years ago

    Hi Yousof,

     

    I have not used the particular hardware or software that you mention, however generally it is not expected to be necessary to code at the L2CAP level. The software stack for BLE for your processor/environment, or firmware inside the RF function inside the chip, will do all that. You normally only have access at a higher level API, which will interact at GAP and GATT level, if not an even higher level friendlier abstraction.

    When you make the API calls that will cause interaction at these higher levels, and the BLE software stack will automatically convert the high level instructions into the low level L2CAP layer.

    It is easiest to imagine it like I2C communication where you normally send bytes to your i2c_write function call, and do not need to toggle the SDA/SCL lines individually.

    The high level API will translate down internally in the stack to the low layer, and will then be handled accordingly over the air.

     

    If you're actually not interested in using the supplied BLE stack and just want to transmit raw bytes and handle your own error detection, retransmits, your own channel selection etc., then the chip may have a 'raw' mode, but then that is not BLE, the stack is too complex to code, and such a raw mode will not work with a PC expecting BLE communications.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • yosoufe
    0 yosoufe over 5 years ago in reply to shabaz

    Hi @shabaz, Thanks

     

    Correrct. The bluenrg library that is provided by ST does not seem to have L2CAP-suppported high level APIs (or I could not find). Maybe because cortex M7 is not powerful enough? Or it is not provided yet? I am not sure.

     

    I was not also thinking that I could write them myself image