Experimenting with Waterproof Connectors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Waterproof Connectors
  • More
  • Cancel
Experimenting with Waterproof Connectors
Blog Monitoring station for Underground Cold Storage (The kit, a box, OS reinstall - extra credit blog 1)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Waterproof Connectors to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: JWx
  • Date Created: 21 Apr 2023 10:00 PM Date Created
  • Views 2249 views
  • Likes 4 likes
  • Comments 13 comments
  • hammond ip68 enclosure
  • experimenting with Waterproof Connectors
  • lattePanda V1
Related
Recommended

Monitoring station for Underground Cold Storage (The kit, a box, OS reinstall - extra credit blog 1)

JWx
JWx
21 Apr 2023
LattePanda setup

14.IV, after minor delay caused by custom's clearance procedure, I have received package containing my challengers kit. Everything was prepared by E14 personnel, shipping procedure was straightforward and required only minimal engagement on receiver's side.

Package was sufficiently protected from accidental damage and contained

  • LattePanda box
  • Hammond waterproof enclosure
  • envelope containing most of connectors
  • and a box with SMA antenna pigtail

{gallery}The kit

image

Package contents

image

Packaged enclosure

image

Connector set - packaged

connector set

Amphenol connector set

image

Amphenol SMA pigtail box

image

LattePanda v.1 box

Provided enclosure was customized with Element14 and manufacturer's logos displayed on the case and dedicated holes were drilled for all the provided connectors.

image

As holes were individually shaped for each connector, correct fitting was very easy. Manufacturing tolerance was also excellent - for example: Ethernet connector would stay in it's place even without securing using screws.

Enclosure customization

Next - as I am planning to use LattePanda as monitoring station - I have decided to install it in dedicated enclosure. I have bought acrylic one - like this:

LattePanda v.1 acrylic enclosure

Inside the packaging one can find two acrylic, paper covered boards that are containing all the elements and one page assembly manual.

image

Assembly process is a little tricky - acrylic elements need to be gently removed as they are somewhat brittle and during the assembly enclosure behaves as some sort of 3D puzzle, but at the end it turns out to be sturdy and even can be opened again if some care is taken to not damage corner braces.

Final effect can be seen on the photo below (well - semi-final - without Wifi antenna. That's why the case needed to be opened again)

LattePanda enclosure

So - lets connect power supply, monitor, keyboard and see what happens...

After brief time Windows 10 desktop appeared:

Win10

but as our monitoring software is Linux-native we will need to reinstall the OS.

LattePanda documentation states that both MS Windows and GNU/Linux are officially supported, so let's use standard procedure described here:

https://docs.lattepanda.com/content/1st_edition/os/#linux-ubuntu-1604-lts

After downloading recommended Clonezilla image of Ubuntu 16.04 LTS (Long Time Support) (and MS Windows image for CR700 H/W version just in case - it is paid for in our version after all) and preparing boot USB drive using Rufus software minor inconsistency was encountered . Manual states that simply inserting USB drive and rebooting initiates installation, but in my case Panda booted into Windows every time.

So - we will need to change boot disk order. As in any PC computer, pressing dedicated key during reset enters BIOS/UEFI. In case of LattePanda, that key is ESC.

This way we entered familiar UEFI/BIOS interface:

Bios1

then, on "Boot" tab changed boot order to prefer USB disk

bios boot order

and after reboot installation has started. System image seems to be dedicated to another H/W version (CR200) but it installs correctly on our hardware.

Installation process progressed as in the manual and at the end we got  working Ubuntu GUI (login using admin:admin)

image

Next step - install SSH server and enable remote access. After connecting Ethernet cable system automatically got address using DHCP, but then repository problem appeared.

After issuing

apt-get update
apt-get install openssh-server

error message appeared informing about unmet dependencies. It turned out that the system used repository mirror at

http://mirror.neu.edu.cn

that seems outdated. Replacing all references to http://mirror.neu.edu.cn with http://archive.ubuntu.com/ in /etc/apt/sources.list file, then re-running

apt-get update
apt-get install openssh-server

installed openssh server correctly. Then let's install some monitoring tools

apt-get install lm-sensors
sensors-detect
sensors

and the result:

root@e14-waterproof-challenger:~# sensors
soc_dts1-virtual-0
Adapter: Virtual device
temp1:        +70.0°C

acpitz-virtual-0
Adapter: Virtual device
temp1:         +0.0°C  (crit = +100.0°C)

coretemp-isa-0000
Adapter: ISA adapter
Core 0:       +70.0°C  (high = +90.0°C, crit = +90.0°C)
Core 1:       +71.0°C  (high = +90.0°C, crit = +90.0°C)
Core 2:       +74.0°C  (high = +90.0°C, crit = +90.0°C)
Core 3:       +73.0°C  (high = +90.0°C, crit = +90.0°C)

soc_dts0-virtual-0
Adapter: Virtual device
temp1:        +71.0°C

No surprise that one type of enclosure has fan installed.

After verifying on the router what address LattePanda gets (or even better - add static DHCP MAC:IP_ADDR mapping  or even static IP address to not be surprised by sudden address change after DHCP lease expiration) we can access our Panda from another computer:

image

That's all about initial LattePanda setup, next we will cover installation of Influxdb, Grafana and our first data source (METAR based information about outdoor weather parameters).

  • Sign in to reply
  • JWx
    JWx over 3 years ago in reply to JWx

    or use the procedure I have described above - install 16.04, decustomize it (to get working repositories at least) and upgrade to 18.04 then 20.04 if needed (upgrade to 22.04 was initial failure for me - it stopped working and needed booting from Live CD image and manually upgrading the kernel). I am thinking about writing something about re/installing modern Ubuntu on LattePanda but it will take me some time - I am currently using it during Roadtest so I have to finish this task before reinstalling...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • JWx
    JWx over 3 years ago in reply to JWx

    Manufacturer suggests using Linuxium custom ISOs:

    https://docs.lattepanda.com/content/1st_edition/os/#install-ubuntu-operating-system-using-linuxium

    but - as far as I checked - they have only some improvements related to HDMI (if I remember correctly) support for Atom and publish Ubuntu versions up to 21.04 - so maybe those changes are merged into mainstream in newer releases... Personally I would try to install official 22.04 LTS ISO (written into USB stick using some program like Etcher or Rufus)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • JWx
    JWx over 3 years ago in reply to me_Cris

    This is rather straightforward from my experience - if one manage to boot Ubuntu image  from USB it will install (at least LattePanda provided Ubuntu 16.04 image I have tested - but upgrade to 18.04 then 20.04 worked flawlessly from standard repositories so standard image should also work). Fortunately hardware looks pretty standard (Intel Atom) so drivers should not be a problem. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • me_Cris
    me_Cris over 3 years ago in reply to JWx

    I tried in Arduino IDE to install ESP boards from manager, but it failed because there is not enough space.
    I'm pretty sure I'll install Ubuntu or something like that, .because I don't see how else I could use this LattePanda.  I'll look for a video on the internet about it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • JWx
    JWx over 3 years ago in reply to me_Cris

    That was also my initial feeling - so I downloaded Windows ISO just in case. But in my opinion there is no point of having Windows on raspberry like SBC with parameters of Intel-based tablet (btw - I have Windows tablet with 16GB of disk and this one is really unusable: it cannot even install bigger updates without external pendrive as temporary space). Maybe for arduino development? But I think that it can be somehow substituted in Linux...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>