Experimenting with Waterproof Connectors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Waterproof Connectors
  • More
  • Cancel
Experimenting with Waterproof Connectors
Experimenting with Waterproof Connectors Forum Can you make a splash with waterproof connectors?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Waterproof Connectors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 36 subscribers
  • Views 2751 views
  • Users 0 members are here
  • design challenge
  • waterproof connectors
Related

Can you make a splash with waterproof connectors?

cstanton
cstanton over 3 years ago

Connectors to me are perhaps the most easily overlooked part of a project.

Thinking about it though, they are obviously required. Whether you're toughing it out in a hostile environment, or designing a submersible!

What're your project ideas and what comes to mind for this design challenge?

  • Sign in to reply
  • Cancel

Top Replies

  • charlieo21
    charlieo21 over 3 years ago +2
    Splash? Submersion? Rain? Snow? Of course, sometimes when we're brainstorming for design ideas, we always assume that the users are idiots and they're going to do something really bad with the product…
  • JWx
    JWx over 3 years ago +2
    as some components are rated IP67, any submersible is not guaranteed to be operational after 30 minutes and/or below 1 meter of water, so operating Panda at the bottom of muddy puddle seems a bit risky…
  • Gough Lui
    Gough Lui over 3 years ago in reply to JWx +2
    Always test the connectors and enclosure without the expensive stuff inside first ... only when you're sure it's all fitted properly and is water tight, then you can risk the expensive stuff. But yes…
Parents
  • JWx
    JWx over 3 years ago

    as some components are rated IP67, any submersible is not guaranteed to be operational after 30 minutes and/or below 1 meter of water, so operating Panda at the bottom of muddy puddle  seems a bit risky... :)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to JWx

    Always test the connectors and enclosure without the expensive stuff inside first ... only when you're sure it's all fitted properly and is water tight, then you can risk the expensive stuff.

    But yes, while some are waterproof, they may not work properly while immersed especially if not mated with their matching counterpart. Standard only guarantees a certain pressure and time, so perhaps longer term tests are a good thing.

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 3 years ago in reply to Gough Lui

    yes - that's something worth testing, but I am afraid that during challenge's timeframe some problems would be hard to single-out (possible corrosion for example)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • JWx
    JWx over 3 years ago in reply to Gough Lui

    yes - that's something worth testing, but I am afraid that during challenge's timeframe some problems would be hard to single-out (possible corrosion for example)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • charlieo21
    charlieo21 over 3 years ago in reply to JWx

    A salt spray test could solve that issue, without a proper chamber that could not be the most accurate test but for experimenting purposes a bucket and some heat could be just enough.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago in reply to JWx

    Of course, and the statement of 'waterproof' makes the assumption that you're working with a clean source, but what if you're not?

    In fact, what if it's not only a contaminated liquid with particulates and free radicals, but a food based liquid?

    So many variables when 'liquid' is more of a state than simply acknowledging 'water'.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 3 years ago in reply to JWx

    I remember once having remote sensor for weather station sporting hole in the enclosure (some foil around LCD display peeled off) - and it was working at least several months (maybe a year) on balcony  (protected from direct rain but not from moisture) until it finally failed, so if water jet/submersion isn't tested one may not see any additional value of waterproof components. I have also encountered small car lamp with damaged seal that only failed when one of it's contacts was almost entirely eaten up by corrosion from being full of rain water...  So - it will be challenge to prepare meaningful tests for specified time-frame...