Experimenting with Waterproof Connectors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Waterproof Connectors
  • More
  • Cancel
Experimenting with Waterproof Connectors
Experimenting with Waterproof Connectors Forum Threaded Inserts to Mount RJ45 Backshell
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Waterproof Connectors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 35 subscribers
  • Views 1707 views
  • Users 0 members are here
  • hammond 1554VA2GYCL enclosure
  • threaded insert
  • experimenting with Waterproof Connectors
  • waterproof rj45 backshell
Related

Threaded Inserts to Mount RJ45 Backshell

ralphjy
ralphjy over 3 years ago

Now that we are getting the waterproof backshell/boot for the RJ45 cable, I've been looking for a threaded insert that could be used to attach the backshell to the enclosure.  Because the enclosure wall is only 3.3mm thick, I thought that a PEM fastener that I've used before for PCBs might be appropriate.  Because of the small shank length (1.5mm) and limited availability in small quantities, I decided to query Hammond Technical Support for their recommendations.

Here is their response:

image

imageimageimage

image

It looks like it might work, but there will be about zero clearance to the RJ45 jack body (because the insert will penetrate 2.2mm).

I also realized that the PEM nut wouldn't work because it would need to be installed from the inside and its shoulder dimension would definitely interfere with the jack body.

Has anyone found a better alternative?  I may try this one because Mouser has availabilty and sells in small quantities.

NFPC-440

image

The other possibility that I found is the E-Z LOK 240-004-CR.  This has a smaller body, so it would have better clearance and is 1mm shorter.  Not sure where to source these.

image

image

  • Sign in to reply
  • Cancel

Top Replies

  • ralphjy
    ralphjy over 3 years ago in reply to JWx +2
    Have not seen those fasteners before. The metric version of the backshell is an M3. The body diameter is 7.9mm of the well nut so this fastener would be too large for this application. It is also quite…
  • JWx
    JWx over 3 years ago +2
    There is something similar - this one is 1.85mm deep, should probably be installed from the inside (to minimize the possibility of accidental removal alongside with the screw) and it seems that even without…
  • JWx
    JWx over 3 years ago +1
    hello! there is something like "neopren rivet nut" (if translated correctly) - it should be waterproof (hole is sealed by neopren) and maybe it will not need specialized tools used in installing other…
Parents
  • JWx
    JWx over 3 years ago

    hello! there is something like "neopren rivet nut" (if translated correctly) - it should be waterproof (hole is sealed by neopren) and maybe it will not need specialized tools used in installing other rivet nuts (it expands when screw compresses neopren tube)...

    something like this

    https://www.albanycountyfasteners.com/blog/well-nuts-what-are-they-and-how-are-they-used/

    the problem is that they are hard to obtain here - especially in small numbers with non-metric threading

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy over 3 years ago in reply to JWx

    Have not seen those fasteners before. The metric version of the backshell is an M3. The body diameter is 7.9mm of the well nut so this fastener would be too large for this application.  It is also quite long.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ralphjy
    ralphjy over 3 years ago in reply to JWx

    Have not seen those fasteners before. The metric version of the backshell is an M3. The body diameter is 7.9mm of the well nut so this fastener would be too large for this application.  It is also quite long.