Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum raspberry pi2 - Internet not connecting through hostname, but connecting through IP
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 8 subscribers
  • Views 1522 views
  • Users 0 members are here
  • -
  • raspberry
  • internet
  • but
  • through
  • ip
  • hostname
  • not
  • connecting
  • pi2
Related

raspberry pi2 - Internet not connecting through hostname, but connecting through IP

e14 Contributor
e14 Contributor over 11 years ago

Hi

Thanks in Advance

Am using Rapsberry Pi2 with Raspbian Debian Wheezy OS, configured the network as static with my LAN Connection and accessing pi2 by Putty. I tried to ping google.com, am getting the following response 

pi@raspberrypi ~ $ ping google.com

ping: unknown host google.com


but if ping with IP Address, it is working. I tried with browser in pi2, google.com is not working whereas IP is working in browser.

 

pi@raspberrypi ~ $ ifconfig

eth0      Link encap:Ethernet  HWaddr b8:27:eb:81:d6:48

          inet addr:192.168.1.141  Bcast:192.168.1.255  Mask:255.255.255.0

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:1542 errors:0 dropped:0 overruns:0 frame:0

          TX packets:529 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:127751 (124.7 KiB)  TX bytes:103054 (100.6 KiB)

lo        Link encap:Local Loopback

          inet addr:127.0.0.1  Mask:255.0.0.0

          UP LOOPBACK RUNNING  MTU:65536  Metric:1

          RX packets:316 errors:0 dropped:0 overruns:0 frame:0

          TX packets:316 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:25456 (24.8 KiB)  TX bytes:25456 (24.8 KiB)

 

I don't know why the internet connection is not working, when am using hostname, Because of this, i couldn't get apt-get update, apt-get install, wget- ....

Pl Help

  • Sign in to reply
  • Cancel
Parents
  • fvan
    fvan over 11 years ago

    Can you show the network configuration file ? Did you specify one or more DNS servers ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fvan
    fvan over 11 years ago

    Can you show the network configuration file ? Did you specify one or more DNS servers ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to fvan

    Thanks for your reply, my network configuration file is

     

    auto lo

    iface lo inet loopback


    auto eth0

    allow-hotplug eth0

    iface eth0 inet static

    address 192.168.1.141

    netmask 255.255.255.0

    gateway 192.168.1.1

    preferred dns 202.138.103.100

    alternate dns 202.138.96.2


    auto wlan0

    allow-hotplug wlan0

    iface wlan0 inet manual

    wpa-conf /etc/wpa_supplicant/wpa_supplicant.conf


    auto wlan1

    allow-hotplug wlan1

    iface wlan1 inet manual

    wpa-conf /etc/wpa_supplicant/wpa_supplicant.conf