Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Starting with Raspberry Pi 3 with Windows 10 IOT and access db engine
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 6 subscribers
  • Views 2698 views
  • Users 0 members are here
  • frontpage
  • msaccess
  • windows 10 iot
Related

Starting with Raspberry Pi 3 with Windows 10 IOT and access db engine

amateurtje
amateurtje over 10 years ago

Hello All,

 

I am new here and the raspberry PI, Win10 IOT etc are all very new to me.

 

I have a system running which is made in vb.net and uses a serial box to read io ports. Information regarding this is stored in a access database. For a lot of reasons is this the easiest to use instead of other db's.

My questions are:

- Is it easy/do-able to transfer my current program developed in Visual studio to a program for the Win 10 IOT?

- I use a accessdatase engine plugin. Will I be able to use this on windows IOT?

          - or is there another way to store data in an access database?

 

Who can help me getting started?

 

Greetz

Amateurtje

  • Sign in to reply
  • Cancel
Parents
  • Workshopshed
    0 Workshopshed over 9 years ago

    Access is a very old application, I was using nearly 20 years ago when I first started work. It's also a desktop application so it's quite heavy weight by modern standards.

     

    We moved across from Access to VB+SQL server about 15 years back, it was a big job but of was also worth it. We've moved again since then to .Net+SQL server but are petty much database agnostic now.

     

    I would recommend porting across to an alternative database, the technologies for connecting to Access (JET and COM) are being phased out if they are not already unsupported.

     

    If you want to use Win10 IOT then SQLLite could be a good choice, or Azure if you want to offload the DB to a server.

     

    Some more on SQLLite

     

    https://blogs.windows.com/buildingapps/2016/05/03/data-access-in-universal-windows-platform-uwp-apps/#XSHq0kcvOYKS6PkA.9…

     

    One of the key technologies for accessing databases on .Net Entity Framework has a cut down version for IOT core.

     

    https://blogs.msdn.microsoft.com/dotnet/2016/06/27/entity-framework-core-1-0-0-available/

     

    One thing I have learnt over the last 20 years is not to get too personally attached to particular technologies as you often find support is dropped or the new version is incompatible. You've probably got a couple of years before Access becomes a real problem to support.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • amateurtje
    0 amateurtje over 9 years ago in reply to Workshopshed

    if ms wants to phase it out, why are they still selling ad including only ms Access in the office platform?

     

    For me the biggest and best reason is that there is no server aplication running on my customers networks. Just locally a db file and make ure it can  be "seen" by all indivudual users. as far as i know, all sql based db's have to run a (sometimes even costly) db server..

     

    or am i wrong? (pease do not tell me that mssql can be downloaded for free up till 5 users. I know, but it still has to run in their netswork as a server.)

    Because of the sensative  data, I also can not use a web based sql db....

     

    If you know a good alternative for that, I am very curious to know, beacause I am for sure not a supporter of the acces db, because untill now, it makes my life rather more difficult than easier.... So which db I can adress by just using a pluging or something in my vb.net program without installing servers...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Workshopshed
    0 Workshopshed over 9 years ago in reply to amateurtje

    >if ms wants to

    I've given up trying to second guess Microsoft.

     

    >all sql based db's have to run a (sometimes even costly) db server..

    No, that's not the case. There are options that don't have a separate server or service. Here's the ones that I know about, there may be others.

     

    For desktops/laptop based applications there is SQL Server Express which is a free edition. It runs locally with your application. We use this for ship-based applications where there is limited infrastructure and intermittent connectivity.

    For the IOT edition there SQLLite, also free, this would also run on desktops, phones etc.

     

    If you use something like Entity Framework(https://blogs.msdn.microsoft.com/dotnet/2016/06/27/entity-framework-core-1-0-0-available/ ) or Massive ( https://github.com/FransBouma/Massive ) then you can swap out different databases without changing code as long as you read your configuration settings from a file.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Workshopshed
    0 Workshopshed over 9 years ago in reply to amateurtje

    >if ms wants to

    I've given up trying to second guess Microsoft.

     

    >all sql based db's have to run a (sometimes even costly) db server..

    No, that's not the case. There are options that don't have a separate server or service. Here's the ones that I know about, there may be others.

     

    For desktops/laptop based applications there is SQL Server Express which is a free edition. It runs locally with your application. We use this for ship-based applications where there is limited infrastructure and intermittent connectivity.

    For the IOT edition there SQLLite, also free, this would also run on desktops, phones etc.

     

    If you use something like Entity Framework(https://blogs.msdn.microsoft.com/dotnet/2016/06/27/entity-framework-core-1-0-0-available/ ) or Massive ( https://github.com/FransBouma/Massive ) then you can swap out different databases without changing code as long as you read your configuration settings from a file.