Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum 25-45 DC in, I need 12V DC out.
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 32 replies
  • Answers 18 answers
  • Subscribers 11 subscribers
  • Views 6249 views
  • Users 0 members are here
Related

25-45 DC in, I need 12V DC out.

maroka
maroka over 9 years ago

I need stable 12v for the LED turn signals on my motorcycle but the bike doesn't have a battery (from the factory) so everything is in AC. I used a bridge rectifier (KBPC5010) which outputs anywhere between 25-45 volts DC (maybe even more since I didn't rev it too high and it depends on engine RPM) but my flasher relay works on 12V. I made a circuit containing a 1000uF capacitor, 7812 stabilizer and 2 smaller ceramic capacitors, the components were connected in that order. It worked, the output I got was a stable 11.9V (according to my butchered multimeter). I put all of that in a plastic shroud from a glowplug relay and hot glued everything in place. It worked for a little bit until it stopped working, the capacitors are fine but the 7812 stabilizer shows no voltage on the output pin. My question is, did I fry it with too much voltage coming out of the rectifier, or was my mistake inadequate cooling? What would you guys suggest I build to make my turn signals work? Thanks in advance!

  • Sign in to reply
  • Cancel
Parents
  • WarrenW
    0 WarrenW over 9 years ago

    Firstly, msimon  is correct the input voltages of a 7812 will not withstand prolonged high voltage. There is a high voltage equivalent but it may be better to consider a transistor series regulator.

    I have attached a simple circuit for reference. Select a transistor that has enough voltage Vce rating and current.

    Filter capacitors do not need to be huge. Input filter is the most critical. Make it perhaps 470Uf 63V. Zener diode is 12 volt.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • maroka
    0 maroka over 9 years ago in reply to WarrenW

    Thanks for the help! I'll see what I can come up with. Can you perhaps suggest some components I should use, like the transistor and the resistor? I went on the local hardware store's website and there so many different kinds that it's overwhelming. Once again, I apologize for asking such questions. Also, about the capacitors, the ones apart from the input, can I get away with using ceramic capacitors?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • maroka
    0 maroka over 9 years ago in reply to WarrenW

    Thanks for the help! I'll see what I can come up with. Can you perhaps suggest some components I should use, like the transistor and the resistor? I went on the local hardware store's website and there so many different kinds that it's overwhelming. Once again, I apologize for asking such questions. Also, about the capacitors, the ones apart from the input, can I get away with using ceramic capacitors?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • WarrenW
    0 WarrenW over 9 years ago in reply to maroka

    It would depend upon the final current draw of the indicators - I would suggest perhaps a TIP3055 on a heatsink and a 2k2 resistor (1 watt). Make the zener a 1 watt as well (softer regulation and more robust). Output filter capacitor can be 100UF 25V the one across the zener can be the same.

    Very reliable circuit and extremely robust - but you should always have a fuse in circuit for protection (input side).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • maroka
    0 maroka over 9 years ago in reply to maroka

    A little update, I found this: DC/DC Понижаващ модул с LM2596HV, LM2576HV | Захранване Ком
    It's pretty cheap and the store is in my country. It's based on the LM2576HV and I've seen some reviews on the internet and people seem happy with it. On the page there's a "drawbacks" section. It says that when the difference between the input and the output voltage is greater 15-20V, the board can't reach its output of 2 amps without overheating, in order to do it, it needs a different inductor. I don't think a bunch of LEDs can draw 2 amps (though as I said I'm no expert so I could be entirely wrong) what do you guys think?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer