Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum 25-45 DC in, I need 12V DC out.
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 32 replies
  • Answers 18 answers
  • Subscribers 11 subscribers
  • Views 5932 views
  • Users 0 members are here
Related

25-45 DC in, I need 12V DC out.

maroka
maroka over 9 years ago

I need stable 12v for the LED turn signals on my motorcycle but the bike doesn't have a battery (from the factory) so everything is in AC. I used a bridge rectifier (KBPC5010) which outputs anywhere between 25-45 volts DC (maybe even more since I didn't rev it too high and it depends on engine RPM) but my flasher relay works on 12V. I made a circuit containing a 1000uF capacitor, 7812 stabilizer and 2 smaller ceramic capacitors, the components were connected in that order. It worked, the output I got was a stable 11.9V (according to my butchered multimeter). I put all of that in a plastic shroud from a glowplug relay and hot glued everything in place. It worked for a little bit until it stopped working, the capacitors are fine but the 7812 stabilizer shows no voltage on the output pin. My question is, did I fry it with too much voltage coming out of the rectifier, or was my mistake inadequate cooling? What would you guys suggest I build to make my turn signals work? Thanks in advance!

  • Sign in to reply
  • Cancel
Parents
  • maroka
    0 maroka over 9 years ago

    Thanks for the input guys, I was looking at some Buck converters, but then I encountered this 14-50V To 12V 5.5*2.5DC Male Converter CPT Power Supply Step Down Regulator Car | eBay

    It's really cheap for what it seems to do, the thing is that it's rated at 1.5A on the output. I'm not an electrical engineer, far from it, so I may be asking stupid questions, but will this converter work? If not, what can I do about the current output being too high on the rectifier. As I said, I apologize for asking questions that may seem stupid. It's all new for me, so I appreciate anything you share.

     

    Thank you for the replies.

     

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • maroka
    0 maroka over 9 years ago

    Thanks for the input guys, I was looking at some Buck converters, but then I encountered this 14-50V To 12V 5.5*2.5DC Male Converter CPT Power Supply Step Down Regulator Car | eBay

    It's really cheap for what it seems to do, the thing is that it's rated at 1.5A on the output. I'm not an electrical engineer, far from it, so I may be asking stupid questions, but will this converter work? If not, what can I do about the current output being too high on the rectifier. As I said, I apologize for asking questions that may seem stupid. It's all new for me, so I appreciate anything you share.

     

    Thank you for the replies.

     

    Regards