Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum 10 Red LED chaser modules
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 5 answers
  • Subscribers 9 subscribers
  • Views 2135 views
  • Users 0 members are here
  • frontpage
Related

10 Red LED chaser modules

starkillerpj
starkillerpj over 9 years ago

i am thinking of making some LED modules that contain 10 LEDs in it and have connections on either end to increase the number of :LEDs and a 2*5 header to connect to a Arduino Mega 2560 or raspberry PI micro controller.

Was going with 8 , but cant get a 2*4 Female Header

  • Sign in to reply
  • Cancel
Parents
  • starkillerpj
    0 starkillerpj over 9 years ago

    Shift Registers won't work with my project, what's actually needed is a 3 to 8 line decoder

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to starkillerpj

    Why not ?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 9 years ago in reply to balearicdynamics

    Why not ?

     

     

    I have the same question. You can chain shift registers together so that the output of one is the input of the next. The software just has to push the extra bits out to cover the extra registers. OpenSprinkler does that for their sprinkler zones. (for details, look at the circuit diagram for their expansion units).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 9 years ago in reply to ntewinkel

    ps, It will probably be easier to have each module include a multiple of 8 LEDs, as that matches what a shift register or decoder can handle.

     

    I suppose another idea is to use a small microcontroller in each module - ATTiny chips are very inexpensive. Use some pins for input, some for output.

    The input takes information from the source, or the previous module, and the output sends a (slightly modified) copy of the input on to the next module. A basic serial connection would probably work.

    Then you could do what Andy said about neopixels to make them individually addressable.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 9 years ago in reply to ntewinkel

    ps, It will probably be easier to have each module include a multiple of 8 LEDs, as that matches what a shift register or decoder can handle.

     

    I suppose another idea is to use a small microcontroller in each module - ATTiny chips are very inexpensive. Use some pins for input, some for output.

    The input takes information from the source, or the previous module, and the output sends a (slightly modified) copy of the input on to the next module. A basic serial connection would probably work.

    Then you could do what Andy said about neopixels to make them individually addressable.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer