Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum S.N.A.F.U. Project - Spoofers Need A Final Undoing
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 6 answers
  • Subscribers 11 subscribers
  • Views 1825 views
  • Users 0 members are here
  • telemarketers
  • robocalls
  • caller id spoofing
Related

S.N.A.F.U. Project - Spoofers Need A Final Undoing

rmcoutu33mcintoshent
rmcoutu33mcintoshent over 8 years ago

Victim less Crimes? Robocalls, Caller ID Spoofing, IRS Scams, These are all things associated with having a telecommunications contract which pretty much affects anyone these days. there are unscrupulous persons all over the face of the earth using VOIP and spoofing services to conduct robocalling campaigns with the intent of defrauding our loved ones and it goes on 24-7 all year long. I am asking the Element 14 community to engage into combat with these insensitive individuals. Technology has been created to allow us to avoid the unwanted annoyances of greedy Telemarketers using Caller ID, Caller ID spoofing has been the criminal response. What some individuals have done is create electronics to weed out robocallers(Tele-zapper,CPR5000, and a number of devices that function so poorly they are no longer available)

 

 

Cutting to the chase, it would be wonderful/and profitable if a member of the community could develop a device that can use the spoofed caller ID information by calling from a celular phone connected via USB dongle to confirm if the ID'd # is indeed busy, and not spoofed to allow the caller to dial 1 to be routed to the base station and either be answered by user or leave a message. In the event the cell call gets a cant't connect , or this number is out of service message, the caller gets disconnected. If the device could access a database of suspected robocall numbers to preempt the previously described process and then follow through on Spoofed call detection that would streamline the call screening process and put a serious SNAFU in the scoundrels process.                                                                                  

 

Pinterest
  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 8 years ago

    Hi Rene,

    I have found myself answering with anger in my voice and then I have to apologize when it turns out to be someone I know and want to talk to. We may all be more connected than ever before but in many ways it is not as good as it used to be. Another thing that bugs me is you can't look anyone up in the phone directory anymore. If you don't have their phone number from some other source you are out of luck. Last gripe is that my children will not answer my calls but they will answer a text message. What's with that?

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • danielw
    0 danielw over 8 years ago in reply to jw0752

    I've answered with a rather gruff tone to the mother in law, I then have to explain about expecting it to be a call centre on about viruses or my internet connection.  She didn't seem impressed!

     

    You're also spot on with children not answering calls but will answer texts.  Yet I see them chatting to their mates holding the phone like they are on the apprentice even when they are on their own, nobody else needs to hear!

    If it's annoying me, sometimes I'll say random words loudly,  "TROM-BONE" is a firm favourite,  Though you do need to emphasise a separation in the word for maximum comedy effect!

    image

    Is she on the phone, or so hungry she's confused it with a cracker with a nice bit of cheese?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • danielw
    0 danielw over 8 years ago in reply to jw0752

    I've answered with a rather gruff tone to the mother in law, I then have to explain about expecting it to be a call centre on about viruses or my internet connection.  She didn't seem impressed!

     

    You're also spot on with children not answering calls but will answer texts.  Yet I see them chatting to their mates holding the phone like they are on the apprentice even when they are on their own, nobody else needs to hear!

    If it's annoying me, sometimes I'll say random words loudly,  "TROM-BONE" is a firm favourite,  Though you do need to emphasise a separation in the word for maximum comedy effect!

    image

    Is she on the phone, or so hungry she's confused it with a cracker with a nice bit of cheese?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer