Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Build a scale that has a display, tare function and be able to fire a relay to switch a valve
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 8 answers
  • Subscribers 10 subscribers
  • Views 3223 views
  • Users 0 members are here
Related

Build a scale that has a display, tare function and be able to fire a relay to switch a valve

sgoodman
sgoodman over 7 years ago

Good morning all,

 

I am looking to build a filling scale that has the ability to be able to have the weight of the bottle removed with a TARE feature and to be able to signal a relay when we hit our fill weight to shut the flow off and repeat to fill hundreds of bottles.

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 7 years ago

    There are many possible technologies and methodologies to perform this function that have been successfully employed in industry, including all the techniques mentioned so far. They all require significant knowledge to implement well, but the issues have been solved and the information is available. The learning curve cannot be avoided when designing a system but the real question is which method should be investigated, researched and learned? Because learning them all is a much bigger task.

    • peristaltic pump - does not contaminate the fluid
    • weight - can be a simple spring with a switch or strain gauges or a load cell with lots of circuitry and possibly software
    • timed valve (volume)
    • mass flow measurement
    • volume flow measurement
    • volumetric cut-off
    • fill level cut-off
    • Presssure measurement
    • float switch
    • spring switch
    • ultrasonic level measurement
    • acoustic resonance
    • conductive switch (level sensor)
    • video inspection
    • overflow switch
    • optical reflection
    • optical attenuation
    • radar level measurement
    • depth gauge
    • balance switch (when the balance starts to move, an optical switch is triggered)

    And there are many more - these are just the ones that immediately come to mind that I have used or researched. Each method could have a whole book full of theory, datasheets, app notes and examples. The best choice cannot be made without knowing the fluid and bottle characteristics and what is riding on the system performance.

    It may be possible to eliminate some of the learning curve by selecting subsystems that meet the requirements - for example it is difficult to design a strain gauge solution because the mechanics and electronics are tricky. A load cell is a ready-made strain gauge solution that includes some of the mechanical design but it is still tricky to make an accurate system. A set of scales with electronic output includes most of the tricky mechanical design and the scales can even have a tare function built-in. Of course as you get more complete systems, the price goes up and the device becomes less specifically designed for the application.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 7 years ago

    There are many possible technologies and methodologies to perform this function that have been successfully employed in industry, including all the techniques mentioned so far. They all require significant knowledge to implement well, but the issues have been solved and the information is available. The learning curve cannot be avoided when designing a system but the real question is which method should be investigated, researched and learned? Because learning them all is a much bigger task.

    • peristaltic pump - does not contaminate the fluid
    • weight - can be a simple spring with a switch or strain gauges or a load cell with lots of circuitry and possibly software
    • timed valve (volume)
    • mass flow measurement
    • volume flow measurement
    • volumetric cut-off
    • fill level cut-off
    • Presssure measurement
    • float switch
    • spring switch
    • ultrasonic level measurement
    • acoustic resonance
    • conductive switch (level sensor)
    • video inspection
    • overflow switch
    • optical reflection
    • optical attenuation
    • radar level measurement
    • depth gauge
    • balance switch (when the balance starts to move, an optical switch is triggered)

    And there are many more - these are just the ones that immediately come to mind that I have used or researched. Each method could have a whole book full of theory, datasheets, app notes and examples. The best choice cannot be made without knowing the fluid and bottle characteristics and what is riding on the system performance.

    It may be possible to eliminate some of the learning curve by selecting subsystems that meet the requirements - for example it is difficult to design a strain gauge solution because the mechanics and electronics are tricky. A load cell is a ready-made strain gauge solution that includes some of the mechanical design but it is still tricky to make an accurate system. A set of scales with electronic output includes most of the tricky mechanical design and the scales can even have a tare function built-in. Of course as you get more complete systems, the price goes up and the device becomes less specifically designed for the application.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer