Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum RE: Seeking Feedback on New Scoring System for Experimenting Challenges
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 12 subscribers
  • Views 6704 views
  • Users 0 members are here
  • Experimenting Challenges
  • new scoring system
Related

RE: Seeking Feedback on New Scoring System for Experimenting Challenges

rscasny
rscasny over 3 years ago

Note: this discussion covers only the Experimenting Design Challenge Competitions

Greetings to All,

I would like to introduce a blog scoring system in addition to the judges I use to determine the top prize winners of the experimenting with components challenges (e.g, capacitors, inductors, vibration sensors, etc.).

I would like to get feedback on this proposal by members of element14.

Before I detail the change, let me explain why I am suggesting it? There are a couple of reasons:

  • Transparency: The blog will be scored on a weekly basis and the score posted in a table similar to what I used in another one of my programs. Here is an example of the table I had used in that program. Click here to see.
  • Strategy: With participants seeing the point totals of all participants, they can plan a strategy for achieving a point total to win.
  • Ensuring Participation Throughout the Program Period: Sometimes participants post their blogs at the end of the 8 to 10 week period, not giving me the opportunity to promote the blogs through the program period. In addition, giving participants a reason to post supporting blogs throughout the active period allows them to pick up points along the way.
  • Making Judging More Convenient: Our judges will receive the final summary blog to judge, which I think will make it easier for them to manage. Since the final summary blog can earn the most points, the judges' decision will have the most weight in the final selections.

What is the Judging/Scoring System In Place Now?

There is a two-blog minimum required to successfully finish the competition. There is no scoring system in place now. Currently, at the conclusion of the competition (usually 8 to 10 weeks), I forward all the blogs of each participant to the judges. The judges rank the blogs and select the winners of the top prizes. At the end of the judging, I notify the winners and write a winner's announcement.

What is the Judging/Scoring System That I Would Like to Introduce?

There will be no blog minimum, but each participant needs to blog to accrue points to win the top prizes. There will be three scoring types, as follows:

  • Introductory Blog: participant describes in detail what he/she plans on doing. Worth up to 75 points.
  • Final Summary Report Blog: participant describes in details what he/she did and proposed in the introductory blog. What experiments were conducted. What results were obtained? What were the takeaways, that is, what was learned. Worth up to 200 points.
  • Intermediary Supporting Blogs: these are blogs that support their experimenting program but are not the Introductory or Final Summary Blogs. Each weekly blog is worth up to 10 points.

The overall point totals will be posted on the table on a weekly basis.

The typical program timeline will be:

  • The up-to-75-point Introductory blog: Needs to be posted in Week 1 and Week 2
  • The up-to-10-point Intermediary Supporting Blogs: Need to be posted each week in Weeks 3 through 9.
  • The up-to-200-point Final Summary Blog: Needs to be posted in week 10.

Element14 will assign points for the Introductory and Supporting Blogs.

The judges will assign points for the Final Summary blog.

The members with the most points at the end of the program period will win.

What do you think?

Randall
--element14 Team; Experimenting Challenge Program Manager

  • Sign in to reply
  • Cancel
Parents
  • rscasny
    rscasny over 3 years ago

    May I ask one more question to everyone?

    We normally have a Grand Prize, a Runner Up prize and a complimentary finisher's prize for those people who wrote a minimum of two blogs.

    I am thinking about dropping the finishers prizes and replacing it with a Third Prize of about the same value as all the finishers' prizes.

    What do you feel about me doing this change?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 3 years ago in reply to rscasny

    I think finisher prize for all who spend some time with competition is better than one more valuable prize because other finishers can feel like it was waste of time and do not apply anymore. If you receive something, even it is very cheap device, then it motivates you to try it again in next competition.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to misaz

    I like the finisher prize too. A little token for having gone along for the ride.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to misaz

    I like the finisher prize too. A little token for having gone along for the ride.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Gough Lui
    Gough Lui over 3 years ago in reply to rscasny

    Yes, I'm also in favour of having a finisher prize ... it can be quite a lot of effort even if you don't win, so something is perhaps nice to have as a token of appreciation, as tempting as it is to have a third prize.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to Jan Cumps

    2 and 0 for the finisher prize and counting!

    • Cancel
    • Vote Up +3 Vote Down