Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum RE: Seeking Feedback on New Scoring System for Experimenting Challenges
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 12 subscribers
  • Views 6533 views
  • Users 0 members are here
  • Experimenting Challenges
  • new scoring system
Related

RE: Seeking Feedback on New Scoring System for Experimenting Challenges

rscasny
rscasny over 3 years ago

Note: this discussion covers only the Experimenting Design Challenge Competitions

Greetings to All,

I would like to introduce a blog scoring system in addition to the judges I use to determine the top prize winners of the experimenting with components challenges (e.g, capacitors, inductors, vibration sensors, etc.).

I would like to get feedback on this proposal by members of element14.

Before I detail the change, let me explain why I am suggesting it? There are a couple of reasons:

  • Transparency: The blog will be scored on a weekly basis and the score posted in a table similar to what I used in another one of my programs. Here is an example of the table I had used in that program. Click here to see.
  • Strategy: With participants seeing the point totals of all participants, they can plan a strategy for achieving a point total to win.
  • Ensuring Participation Throughout the Program Period: Sometimes participants post their blogs at the end of the 8 to 10 week period, not giving me the opportunity to promote the blogs through the program period. In addition, giving participants a reason to post supporting blogs throughout the active period allows them to pick up points along the way.
  • Making Judging More Convenient: Our judges will receive the final summary blog to judge, which I think will make it easier for them to manage. Since the final summary blog can earn the most points, the judges' decision will have the most weight in the final selections.

What is the Judging/Scoring System In Place Now?

There is a two-blog minimum required to successfully finish the competition. There is no scoring system in place now. Currently, at the conclusion of the competition (usually 8 to 10 weeks), I forward all the blogs of each participant to the judges. The judges rank the blogs and select the winners of the top prizes. At the end of the judging, I notify the winners and write a winner's announcement.

What is the Judging/Scoring System That I Would Like to Introduce?

There will be no blog minimum, but each participant needs to blog to accrue points to win the top prizes. There will be three scoring types, as follows:

  • Introductory Blog: participant describes in detail what he/she plans on doing. Worth up to 75 points.
  • Final Summary Report Blog: participant describes in details what he/she did and proposed in the introductory blog. What experiments were conducted. What results were obtained? What were the takeaways, that is, what was learned. Worth up to 200 points.
  • Intermediary Supporting Blogs: these are blogs that support their experimenting program but are not the Introductory or Final Summary Blogs. Each weekly blog is worth up to 10 points.

The overall point totals will be posted on the table on a weekly basis.

The typical program timeline will be:

  • The up-to-75-point Introductory blog: Needs to be posted in Week 1 and Week 2
  • The up-to-10-point Intermediary Supporting Blogs: Need to be posted each week in Weeks 3 through 9.
  • The up-to-200-point Final Summary Blog: Needs to be posted in week 10.

Element14 will assign points for the Introductory and Supporting Blogs.

The judges will assign points for the Final Summary blog.

The members with the most points at the end of the program period will win.

What do you think?

Randall
--element14 Team; Experimenting Challenge Program Manager

  • Sign in to reply
  • Cancel
  • rscasny
    rscasny over 3 years ago in reply to dougw

    This is my first thought on this system:

    --If the supporting blog is value adding (better explains something, helps some understand better, is very relevant, etc.), it merits the full ten points

    --If the supporting blog is only an unboxing that adds images and repeats info in data sheets, it merits 5 points.

    --If the supporting blog is a blog just for the sake of writing a blog (ie., telling me he received the kit and photos of the kit and nothing more, it merits only 2 points

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to misaz

    This needs clarification. Let's say for example Week 3 starts on Jan 22 and Week 4 starts on Jan 29th and week 5 starts on Feb 5th. In other words, three weeks. Each week you will get awarded a maximum of ten points for supporting blogs. Hence, for 3 weeks, that's 30 points. If people understand that, they are not going to write 50 blogs nor expect 500 points. Thus, I need to work on clarifying these instructions. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to misaz

    You mention a lot of things. Thanks for taking the time to join this conversation. I'll address two of them now. 

    Supporting blogs should not get all the same points. Yes, for the 7 ways program, most of the activities but not all of them I awarded with the same points. But this was different from Experimenting. If I asked them to write the differences between Spartan 6 and Spartan 7, the blogs would be similar since they were based on the same source info from the sponsor. Hence, similar point awards. For experimenting challenge, the supporting blogs would inherently be different. But to answer your question, yes they could be score differently. I am thinking of a standard such as the following:

    If the supporting blog is value adding (better explains something, helps some understand better, is very relevant, etc.), it merits the full ten points

    If the supporting blog is only an unboxing that adds images and repeats into in data sheets, it merits 5 points.

    If the supporting blog is a blog just for the sake of writing a blog (ie., telling me he received the kit and phots of the kit and nothing more, it merits only 2 points. 

    Your other suggestions concerned quantifying forum assistance. Very hard to track that in not only a democratic manner but also would not take much time. I would have to do that. I would not burden the judges with that task. 

    Perhaps I could create a poll at the end of the program asking the community which participant do you feel has provided the most support? The top vote get would receive, say, a 20-point bonus. Just thinking out loud. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to dougw

    Yes, there is more :"administrative overhead" with the table. As I told shabaz, 7 ways had 25 participants, while my upcoming Experimenting Challenge will have 7, due primarily due to budgeting limitations. So, it's less work. I'd also add the updating of the table into our project management tool. You ask some really great questions. I felt that the 7 Ways approach got more participation and it was a checklist for the participants. Would it alter the results? I can't be certain, but for one or two of them, it could have. I've really soul-searched about how much a burden I should be placing on the judges. I know some of them have full time jobs. I have been concerned about sending the judges 30 or 40 individual blogs to judge and then requiring them to rank the participants. I want the final decision to rest with the judges,yet at the same time foster participation throughout the program's timeline. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago

    How many of these are important in a scoring system and how would you rank their importance? Are there other important properties?

    • technical content
    • creativity
    • entertainment and engagement value
    • significant content published regularly throughout the contest period
    • clarity & completeness
    • effort expended
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to shabaz

    For the 7 Ways program, there were 25 participants. I was able to update the table and it didn't take that much time. I did have to spend a bit of time verifying if a participant completed a task. Actually, the quiz was the most time consuming because we have to go to a database and then search through some data. For the upcoming Experimenting challenges, I am looking at 7 to 10 applicants. So, I think it's manageable to do a table of this sort. The reports I got back from participants is that they really like the transparency. They knew were they stood, point wise.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 3 years ago in reply to shabaz

    I did not take abuses in account. Of course if some start flooding too much questions, then he/she will receive 0 or very few points for it. Similarly you can abuse intermediary blogs. Some can split his text in a ways one blog -> one paragraf and then he will easily have tons of intermediate blogs but I gues it will not receive lot of points for it. Even worse, you can post 50 blogs of lorem ipsum with idea that 50 blogs can bring you up to 500 points! In this cases the magic words "up to" should apply and zero points still satisfy rule up to 10 points.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 3 years ago in reply to dougw

    I agree that it is lot of work and maybe this rule can be relaxed slightly. I mainly highlighted the situation when all received full points which eficiently decraded score to true/false ranking.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to misaz

    I like the idea that every score should be different, but that adds a lot of judging work. Maybe someone can come up with an easy way to achieve accurate differentiated scores without a huge amount of judging work.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to misaz

    Interesting points. For what it's worth, I think the "forum activity should count. Both question and answers should count." would be hard to deal with, because then judges need to go through all the comments as well as the blog content. Also, it could be open to abuse, by people just replying many times with not as much help as required (e.g. mundane comments instead of well thought out responses). i think the onus on getting answers to challenge issues should be on the contestants, they are best placed to do it, and if they cannot find the answer on the forum then they can ask a question anwhere, e.g. on their blog, on someone elses blog or other sites. Collecting up questions and answers in discussions seems (to me) difficult (unless I've misunderstood it). If people are not responding to questions asked of them, then it becomes clear they are not a team player, and you wouldn't get much of an answer from them even if there were (say) 10 points for a response.

    Regarding ranking, sometimes content is just as good, so it would be nice if there was still a way to recognize that sometimes people do equally well in different ways. But I can see it would make it hard for contestants during the contest, who might prefer ranking (unless they are going to come second or third when their content may be equally as good! :) 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>