Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Seeking your Feedback on Proposed Kit and Prizes for Single Pair Ethernet Challenge
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 33 replies
  • Subscribers 12 subscribers
  • Views 4506 views
  • Users 0 members are here
  • experimenting with single pair ethernet
  • member discussion
Related

Seeking your Feedback on Proposed Kit and Prizes for Single Pair Ethernet Challenge

rscasny
rscasny over 2 years ago

Hi All.

In July I had a discussion with you regarding my plans to launch an Experimenting with Single Pair Ethernet Challenge.

Back then, I just began thinking about the challenge's kit and was interested in getting your input on what a kit could include. I took that feedback and began looking at the kit and the costs, etc.

In this follow up discussion, I am listing below a kit I would like you to take a look at. BEfore I get into the kit, let me talk about the challenge a bit more.

There are a couple important things to achieve in this challenge.

I don't believe we have had a sponsored activity on Single Pair Ethernet (SPE). So, one important thing is to begin exploring and learning about SPE in this challenge. Unfortunately, costs and/or budgets limit what I can offer in the kit, but I hope what we can afford to offer is worth your time to participate.

Since this challenge is primarily sponsored (paid for) by Molex, we would like you to use the Molex parts in whatever you do.

So here's the kit below.

Take a look and vote in the polls or leave a comment. Thanks.

ANALOG DEVICES EVAL-ADIN1110EBZ Evaluation Kit, ADIN1110CCPZ, Ethernet Physical Layer Device, Ethernet MAC-PHY, 10BASE-T1L

image

User Guide

ANALOG DEVICES EVAL-ADIN1100EBZ Evaluation Kit, ADIN1100CCPZ, Ethernet Physical Layer Device, 10BASE-T1

image

User Guide

RASPBERRY-PI RPI4-MODBP-4GB SBC, Raspberry Pi4 B 4GB, BCM2711, ARM Cortex-A72, 4GB RAM

image

Datasheet

ANALOG DEVICES EVAL-CN0575-RPIZ Evaluation Board, LTC9111IDE#TRPBF, Raspberry Pi Platform

image

User Guide

DIGILENT 410-221 Pmod TMP2: Temperature Sensor 

image

Datasheet

MOLEX 2209570104 Ethernet Cable, SPE Plug to SPE Plug, STP (Shielded Twisted Pair), Green, 1 m, 3.3 ft

and

MOLEX 2209570108 Ethernet Cable, SPE Plug to SPE Plug, STP (Shielded Twisted Pair), Green, 5 m, 16.4 ft

image

Datasheet (1m)

Datasheet (5m)

MOLEX 2209570001 Modular Connector, SPE Jack, 1 x 1 (Port), 2P2C, IP20, Through Hole Mount

image

Datasheet

MOLEX 2209570002 Modular Connector, SPE Jack, 1 x 1 (Port), 2P2C, IP20, Through Hole Mount

image

Datasheet

Should anything be added to this kit?

None of our challenges offer a totally comprehensive kit. Hence, no kit is perfect. But given the kit we are proposing, is there anything you feel should be added? If it is something that doesn't bust the budget, we would consider adding it to the kit.

Proposed Prizes

Grand Prize

MULTICOMP PRO MP720025 US Digital Oscilloscope, 4 Analog, 100 MHz, 1 GSPS, 40 Mpts, 3.5 ns

image

Runner Up Prize

MULTICOMP PRO MP720011 US Digital Oscilloscope, 2 Analog, 100 MHz, 1 GSPS, 10 kpts, 3.5 ns

image

Finisher Prize

MULTICOMP PRO MP720782 US Oscilloscope, 2 Channel, 70 MHz, 250 MSPS, 6 kpts, 5 ns

image

  • Sign in to reply
  • Cancel
Parents
  • kmikemoo
    kmikemoo over 2 years ago

    I would like to see some male connectors added.  I get that there will be cables provided, but let's go crazy and (maybe) make our own, longer cables.  If I'm installing this in my plant, I want to know if I can use existing wiring - even if "less than compliant" in my application.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to kmikemoo

    I think that cable connectors are doubled as screwed terminal blocks in many cases, allowing for more permanent (but easier to prepare) connection - to be seen if in components in the kit...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago in reply to JWx

    Yes there are terminal blocks for cable connection. But I really need to have them connected by the connector/jacks, at least in one instance because the sponsor is wanting to see people use their connectors. Ideally, both could be used. I can add the make connectors since I believe I will be getting them directly from the sponsor. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rscasny
    rscasny over 2 years ago in reply to JWx

    Yes there are terminal blocks for cable connection. But I really need to have them connected by the connector/jacks, at least in one instance because the sponsor is wanting to see people use their connectors. Ideally, both could be used. I can add the make connectors since I believe I will be getting them directly from the sponsor. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • kmikemoo
    kmikemoo over 2 years ago in reply to rscasny

     rscasny Thumbsup  I've driven many, many miles just to switch two wires and heal a MODBUS network.  Connectors good.  Laughing