Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Seeking your Feedback on Proposed Kit and Prizes for Single Pair Ethernet Challenge
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 33 replies
  • Subscribers 12 subscribers
  • Views 4550 views
  • Users 0 members are here
  • experimenting with single pair ethernet
  • member discussion
Related

Seeking your Feedback on Proposed Kit and Prizes for Single Pair Ethernet Challenge

rscasny
rscasny over 2 years ago

Hi All.

In July I had a discussion with you regarding my plans to launch an Experimenting with Single Pair Ethernet Challenge.

Back then, I just began thinking about the challenge's kit and was interested in getting your input on what a kit could include. I took that feedback and began looking at the kit and the costs, etc.

In this follow up discussion, I am listing below a kit I would like you to take a look at. BEfore I get into the kit, let me talk about the challenge a bit more.

There are a couple important things to achieve in this challenge.

I don't believe we have had a sponsored activity on Single Pair Ethernet (SPE). So, one important thing is to begin exploring and learning about SPE in this challenge. Unfortunately, costs and/or budgets limit what I can offer in the kit, but I hope what we can afford to offer is worth your time to participate.

Since this challenge is primarily sponsored (paid for) by Molex, we would like you to use the Molex parts in whatever you do.

So here's the kit below.

Take a look and vote in the polls or leave a comment. Thanks.

ANALOG DEVICES EVAL-ADIN1110EBZ Evaluation Kit, ADIN1110CCPZ, Ethernet Physical Layer Device, Ethernet MAC-PHY, 10BASE-T1L

image

User Guide

ANALOG DEVICES EVAL-ADIN1100EBZ Evaluation Kit, ADIN1100CCPZ, Ethernet Physical Layer Device, 10BASE-T1

image

User Guide

RASPBERRY-PI RPI4-MODBP-4GB SBC, Raspberry Pi4 B 4GB, BCM2711, ARM Cortex-A72, 4GB RAM

image

Datasheet

ANALOG DEVICES EVAL-CN0575-RPIZ Evaluation Board, LTC9111IDE#TRPBF, Raspberry Pi Platform

image

User Guide

DIGILENT 410-221 Pmod TMP2: Temperature Sensor 

image

Datasheet

MOLEX 2209570104 Ethernet Cable, SPE Plug to SPE Plug, STP (Shielded Twisted Pair), Green, 1 m, 3.3 ft

and

MOLEX 2209570108 Ethernet Cable, SPE Plug to SPE Plug, STP (Shielded Twisted Pair), Green, 5 m, 16.4 ft

image

Datasheet (1m)

Datasheet (5m)

MOLEX 2209570001 Modular Connector, SPE Jack, 1 x 1 (Port), 2P2C, IP20, Through Hole Mount

image

Datasheet

MOLEX 2209570002 Modular Connector, SPE Jack, 1 x 1 (Port), 2P2C, IP20, Through Hole Mount

image

Datasheet

Should anything be added to this kit?

None of our challenges offer a totally comprehensive kit. Hence, no kit is perfect. But given the kit we are proposing, is there anything you feel should be added? If it is something that doesn't bust the budget, we would consider adding it to the kit.

Proposed Prizes

Grand Prize

MULTICOMP PRO MP720025 US Digital Oscilloscope, 4 Analog, 100 MHz, 1 GSPS, 40 Mpts, 3.5 ns

image

Runner Up Prize

MULTICOMP PRO MP720011 US Digital Oscilloscope, 2 Analog, 100 MHz, 1 GSPS, 10 kpts, 3.5 ns

image

Finisher Prize

MULTICOMP PRO MP720782 US Oscilloscope, 2 Channel, 70 MHz, 250 MSPS, 6 kpts, 5 ns

image

  • Sign in to reply
  • Cancel
  • kmikemoo
    kmikemoo over 1 year ago

    Not directly related to the Experimenting with Single Pair Ethernet Challenge, but it does involve single pair ethernet.

    Arduino has launched its Uno SPE shield (November 12, 2024).  Nothing I've read leads me to believe that the shield can power the Arduino.  According to ElectronicsWeekly.com, the SPE variant is 10BASE-T1S - the multidrop one - as opposed to the 10BASE-T1L variant used by the Analog Devices EVAL-ADIN1110EBZ Evaluation Kit (the long distance one).
    Arduino's target audience for this shield probably won't be dissuaded from trying it as power would be available at the point of application.  Still... not having that capability just seems to miss  out on one of the major features of SPE.

    And we're still wondering about that mysterious power coupler. Laughing

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to TAnsell

    I think it is a in the preparation phase. It will be under Challenges & Projects -> Design Challenges when it officially starts

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • TAnsell
    TAnsell over 2 years ago

    Looks like a very interesting bit of kit. The 100/1000Mbps alternatives are more directly applicable to my use cases, but the 10BASE-T1 version has a place, and is a great starting point for exploring. What's the process for participating?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mp2100
    mp2100 over 2 years ago

    I voted No (you don't need to add anything).  The pieces suggested look good.  If anything, I don't need another raspberry Pi, but I assume some testers would need it.  From what I've read, there will eventually be 100baseT-to-10baseT1L network switches.  I guess the EVAL-ADIN1100 serves that purpose for this Challenge.

    I've been seeing press releases that SPE is "coming soon" for at least 2 years now.  I am glad to see that there are some products to test, especially the temperature sensor.  My main interest in the SPE is to use it to replace the 4-20mA sensors, being able to gather sensor data and power them using SPE.

    I am also glad to see the connectors included, a mechanically robust improvement to RJ45 would be welcome. it's great that Molex wants these tested.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago in reply to JWx

    JWx That was exactly what I was wondering.  You answered my question.  Thank you.  Relaxed  It may or may not work in the factory but it's worth trying it out.  If it doesn't work... I'm not out a bunch of money.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 2 years ago in reply to scottiebabe

    scottiebabe said: "That card has a fancy SPE PSE controller on it"

    Isn't that what's needed for negotiating with the chip on the CN0575 board at the RPi end? Or am I missing something?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 2 years ago in reply to kmikemoo

    The application note says power source can be either the coupler or a USB cable to power the Pi. So this part can be optional in the kit. For me, the current kit looks fine.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to jc2048

    jc2048 That card has a fancy SPE PSE controller on it

    image

    https://www.analog.com/media/en/technical-documentation/data-sheets/ltc4296-1.pdf 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to kmikemoo

    would be nice, but I am not sure I can manage a project of that complexity in the expected time - additionally, if we could be getting a simple power coupler, no PD negotiation would be possible: LTC9111 would require a proper PSE to negotiate with...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to kmikemoo

    I think I have seen some companies offering connectors for terminating CAT[?] as parallel runs of SPE (with LC connectors) - like one below (but it could be something better than CAT5) - anyway, in my roadtest I have made a connection using 30m of CAT5 UTP and it worked (but it was in home not factory so the interference level was different)

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>