Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Seeking your Feedback on Proposed Kit and Prizes for Single Pair Ethernet Challenge
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 33 replies
  • Subscribers 12 subscribers
  • Views 4498 views
  • Users 0 members are here
  • experimenting with single pair ethernet
  • member discussion
Related

Seeking your Feedback on Proposed Kit and Prizes for Single Pair Ethernet Challenge

rscasny
rscasny over 2 years ago

Hi All.

In July I had a discussion with you regarding my plans to launch an Experimenting with Single Pair Ethernet Challenge.

Back then, I just began thinking about the challenge's kit and was interested in getting your input on what a kit could include. I took that feedback and began looking at the kit and the costs, etc.

In this follow up discussion, I am listing below a kit I would like you to take a look at. BEfore I get into the kit, let me talk about the challenge a bit more.

There are a couple important things to achieve in this challenge.

I don't believe we have had a sponsored activity on Single Pair Ethernet (SPE). So, one important thing is to begin exploring and learning about SPE in this challenge. Unfortunately, costs and/or budgets limit what I can offer in the kit, but I hope what we can afford to offer is worth your time to participate.

Since this challenge is primarily sponsored (paid for) by Molex, we would like you to use the Molex parts in whatever you do.

So here's the kit below.

Take a look and vote in the polls or leave a comment. Thanks.

ANALOG DEVICES EVAL-ADIN1110EBZ Evaluation Kit, ADIN1110CCPZ, Ethernet Physical Layer Device, Ethernet MAC-PHY, 10BASE-T1L

image

User Guide

ANALOG DEVICES EVAL-ADIN1100EBZ Evaluation Kit, ADIN1100CCPZ, Ethernet Physical Layer Device, 10BASE-T1

image

User Guide

RASPBERRY-PI RPI4-MODBP-4GB SBC, Raspberry Pi4 B 4GB, BCM2711, ARM Cortex-A72, 4GB RAM

image

Datasheet

ANALOG DEVICES EVAL-CN0575-RPIZ Evaluation Board, LTC9111IDE#TRPBF, Raspberry Pi Platform

image

User Guide

DIGILENT 410-221 Pmod TMP2: Temperature Sensor 

image

Datasheet

MOLEX 2209570104 Ethernet Cable, SPE Plug to SPE Plug, STP (Shielded Twisted Pair), Green, 1 m, 3.3 ft

and

MOLEX 2209570108 Ethernet Cable, SPE Plug to SPE Plug, STP (Shielded Twisted Pair), Green, 5 m, 16.4 ft

image

Datasheet (1m)

Datasheet (5m)

MOLEX 2209570001 Modular Connector, SPE Jack, 1 x 1 (Port), 2P2C, IP20, Through Hole Mount

image

Datasheet

MOLEX 2209570002 Modular Connector, SPE Jack, 1 x 1 (Port), 2P2C, IP20, Through Hole Mount

image

Datasheet

Should anything be added to this kit?

None of our challenges offer a totally comprehensive kit. Hence, no kit is perfect. But given the kit we are proposing, is there anything you feel should be added? If it is something that doesn't bust the budget, we would consider adding it to the kit.

Proposed Prizes

Grand Prize

MULTICOMP PRO MP720025 US Digital Oscilloscope, 4 Analog, 100 MHz, 1 GSPS, 40 Mpts, 3.5 ns

image

Runner Up Prize

MULTICOMP PRO MP720011 US Digital Oscilloscope, 2 Analog, 100 MHz, 1 GSPS, 10 kpts, 3.5 ns

image

Finisher Prize

MULTICOMP PRO MP720782 US Oscilloscope, 2 Channel, 70 MHz, 250 MSPS, 6 kpts, 5 ns

image

  • Sign in to reply
  • Cancel
  • rsjawale24
    rsjawale24 over 2 years ago

    This is going to be an interesting challenge! In most of the previous ones, we had some component based kits. Looking forward to the projects, would apply as well Slight smile

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago in reply to JWx

    JWx If you are going this route, you should get the ANALOG DEVICES LTC9111RMSE#PBF Industrial SPoE PD Controller as well. Thumbsup
    Newark p/n 65AK1982

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to rscasny

    yes - I would like to check if it is possible to build a low cost SPE PHY for some popular MCU using an universal PCB and hobbyist level tools... The package is smaller than some other designs, but having ADI as a sponsor makes part selection somewhat easier Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago in reply to JWx

    You would like one of these. Just the chip:

    ADIN1100BCPZ - Analog Devices - Ethernet Controller, Ethernet PHY, IEEE 802.3cg-2019 (newark.com)

    YEs, that can be added.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago

    personally I would like to also obtain a sample of SPE PHY chip (like ADIN1100) to try to interface it to something - I know that there is a development board with it, but it is much bigger than the board I would like to interface it to...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago in reply to rscasny

     rscasny Thumbsup  The root of my request / recommendation / idea is "Can I use my existing cable?"  Can I use an existing RS-485 run?  I think the answer is "yes".  Can I parallel an existing Cat5 run and make it work?  Maybe?  I understand that this isn't the way it's designed, but can it work?  If the run already exists in the building...  I think of those times that I've pulled wire through the rafters and stuffed it down walls.  Unpleasant memories.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago in reply to rscasny

     rscasny Thumbsup  I've driven many, many miles just to switch two wires and heal a MODBUS network.  Connectors good.  Laughing

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago in reply to kmikemoo

    I had pondered adding a length of base SPE cable. But I see that the sponsor makes cable assemblies up to 20 meters, so I decided not to. But this is why I create this discussion to shake the trees a bit before I finalize the kit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago in reply to JWx

    Yes there are terminal blocks for cable connection. But I really need to have them connected by the connector/jacks, at least in one instance because the sponsor is wanting to see people use their connectors. Ideally, both could be used. I can add the make connectors since I believe I will be getting them directly from the sponsor. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago in reply to jc2048

    I had thought this had the processor onboard:

    ANALOG DEVICES EVAL-ADIN1110EBZ Evaluation Kit, ADIN1110CCPZ, Ethernet Physical Layer Device, Ethernet MAC-PHY, 10BASE-T1L

    And this has a media converter to connect to a PC or Pi:

    ANALOG DEVICES EVAL-ADIN1100EBZ Evaluation Kit, ADIN1100CCPZ, Ethernet Physical Layer Device, 10BASE-T1

    Anyway, let me look at that part a little closer this week. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>