Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum 3 Phase 400 Hz Low Voltage Generator
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 4 subscribers
  • Views 574 views
  • Users 0 members are here
Related

3 Phase 400 Hz Low Voltage Generator

botaman
botaman over 10 years ago

Does anyone have plans for a 3 phase 400 Hz low voltage generator?  It is my intent to design or use an existing design as a test device for certain field equipment. I have researched a bit and discovered several testers that are very expensive. Would like to keep the cost down as my need for this tester is limited to 4 UUT's and outsourcing is expensive as well (though I am forced into that option presently, this is brand new tooling).

Here is what I am planning to develop:

 

Output:

24 to 50 VAC variable @ 1 to 4 Amp maximum, 400 Hertz +/- 1 Hz Sine

 

Voltage source:

115 VAC @ 20 Amp, 60 HZ

 

As you can see, voltage is not my primary concern here, it is a highly stable 400 Hz output that is important. Also need to be able to plug it into the power at my test bench. Portability would be nice as well.

  • Sign in to reply
  • Cancel
  • ajens23
    ajens23 over 10 years ago

    Have you looked at a VFD drive?

    They start around $120 US on e-bay

    Output voltage might need a step-down transformer, but it's close to what you want.

    Al