Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Linearly control output voltage from 80V to 260V AC Single Phase
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 7 subscribers
  • Views 931 views
  • Users 0 members are here
  • frontpage
Related

Linearly control output voltage from 80V to 260V AC Single Phase

nprodigy
nprodigy over 9 years ago

Dear All,

 

Am looking forward in designing a product which can vary output voltage from 80V to 260V AC across load as per desired.

 

For example : Input voltage is 230V AC

 

I need an output of 100V....it should automatically correct to 100V o/p. If desired to be changed to 120V....it should auto correct.

I dont want to use a motorised auto transformer for this purpose as it is bulky and not cost effective.

Do help with ideas.

Regards

Niranjan G.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 9 years ago

    You need to tell us how much current there will be as well as the voltage you want. Is the working frequency 50 - 60Hz or over  a wider range ?

     

    Solid state  AC output converters with variable output voltage and frequency do exist but they are expensive.

     

    How many would you make and what is the application.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 9 years ago

    You need to tell us how much current there will be as well as the voltage you want. Is the working frequency 50 - 60Hz or over  a wider range ?

     

    Solid state  AC output converters with variable output voltage and frequency do exist but they are expensive.

     

    How many would you make and what is the application.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • nprodigy
    nprodigy over 9 years ago in reply to michaelkellett

    Dear MK,

     

    Thanks for your reply. For 240V Current will be approx 52A. Working freq is 50Hz. Application is : I want to change the Kvar of Single Phase Power Capacitor by changing Voltage across the capacitor.

     

    Regards

     

    Niranjan