Forget Me Not Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Forget Me Not Design Challenge
  • More
  • Cancel
Forget Me Not Design Challenge
Blog Episode 4: Forget Me Not: Medication System
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelwylie
  • Date Created: 17 Aug 2014 5:46 AM Date Created
  • Views 2310 views
  • Likes 1 like
  • Comments 11 comments
  • forget_me_not
  • forget-me-not
  • iot_monitor_auto
  • forget-me-not-challenge-2014
Related
Recommended

Episode 4: Forget Me Not: Medication System

michaelwylie
michaelwylie
17 Aug 2014

Previous Posts:

Epidode 1: Forget Me Not: Application

Episode 2: Forget Me Not: The Best Laid Plans ...

Episode 3: Forget Me Not: Setup EnOcean with openHAB

 

I was notified of a possible delay in shipment from Newark, so I have worked on the Medication Reminder System in the mean time. It took a while to work through the examples on https://github.com/openhab/openhab/wiki/Samples-Rules to learn about setting up rules. My rules system can be summarized as follows:

 

1. Initialize System - Set The rocker switch states

 

This part is extremely important. Even though I can load the openHab interface and see the state of the switches are not ON it doesn't mean the states of the switches are OFF. There must be a tri-state option? In demo.rules I have this rule for the system startup.

 

rule "System Start"          //demo.rules
when
    System started
then
    Rocker1B.setState(OFF)
    Rocker1A.setState(OFF)
    medicationTakenFlag = 0          //Flag set when medication taken
end

 

Note: In demo.items, my rocker switches are defined as:

Switch Rocker1A {enocean="{id=00:29:E4:66, eep=F6:02:01, channel=A}"}
Switch Rocker1B {enocean="{id=00:29:E4:66, eep=F6:02:01, channel=B}"}

 

2. Set the medicationTakenFlag when I take the medication

 

If the Rocker Switch is pressed, the medicationTakenFlag gets set.

 

//Set the medication flag when I take my medication
rule "Medication Taken"
when
    Item Rocker1A changed from OFF to ON
then
    medicationTakenFlag = 1
end

 

3. Attempt to leave the home without taking medication

 

I have mounted a magnetic contact switch on my front door and named it EnOcean_sensor_CONTACT2. If I attempt to leave the home without having set the medicationTakenFlag (pressing the rocker switch) my Raspberry Pi will notify me with a voice command "Take Medication". This should only occur after 4 AM, because before that would just be annoying.

 

//Haven't taken medication and leave the apartment
rule "Remind Me While I am Leaving"
when
    Item EnOcean_sensor_CONTACT2 changed from CLOSED to OPEN
then
    var Number hour = now.getHourOfDay
    if ( (Rocker1A.state == OFF) && (hour > 4) )
    {
        //Rocker1B.setState(ON)
        say("Take Medication")
    }   
end

 

4. Reset the rocker switch everyday at 3:59 AM.


This should be one of the easiest settings, but I had to learn how cron works in Linux to setup the check.Have a look here for the details Quartz Scheduler | Documentation | Tutorial Lesson 06. It's still a bit confusing. The code below should turn off the rocker switch and reset the medicationTakenFlag at 3:59:00 AM everyday.

 

//Reset medication flag every night at 03:59
rule "Reset me"
when
    Time cron "0 59 03 * * * "        //03:59:00 AM everyday
then
    sendCommand(Rocker1A, OFF)
    medicationTakenFlag = 0;
end

 

5. The last rule is a little trickier. What if it's the weekend or I have the day off? I still need to be reminded if I didn't take the medication.

 

This last rule reminds me every 15 minutes between 8AM and 11AM if medicationTakenFlag is not set that I should take the medication. I will come up with a better way to do this one eventually because this could get really annoying.

 

rule "Remind Me and I Haven't Left"

when
    Time cron "* */15 * * * ?"
then
    var Number hour = now.getHourOfDay
    if ((hour > 8) && (hour < 11) && (medicationTakenFlag == 0))
        say("Take Medication")
end

 

That's the medication system so far. Next I might try to get Notify My Android to notify our smart devices at home as well as the voice command to take medication.

 

Things I learned this week:

  • Initialize switch states, holy moly this can cause you a lot of grief!
  • The smart phone apps respond a lot quicker than the web interface. I was watching the web interface waiting for a rocker switch state to change but it didn't change until I reloaded the interface. The app responds immediately.
  • If you are working in openHab designer and you want to see the autofill options, ie you type Rocker1A. and you want to see the parameter options, hit ctrl-space.
  • Sign in to reply
  • mcb1
    mcb1 over 12 years ago in reply to fvan

    Thanks for that

    If you have the right bits first it does help.

     

    I also seem to have colour on mine now, not sure why I didn't before.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 12 years ago in reply to mcb1
    The designer version doesn't exactly add a lot

     

    One thing I do find useful in the designer is the auto completion (CTRL + spacebar):

    image

     

    Especially when you don't know which commands are available/usable, this can list them and give more insight.

     

    Frederick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 12 years ago in reply to fvan

    This is a good idea! I was relying on the packaging dates/days to keep track of that but I could definitely use a persistence for it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 12 years ago in reply to mcb1

    I'd use some rules to keep track of a counter then and put it together with the sensors state in a chart.

    That way, you now when and how long there was movement, and also the total number of occurrences.

     

    The rule would be in charge of two things:

    • increment the movement counter when sensor updates from no movement to movement
    • reset the counter at midnight everyday (if reset is needed)

     

    Frederick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to fvan

    Frederick

    My plan was to treat it like a contact, using either the occupancy input on STM330x or simply as a contact like a door switch.

     

    The idea of treating it like a number was to see the occurrences during the day.

    Together with other changes in temperature and light level over the same timescale, you will get picture of what's happening..

     

    Since my parts aren't here yet, I'm going to have to fudge some data in order to be able to work on the presentation.

     

    BTW the Notepad++ with the highlighting helps.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>