Forget Me Not Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Forget Me Not Design Challenge
  • More
  • Cancel
Forget Me Not Design Challenge
Blog Forget me Knot - SPI Woes
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: crosseyejack
  • Date Created: 22 Sep 2014 6:15 PM Date Created
  • Views 1693 views
  • Likes 0 likes
  • Comments 10 comments
  • forget_me_not
  • internet_of_things
  • raspberrypi
Related
Recommended

Forget me Knot - SPI Woes

crosseyejack
crosseyejack
22 Sep 2014

First sorry I've not been about. Work and family commitments have been killing most of my time :-(

 

So what have I been up to? After getting getting the RF Sockets working with OpenHAB I set out getting some wireless transceiver modules working with OpenHAB too. If I wanted an easier time I should of researched it more, but then again I've always like a challenge.

 

The modules I choice were the MRF24J40MA modules from Microchip. They are an SPI driven module and I thought I would easily integrated with the PI. Before I ordered them I did some quick Googling and some some code that got them working so I thought I wouldn't have too many issues. When I came to trying it myself though I just kept banging my head against the wall.

 

My plan is to use these modules to create my own wireless sensors/actuators. I easily got these modules talking to each other using some ATMega's and some Arduino code. But then I tried to port this code to the Pi I just couldn't get the thing to talk correctly. After a week of trying and failing I decided that my SPI skills still need a lot of work.

 

SO instead of scratching my head over this issue (for now) I decided to work around the problem. In the past I have successfully got the Pi to communicate with a microcontroller with both SPI and i2c, so I decided to use an intermediate micro to get the Pi communicating with the wireless module.

 

As the module uses SPI I decided to use i2c to talk to the Pi. So the set-up if currently set up like this:

PI <--i2c--> ATMega <--SPI--> MRF24J40MA.


The ATMega is running some Arduino code based of a modified version of KarlP's library for these modules.
KarlP's original lib

The modified version I an currently using

The Arduino Sketches I'm currently using

 

What I am doing for the MRF24J40_RX_Test code that is being used on the intermediate micro is waiting to receive a valid transmission from the MRF24J40_RTX_Test code, reading out the sender address, RSSI, LQI and the payload data and copying that into a buffer. The micro then sends a pin high which is connected to an interrupt pin on the Pi.

 

The MRF24J40_RTX_Test code reads an analog input from an Analog Devices TMP36 formats that data and broadcasts the data to the module connected to the micro attached to the Pi.

 

A piece of software running on the Pi waits for this interrupt, reads out the data, preforms some sanity checks, processes that data and hands that data off to OpenHAB via its REST API using curl. I have uploaded the software I am writing to do this to GitHub https://github.com/CrosseyeJack/atmega-rpi-openhab-i2cbridge

 

This software is nowhere near complete, but right now it can receive the temp reading and hand that off to OpenHAB. At the moment pretty much everything is hard coded, runs in the foreground and has debug messages all over the place.

 

My current plan of action if to to the following

  • Figure out how I want to transmit the data. The data is currently transmitted as <Pin Type><Pin Number>;<Value>; so for example the transmitter code transmits A0:18.7; using this method I should be able to break down what data is being sent (is the first char a A or a D? what is the number following the first char upto ":"? What is the data between ":" and ";"? Is there any more data being send after the ";" terminator? If so rinse and repeat.
  • Decide on how I want to store OpenHAB item mappings. Do I want to store such mapping in a config file with the application which I believe would be the easier way or should try and read the mappings from the item in OpenHAB? This is something I will have to ponder.
  • Modify the RX code so it has an incoming data buffer which I can write to from the Pi and transmit that buffer to a wireless module.
  • Modify the bridging software running on the Pi to create a named pipe so I can pass it data from OpenHAB or other programs which will be passed onto the micro to be transmitted out.
  • Modify the bridging software so its hard coded, but I need to decide on how I am going to store the mappings first.
  • Turn the bridging software into a daemon application (this is pretty easy to do, the code is already there I just need to trigger it)

Once I have got most of the code running on the intermediate micro I will move it onto the board that is also home to the 433Mhz transmitter used for controlling the RF Sockets. For now I am programming and testing using another Raspberry Pi.

 

With only a month left I think I am going to have to ask the Bosses if I can take a week off.

Not really go much to show you in the way of pictures, but here are breadboards I have using building this crazy concoction with.

image

And here are few screenshots of the bridging software running on the pi printing out its debug messages and the OpenHAB webUI in the background displaying the value.
imageimageimage

As always, feel free to leave any questions in the comments and I will get back to you. Gotta run out for a short while and then track back on with the bridging application.

 

Dan.

  • Sign in to reply
  • ipv1
    ipv1 over 12 years ago in reply to crosseyejack

    As for your idea do you mean using cylon.js on the Raspberry Pi and firmata on the ATMega?

    Well yes. Its a bit convoluted but doable. Will definitely be something to show image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crosseyejack
    crosseyejack over 12 years ago in reply to ipv1

    Well I've not given up completely on getting the Module talking to the Pi directly. But I needed to get some progress done so reverted back to something I know.

     

    As for your idea do you mean using cylon.js on the Raspberry Pi and firmata on the ATMega?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 12 years ago in reply to crosseyejack

    So instead of the UART use the spi protocol directly. Write the sequence in JS and call it in cylon. At the other end wrap the spi driver in a function and let firmata call that... Simple.... I think,.?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crosseyejack
    crosseyejack over 12 years ago in reply to ipv1

    I did give it a think BUT the EnOcean Pi uses the serial port on the GPIO headers so I would of have to add a USB<->Serial converter. The payload size to and from the micro is small enough to use i2c to get the job done.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 12 years ago

    Dunno if this will be useful or not but you can look into firmiata and Cylon.js

     

    Firmata is a lib for controlling ios over serial. You can transmit serial over the module and the have control over the arduino over that... Just a thought.

     

    Cheers

    Ip

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<