Forget Me Not Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Forget Me Not Design Challenge
  • More
  • Cancel
Forget Me Not Design Challenge
Blog IP Post 10: My Story Of Persistence with persistence on OpenHAB. AND a tutorial on Rule and Timers
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ipv1
  • Date Created: 29 Aug 2014 12:37 PM Date Created
  • Views 3440 views
  • Likes 3 likes
  • Comments 20 comments
  • forget_me_not
  • forget_what
  • openhab
  • iot
Related
Recommended

IP Post 10: My Story Of Persistence with persistence on OpenHAB. AND a tutorial on Rule and Timers

ipv1
ipv1
29 Aug 2014

    • Introduction
    • The Problem
    • RRD4J- The setup (illustrated)
    • The Output
    • Combining Plots
    • Doing Calculations
    • One More Thing
    • While on the topic... Timers and Rules
    • EnOcean Modules and Things other than Temperature

Introduction

 

The raspberry pi does not have the conventional x86 architecture for a processor. Instead it has an ARM processor running at 400MHz. Now this means that even though you are running Linux and even though you can compile the same program using GCC on ARM as on a PC, the output of the compiler will be totally different due to the underlying instruction set. This ultimately means that programs such as MySQL may be different on a PC than the RPi in terms of their execution as well. A lot of times the code is also optimized for the platform such as RPi and all this means that MySQL on the PC might not be the same as on the RPi. Java is an exception because it run on top of the JVM BUT resources on the JVM are not same across platform. Like com ports on windows are like com1, com2 etc but in Linux, everything is a file like /dev/usb0 /dev/AMA0 etc.

 

The Problem

I struggled with getting persistence to work on the RPi and it simply did not work. I tried the MySQL approach but OpenHAB just did not post values as expected. I got the following on the console.

 

image

It did work some times but it seemed temperamental and I was not interested in fiddling around more than I already had. All I want is some graphs of temperatures and other things. I might try setting up MySQL elsewhere and then try connecting it from the RPi but I don't need that right now. I already have an MQTT broker, Samba and SSH running so if I can do without MySQL, I would be better off. Additionally, the MySQL database can grow with time which will needs to be maintained. If I plan this to be an independent device, I would much rather have a database else where. MySQL not now...

 

image

 

 

RRD4J- The setup (illustrated)

I opted for RRd4J which is a Round Robin Database for Java. The upside is that it stores everything in a file and with time, it discards intermediate samples so that the database gets compressed. I wont need temperature for every minute from 10 months ago. For that I would have a database elsewhere. The second upside is that OpenHAB uses it to create graphs anyways. There is a downside as well. It cannot be queried like a standard database. But I'm OK with that. I started by downloading the add-on for RRD4J. I then created a persist file that looked like this.

 

image

The strategies are basically names given to cron arguments. The items section tells us what to store and when. Now with time, you can add a lot of things to the database and you can use a wildcard (*) to store everything, but I would rather add individual items. For buttons, I used the 'onChange' strategy so that it gets saved only when there is a click. Honestly, I won't need em but hey, why not. The next is my temperatures. Now people would use onChange here as well but then how would you plot em if the temperature never changed through the night? Instead I choose the everyMinute and onChange strategy. The EnOcean modules by default, will send significant changes after 100 seconds which can be changed by pins or via software. I will get to that in a different blog, but right now the focus is persistence. For RRD4J, you do not need to set permissions, access control etc. At this point we are basically done. The RRD4J is setup and will save data in files as per strategy.

 

The Output

 

Now to display these things. The simplest thing to do would be to plot something. For that, my sitemap and output looks like....

 

imageimage

 

Combining Plots

Here I have plotted the graph individually. I have three temperature sensors so I would rather plot them all together. To do that we need to change the Items file and make the temperatures part of a group. First we define a group and add the temperature variables to that group.

image

Items File

image

Modified Site Map

Next we can simple plot the entire group instead of individual items. Simple.

 

image

 

Doing Calculations

 

Next I would like to measure the average, maximum and minimum temperatures... For that we add another variable to the items. Below the three number items add the following...

Number TempAvg  "Avg Temperature [%.1f °C]" <temperature> (Temperatures)

This is where we can store the average temperature. Next we need to calculate the average temperature. We can simply do that using the in build functions. I found a list at the wiki.

 

https://github.com/openhab/openhab/wiki/Persistence

 

image

I use the following rule

 

rule "Calculate Average I"
when
  Item TemperatureI changed
then
  var temp = TemperatureI.averageSince(now.minusHours(4))
  postUpdate(TempAvgI, temp)
end

 

You can do a multitude of things using persistence and the in built functions. I will be looking at thresholds. My requirement is to use rules in thresholds to generate notifications and alarms. Here is a scenario.

 

One More Thing

 

One last thing about charts is that the ones we have worked out have a fixed duration. The period has be set to 'h'. This can be changed on the fly. What we want is to be able to move between hours, days and weeks for periods. Credit for the code goes to F. Vanderbosch and his post. For this the first thing we need is a set of buttons. Add the line to the sitemap where you want the selection buttons.

 

Switch item=Temperature_Chart_Period label="Chart Period" mappings=[0="Hour", 1="Day", 2="Week"]

 

Here the item Temperature_Chart_Period will have value 0,1 or 2 and will have labels Hours, Day and week. You can change things here as per requirement. Now we do not generate charts on the fly. Actually we will be generating all the desired charts but will be setting the visibility for only the one we want but adding some code to the chart item in the sitemap. Modify the chart items as follows:

 

Frame label="Graphs"{
  Switch item=Temperature_Chart_Period label="Chart Period" mappings=[0="Hour", 1="Day", 2="Week"]
  Chart item=TemperatureI period=h refresh=300  visibility=[Temperature_Chart_Period==0, Temperature_Chart_Period=="Uninitialized"]
  Chart item=TemperatureI period=D refresh=1800 visibility=[Temperature_Chart_Period==1]
  Chart item=TemperatureI period=W refresh=3600 visibility=[Temperature_Chart_Period==2]
  }

 

This should produce a row of buttons with one graph being visible at a time. Be creative!

 

I really recommend visiting the following link. https://code.google.com/p/openhab-samples/wiki/Tricks

 

While on the topic... Timers and Rules

 

While we are on the subject I wanted to show some basic examples on making time based rules.

Example 1. When you want to start a timer on an event and stop on a different event AND snooze on another.

I have in my project a contact switch which is part of the waiting platform which is used as a placeholder for hot food. We expect the food to cool down in say 20 minutes. After 20 minutes, an alarm should sound. If we want to snooze the notification, we should click a rocker switch and that should extend the timer for say 5 minutes and so on. The alarm should also keep ringing till the platform is emptied. Here we go.

 

var Timer waitTimer=null
var boolean alarmState=false

rule "Waiting Begins"
when
     Item Contact1 changed
then
     if(Contact1.state==CLOSED) {
         waitTimer=createTimer(now.plusMinutes(20))[
               alarmState=true //Set the variable once Time is over
          ]
     } else { // if we have lifted the utensil
           if(waitTimer!=null){
                waitTimer.cancel
                waitTimer=null
                alarmState=false
          }
     }
end

 

Now For the alarm rule

 

rule "Alarm State every minute"
when
     Time cron "0 0 * * * ?"
then
     if(alarmState==true) {
          playSound(doorbell.mp3)
     }
end

 

And lastly, we need to snooze

 

rule "Snooze Waiting"
when
     Item Rocker1BO changed from OFF to ON
then
     if(Contact1.state==CLOSED){
          waitTimer=createTimer(now.plusMinutes(5))[
               alarmState=true
          ]
     }

 

I took pointers from this link https://code.google.com/p/openhab-samples/wiki/Rules

 

EnOcean Modules and Things other than Temperature

 

I initially intended to use the EnOcean Temperature sensor to send temperature as well as another analog value to the EnOcean Pi. I am able to do so, but it seems that the OpenHAB Binding does not support anything other than the TEMPERATURE parameter at this point. I would like to make changes to the bindings themselves but I do not thing it will be a good exercise at this point. If anyone can help please send me a message.

 

 

There is a problem with the network so I will continue this a bit later.

TO BE CONTINUTED HERE

  • Sign in to reply

Top Comments

  • hlipka
    hlipka over 12 years ago +1
    I had the same problems with the mySQL storage. In the end, it looked like multiple issues. There was a small error in my items configuration (a missing " in one place where openHAB did not complain about…
  • ipv1
    ipv1 over 12 years ago in reply to mcb1 +1
    In the items section, I would just add the individual item names separated by commas. then the colon and the rest: Items { temperature1, temperature3: strategy = everyChange, restoreOnStartup Works for…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to ipv1 +1
    Thanks for your responses! I am actually an OpenHab beginner, and I want to use google chart but I dont know where to update in the openHab code: *where to put my front end as a google chart *where to…
  • ipv1
    ipv1 over 12 years ago in reply to hlipka

    To store dates, in the openhab.cfg file add this line to the mysql configuration section

     

    mysql:sqltype.datetime=DATETIME

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to hlipka

     

    The reason is that OpenHAB cannot store Date values in MySQL properly

     

    I figured it was to do with the formatting, and since it wasn't obvious ..... elected to change and move on.

    I haven't tried using any of the ntp styles ie { ntp="Europe/Berlin:de_DE" }


    but specify what values should be persisted.

    I was rather hoping there was an example to exclude Date ... to save on having to specify everything.

    I'm still sorting out my groups and layouts and having another variance in the equation is not helpful at this stage ... again change and move on.

     

    I have however learned that you do need to restart OpenHAB if you do make a change .... thanks fvan

     

     

    Inderpreet

    I'm not in a position to say one way or the other.

    My concept was to move the data out at set times, to a remote location.

    A database of some flavour seems a logical way to achieve that. .... but I'm open to ideas.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hlipka
    hlipka over 12 years ago

    The reason for that error is not directly having both NTP and MySQL (I run that setup just fine). The reason is that OpenHAB cannot store Date values in MySQL properly. I darkly remember that there might be some workaround, but I don't remember it. So just don't use '*' for your persistence rules, but specify what values should be persisted.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 12 years ago in reply to mcb1

    I never thought of that. I'm running the ntp as well.

     

    The whole SQL thing is overrated. Rrd4j is working nicely. If I really need to retain some data for use in another app I might get mysql on a separate PC or just another RPi

     

    Thank you for the info.

    Ip

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to fvan

    fvan

     

    Guys I had issues as soon as I got my ntp working (I hadn't shifted the ntp.jar file).

    SQL throws this error

    image

     

    So I've stopped the SQL for the meantime.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>