Forget Me Not Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Forget Me Not Design Challenge
  • More
  • Cancel
Forget Me Not Design Challenge
Blog Pas Home / Home ventilation with RPiSoC
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: verrverr
  • Date Created: 1 Sep 2014 12:38 AM Date Created
  • Views 1794 views
  • Likes 0 likes
  • Comments 7 comments
  • forget_me_not
  • pas_home
Related
Recommended

Pas Home / Home ventilation with RPiSoC

verrverr
verrverr
1 Sep 2014

Pas Home - Index

 

I will use the RPiSoC to control and catch the status of my home ventilation system. Integrate with OpenHAB and my humidity sensor, when i take my shower humidity sensor detect the humidity increase and automatically start the ventilation. I suck in electronics I'm going to need your help.


The plan


image


The timer

I open the current control and check component.

Its seems simple enough:

      4 wire 12v, GND, LED Control, SW (Switch),

     LM2901DG Chip (From spec 'Designed for use in level detection')

     3 LED

     Push button

     100uf 63v 85°C (Capacitor)


imageimageimageimage

The signal

With the Tektronix oscilloscope i check what happen in SW and LED wire.


SW wire, have continuous 5v DC and when i press control button its drope near 0v and when i release it return to 5v. When signal is reduce to 0v for about 1 second or more the main control unit detect it and start ventilation and switch between each timer state.

What is the name of this transition? Do you know some tutorial links to reproduce this with RPiSoC ?


imageimage


The LED wire have his voltage between 0v to 10v. Each value indicate a state. Measure voltage between 0v to 5v with RPiSoC its seem very easy with analog port and this sample code https://github.com/EmbeditElectronics/psoc_2_pi/blob/master/API_Python_v_1_1/SAR_ADC_voltmeter.py

But how measure voltage with range 0v-10v? Use a Voltage Dividers? Do you know a good tutorial?


image




  • Sign in to reply

Top Comments

  • kipe
    kipe over 11 years ago in reply to verrverr +1
    Hey. Try with larger resistors, so the affect on the existing circuit won't be that much. Something like 1M and 470k might work...
Parents
  • hlipka
    hlipka over 12 years ago

    What you measure for the switch looks like a normal input with a pull-up resistors. You should be able to control that with a transistor (or a small relay if you want to have isolation).

    Are the switches on the panel mechanical?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • hlipka
    hlipka over 12 years ago

    What you measure for the switch looks like a normal input with a pull-up resistors. You should be able to control that with a transistor (or a small relay if you want to have isolation).

    Are the switches on the panel mechanical?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • verrverr
    verrverr over 12 years ago in reply to hlipka

    Hi thank for your help, for the pull-up resistor if I understand if a use a relay I just need to link the gnd and switch wire using the relay for a small duration?

    The current push button on the switch have a 100uf capacitor on the vcc side, do I also have to use one?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hlipka
    hlipka over 12 years ago in reply to verrverr

    Yes. No. A relay can alway replace a button, just connect it in parallel. And if there is already a cap (though I'm not sure what its used for), you should not add another one.