Get Closer Wearables Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Get Closer Wearables Design Challenge
  • More
  • Cancel
Get Closer Wearables Design Challenge
Blog Playing with Neopixel Rings
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: faithkill
  • Date Created: 23 Sep 2013 11:53 PM Date Created
  • Views 1148 views
  • Likes 0 likes
  • Comments 2 comments
  • flora
  • get_closer_challenge
  • Wearables
  • wearable_tech
  • adafruit
  • get_closer
Related
Recommended

Playing with Neopixel Rings

faithkill
faithkill
23 Sep 2013

September has been crazy busy.  I can remember the last few days of August just as I was gatting into full swing with Wearables challenge and then Whoosh or something like that,  its nearly the end of September and the challenge part of the Wearables challenge will be coming to an end soon.

I decided that after coming up with the initial design I would do some work with each of the components I would be using.

First up was the Neopixels.  Initially had a bit of a problem as I rushed through reading the Adafuit instructions and rather than downloading the correct Example file for the Neopixel I tried running the Florapixel example, which unsurprisingly didn’t work.

Once I had corrected that and ran the correct example they worked great.


Looking at the Neopixels made me realise something. As  I wanted to use a lot of pixels sewing a lot of individual pixels would be a real pain, and could potentially lead to a lot more failures on the garment.  I realised the  the solution to this was to  use the Adafruit Neopixel ring. 

Here is a video of my first test of the NeoPixel rings  http://www.youtube.com/watch?v=WGIzBeo4AQs 


I love the weird glow effect that my rubbish phone camera has produced.  The Neopixel Rings are really bright.  I found that the standard battery pack would only power around five  of the Neopixel rings.  I really want to use  seven  so have decided to buy a Lithium Polymer battery and charger and test that with the Flora and Neopixels.  It may be the case that I have to write my code so that it limits to just a few of the Neopixel rings but will see how it goes.

I'm going to post my experiences with the other Flora components I'm using soon along with a much needed update on the actual project (Hint: it involves a lot of sewing copper briaid)

  • Sign in to reply
  • vsluiter
    vsluiter over 13 years ago

    Hello Catherine,

     

    You might also decrease the brightness of the LEDs (half the r,g,b values), that will save your eyes and make the standard battery operate with more pixels. It's a software solution, and maybe not the best, but it might help you speed forward while waiting for the battery!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • zengirl2
    zengirl2 over 13 years ago

    Catherine, I think the neopixel rings are just amazing and I so want to make an IronWoman t-shirt with one.  I was busting out laughing when you made the comment about your phone and the way the pixels look -- I have the same trouble when I do my little videos.  I was telling someone recently that if you want bling, you absolutely need neopixels because they will blow your eyes out.  Anyway, hopefully your project will end up being the next art gallery craze and maybe even something for Lady Gaga.  Copper braid sounds like a great feature --both practical and interesting looking.