Hats Off Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Hats Off Design Challenge
  • More
  • Cancel
Hats Off Design Challenge
Blog Hats Off Fascinator 17: The Code
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: brenyc13
  • Date Created: 29 Oct 2014 1:39 PM Date Created
  • Views 981 views
  • Likes 0 likes
  • Comments 1 comment
  • jaunty_fascinator
  • hats_off
  • accelerometer
  • code
  • gemma
  • adafruit
Related
Recommended

Hats Off Fascinator 17: The Code

brenyc13
brenyc13
29 Oct 2014

image

I was so excited to share my final result that I very nearly forgot to post the code. Here it is below. I have to admit that significant portions of it were dictated or outright created by my Hunky Assistant. But the challenge did prompt me to do a couple of smaller projects better suited to a programming novice. Anyway, take a look! Let me know if there's a better way to do what we did...


#include <TinyWireM.h> //software I2C library, lets you talk to any I2C device
#include <Adafruit_NeoPixel.h>
#include <util/delay.h>


#define NEOPIXEL_PIN 1


// this is the "callsign" of the accelerometer.
// When it hears this, it knows the Gemma is talking to him
#define ACCEL_ADDR (0x32 >> 1)


// this is the address for the output of one byte for the X low order bits.
// The y and z registers immediately follow this so we can just have the
// computer call this one and the 5 that follow
#define OUT_X_L_A 0x28


#define CTRL_REG1_A 0x20


#define NUM_PIXELS 4


Adafruit_NeoPixel strip = Adafruit_NeoPixel(NUM_PIXELS, NEOPIXEL_PIN, NEO_GRB + NEO_KHZ800);


const uint8_t stages[][3] = {
  { 0, 0, 0 },
  { 0, 0, 60 },
  { 0, 60, 0 },
  { 127, 0, 0 },
  { 255, 0, 255 },
  { 0, 255, 255 },
  { 255, 255, 0 },
  { 255, 255, 255 },
};


const size_t num_stages = sizeof(stages)/sizeof(stages[0]);


void init_accelerometer()
{
  TinyWireM.beginTransmission(ACCEL_ADDR); // start sending a message to this address: ACCEL_ADDR
  TinyWireM.send(CTRL_REG1_A); // send this byte as part of the message: CTR:L_REG1_A
  TinyWireM.send(0x37); // send this other byte as part of the message: 0x37
  TinyWireM.endTransmission(); // finish sending the message

  //the sum of these functions sets the mode of the accelerometer
}


void setup()
{
  TinyWireM.begin(); // this initializes the ability to talk over I2C

  init_accelerometer(); // this initializes the ability to talk with the accelerometer

  strip.begin(); //this initializes the "strip" aka the NeoPixels
  strip.show(); //initializes all pixels off
}


int16_t recv_2bytes()
{
  uint16_t v;

  uint8_t l = TinyWireM.receive();
  uint8_t h = TinyWireM.receive();

  v = h;
  v <<= 8;
  v |= l;


  return v;
  //this part gets the values of x y z and reassembles the two bytes of each into one number
}


void get_accelerometer_values(int16_t *x, int16_t *y, int16_t *z) // asterisks mean to get the address, not value
{
  TinyWireM.beginTransmission(ACCEL_ADDR); // begin transmission to a device that has this address
  TinyWireM.send(OUT_X_L_A | 0x80); // part of the transmission is this
  TinyWireM.endTransmission(); // finish transmission

  TinyWireM.requestFrom(ACCEL_ADDR, 6); // start getting information from the accelerometer

  *x = recv_2bytes();
  *y = recv_2bytes();
  *z = recv_2bytes();
}


#define iter1(N) \
    tr = root + (1 << (N)); \
    if (n >= tr << (N))   \
    {   n -= tr << (N);   \
        root |= 2 << (N); \
    }


uint32_t sqrti(uint32_t n)
{
    uint32_t root = 0, tr;
  
    int N;
    for (N=15; N>=0; N--) {
      tr = root + (1 << (N));
      if (n >= tr << (N)) {
        n -= tr << (N);
        root |= 2 << (N);
      }
    }
  
    return root >> 1;
}


uint16_t get_accelerometer_vector_length()
{
  int16_t x,y,z; // make a space for an integer of 16 bits, a space each for x,y,z
  int32_t t;
  int32_t v;

  get_accelerometer_values(&x, &y, &z);
  //this is a little complicated. "&" has a very specific meaning
  //Give me the addresses of where "x" "y" "z" live in memory

  v = 0.0;
  t = x;
  t *= t; // t=t*t
  v += t; // v=v+t
  t = y;
  t *= t;
  v += t;
  t = z;
  t *= t;
  v += t;
  v = sqrti(v);

  // here we're taking the values of x y z and squaring them and adding that and then getting the square root of the whole

  v -= 16384.0;
  if (v < 0) {
    v = -v; // inverting the number. taking a negative and making it positive -- getting the absolute value
  }

  return v; // return is a very special keyword in C
  //it is a statement, not a variable declaration
  //it means "stop executing this function and return a value"
}


void out_value(uint8_t v)
{
  uint8_t i;

  for (i = 0; i < 8; i++) {
    digitalWrite(1, LOW);
    delay(1);
    digitalWrite(1, HIGH);
    delay(1);
    digitalWrite(1, LOW);
    delay(1);
  
    digitalWrite(1, (v>>(7-i))&1);
    delay(4);
  }
  digitalWrite(1, LOW);
  delay(100);
}


void interpolate_detailed(int frame, const uint8_t *initial, const uint8_t *next, uint8_t *vals)
{
  int i;

  for (i = 0; i < 3; i++) {
    int16_t attrib_prev_val;
    int16_t attrib_next_val;

    attrib_prev_val = initial[i];
    attrib_next_val = next[i];
    int32_t tmp = (attrib_next_val - attrib_prev_val);
    tmp = tmp * frame / 255;
    vals[i] = attrib_prev_val + tmp;
  }
}


void apply_fade(uint16_t current_fade_frame, uint16_t total_fade_frames, uint8_t *values)
{
  int i;
  for (i=0; i<3; i++) {
    uint32_t tmp = (total_fade_frames - current_fade_frame);
    tmp *=values[i];
    tmp /=total_fade_frames;
    values[i] = tmp;
  }
}


#define ACC_THRESHOLD 1000


enum {
  STATE_ZERO,
  STATE_INCREASING,
  STATE_WAITING,
  STATE_DECREASING,
} mstate = STATE_ZERO;


/* Shared */
uint8_t current_values[3] = {0, 0, 0};
int current_stage = 0;


/* Increasing */
//uint8_t goal[3];
int goal_stage;
int current_frame;


/* Waiting */
int iterations_left;


/* Decreasing */
// use current_frame too
uint16_t fade_frames;
uint16_t current_fade_frame;


void loop()
{
  int16_t acc_sample;
  acc_sample = get_accelerometer_vector_length(); // first, call the function get_accelerometer_vector_length and put its value in a
  int i;
  int delay_val = 0;


  if (mstate == STATE_ZERO) {
    current_stage = 0;
    delay_val = 10;
  
    if (acc_sample > ACC_THRESHOLD) {
      /* Transition to increasing */
      goal_stage = current_stage + 1;
      current_frame = 0;
      delay_val = 0;
      mstate = STATE_INCREASING;
    }
  } else if (mstate == STATE_INCREASING) {
    interpolate_detailed(current_frame, stages[goal_stage-1], stages[goal_stage], current_values);
  
    if (current_frame == 255) {
      /* Transition to waiting */
      iterations_left = 100;
      current_stage++;
      mstate = STATE_WAITING;
    }
  
    current_frame++;
    delay_val = 10;
  } else if (mstate == STATE_WAITING) {
    iterations_left--;
  
    if (acc_sample > ACC_THRESHOLD && current_stage < num_stages - 1) {
      /* Transition to increasing */
      goal_stage = current_stage + 1;
      current_frame = 0;
      delay_val = 0;
      mstate = STATE_INCREASING;
    }
  
    delay_val = 10;
  
    if (iterations_left == 0) {
      /* Transition to decreasing */
      current_frame = 0;
      current_fade_frame = 0;
      fade_frames = current_stage * 256;
      mstate = STATE_DECREASING;
    }
  } else if (mstate == STATE_DECREASING) {
    const uint8_t black[3] = { 0, 0, 0};
    interpolate_detailed(current_frame, stages[current_stage], stages[current_stage-1], current_values);
    apply_fade(current_fade_frame, fade_frames, current_values);
  
    current_frame++;
    delay_val = 10;
    current_fade_frame++;
  
    if (current_frame == 255) {
      current_stage--;
      if (current_stage == 0) {
        /* Transition to zero */
        mstate = STATE_ZERO;
      } else {
        current_frame = 0;
      }
    }
  }


  for (i=0; i<NUM_PIXELS; i++) {
    strip.setPixelColor(
      i,
      current_values[0],
      current_values[1],
      current_values[2]);
  }

  strip.show();

  delay(delay_val);


}


  • Sign in to reply
  • DAB
    DAB over 11 years ago

    Good job Barbara.

     

    DAB