In Reach! – Ultrasonic Sensor Sensing Challenge
  • Challenges & Projects
  • Design Challenges
  • In Reach! – Ultrasonic Sensor Sensing Challenge
  • More
  • Cancel
In Reach! – Ultrasonic Sensor Sensing Challenge
Forum SwishMaster - #3 - Experimenting with the USSM
  • News
  • Forum
  • Projects
  • DC
  • Files
  • Members
  • More
  • Cancel
  • New
Join In Reach! – Ultrasonic Sensor Sensing Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 42 subscribers
  • Views 433 views
  • Users 0 members are here
  • ultrasonic sensor
  • design challenge
  • SwishMaster
  • tdk
  • TDK waterproof sensors
  • Ultrasonic Sensor Sensing Challenge
  • In Reach
  • TDK USSM Plus-FM
  • TDK USSM1.0 PLUS-FS
Related

SwishMaster - #3 - Experimenting with the USSM

amgalbu
amgalbu over 1 year ago

In this post, I will talk about my experiments with the TDK USSM that are aimed at checking out how precisely and how far the ball position can be detected

Setup

To conduct the experiments, a reference line approximately 3 meters in length was drawn, with markings at 20-centimeter intervals. It is assumed that the sensor exhibits isotropic behavior, i.e., identical performance in all directions. However, to ensure consistency across trials, a reference mark was applied to the sensor to maintain the same orientation. The basketball was suspended from the ceiling, positioned directly above the center of the marked grid. The testbed is shown in picture below

image

I moved the USSM over the different positions on the grid. For each position, I took a screenshot of the envelop and took note of the detected distance. The test procedure is shown in the following flowchart

image

Results

Here is the result of the experiments

image

And here is the same diagram with the distances measured by the USSM

image

The area where the basketball is detected has approximately this shape

image

The sensors has a "field of view" of about 25 degrees on each side

image

So I think the optimal angle between the sensors is about 50 degrees

image

Given the shape of the covered area, I can also correct the distance measurement to take into account the horizontal offset of the ball. The algorithm I have in mind is quite simple (it applies to the two USSMs). 

  1. When all the samples have been collected, I calculate the average height of the basketball
  2. Given the average height, I can estimate the width of the covered area at that specific distance. I can simply store the width of the covered area at different heights, and interpolate to get an approximation of the area width
  3. The horizontal distance between samples (I will call it "step") can be calculated as the width of the covered area divided by the number of samples
  4. An horizontal position can now be assigned to each sample

Samples taken by the left USSM, will have negative values for the horizontal position

  1. 1st sample will have an horizontal position equal to  - step * (num samples - 1)
  2. 2nd sample will have an horizontal position equal to  - step * (num samples - 2)
  3. ...
  4. last sample will have an horizontal position equal to 0

Samples taken by the right USSM, will have positive values for the horizontal position

  1. 1st sample will have an horizontal position equal to 0
  2. 2nd sample will have an horizontal position equal to  + step * 1
  3. ...
  4. last sample will have an horizontal position equal to + step * (num samples - 1)

Now, with a known horizontal position, I can correct the measured distance using the Pitagora theorem

image

Next steps

With less than a month left and so much work to do, it's time to start writing code and see if I can interface with the USSM. Stay tuned!  

  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB over 1 year ago

    Nice post.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • amgalbu
    amgalbu over 1 year ago in reply to DAB

    Thanks DAB !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • amgalbu
    amgalbu over 1 year ago in reply to DAB

    Thanks DAB !