In Reach! – Ultrasonic Sensor Sensing Challenge
  • Challenges & Projects
  • Design Challenges
  • In Reach! – Ultrasonic Sensor Sensing Challenge
  • More
  • Cancel
In Reach! – Ultrasonic Sensor Sensing Challenge
Forum SwishMaster - #6 - Hardware assembly
  • News
  • Forum
  • Projects
  • DC
  • Files
  • Members
  • More
  • Cancel
  • New
Join In Reach! – Ultrasonic Sensor Sensing Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 42 subscribers
  • Views 331 views
  • Users 0 members are here
  • ultrasonic sensor
  • design challenge
  • SwishMaster
  • tdk
  • TDK waterproof sensors
  • In Reach!
  • Ultrasonic Sensor Sensing Challenge
  • In Reach
  • TDK USSM Plus-FM
  • TDK USSM1.0 PLUS-FS
  • TDK USSM Demo Kit
Related

SwishMaster - #6 - Hardware assembly

amgalbu
amgalbu over 1 year ago

In this post, I am going to share my progress on building the container and assembling the electronic components of the SwishMaster device

The case

The SwishMaster case is made up of three main parts

1. The main case

The main case has slots for all the electronics components, namely

  1. 2 USSMs
  2. The Arduino Nano 33 IoT board
  3. The stepup converter
  4. The level shifter

Each component will be housed in the position shown in the following picture

image

Note that the holes for the USSMs are 50 degrees apart, to match my findings on the area covered by the USSMs themselves (see my post here)

2. The cover

The cover is quite simple. It stays in place thanks to a bevel and is secured to the case with two screws

image

3. The base

The base has two brackets to hold the power bank and features a bolt to fix the SwishMaster to a camera tripod

image

Installation

The following pictures show the installation process of the electronic components that make up the SwishMaster

1. USSMs

image  image

2. LCD display

image  image

3. Electronic boards

All the boards are kept in place by the bevels (the boards fits exactly in the slots). For a better hold, I added some double-sided tape.

I also created a piggy-back for the Arduino board to simplify the soldering of the connections.

image  image

image

The final result

And, finally, here are some pictures of the first (almost) completed SwishMaster prototype

image  image

Next steps

Hardware assembly is 90% completed: some finishing are missing here and there. Firmware has been partially debugged: LCD display works as expected and trajectory calculation algorithm has been tested with simulated data. Now it's time to mount the device on a camera tripod and make some tests on field

  • Sign in to reply
  • Cancel
  • DAB
    DAB over 1 year ago

    Nice update.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • amgalbu
    amgalbu over 1 year ago in reply to DAB

    thanks DAB