In Reach! – Ultrasonic Sensor Sensing Challenge
  • Challenges & Projects
  • Design Challenges
  • In Reach! – Ultrasonic Sensor Sensing Challenge
  • More
  • Cancel
In Reach! – Ultrasonic Sensor Sensing Challenge
Forum Measuring Water Level (EchoFill #3)
  • News
  • Forum
  • Projects
  • DC
  • Files
  • Members
  • More
  • Cancel
  • New
Join In Reach! – Ultrasonic Sensor Sensing Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 42 subscribers
  • Views 794 views
  • Users 0 members are here
  • TDK waterproof sensors
  • In Reach!
  • Ultrasonic Sensor Sensing Challenge
  • TDK USSM1.0 PLUS-FS
  • TDK USSM Demo Kit
Related

Measuring Water Level (EchoFill #3)

taifur
taifur over 1 year ago

One of the main goals of my project is to measure the water level using the ultrasonic sensor. So, I was trying to measure the water level using the TDK Demo Kit. I used a 25-liter water jar and positioned the sensor unit at the top opening of the jar. After launching the demo kit software, I activated the sensor’s zero calibration. With this setup, the sensor measured a distance of 235 cm. I was a bit confused about the reading because the actual height of an empty jar should be more. 

image

I filled one-third of the jar and measured the distance again. Surprisingly, I got the same reading from the sensor, which is shown in the following image. 

image

I filled the jar to about half and still read the same value. I became very disappointed. 

image

I continued the experiment and filled the jar to about two-thirds of its capacity, but the measured value remained unchanged. 

image

I was quite disappointed with the reading, yet at the same time, curious to understand the reason behind it. I suspected that the narrow neck of the jar might be causing the inaccurate measurement. To eliminate this issue, I decided to use a water bucket instead of the jar. The bucket has a wide opening, which should prevent any obstruction or disturbance to the sensor readings. I made the following setup to measure the water level of the bucket using the sensor kit. 

image

With a portion filled, I was getting the following result (not 235cm at this time!). The reading was around 165cm. 

image

I added more water to the bucket until it was nearly full, and the sensor reading changed as expected. This confirmed that the previous error was for the narrow neck of the jar. 

image

Since I plan to measure the water level in a large tank that doesn’t have a narrow opening, the sensor is unlikely to face any difficulties or produce errors in level detection. I got a very accurate level in the case of the water bucket. 

  • Sign in to reply
  • Cancel

Top Replies

  • taifur
    taifur over 1 year ago in reply to beacon_dave +1
    I tried with less than 235mm, but I am still getting the same reading.
Parents
  • kmikemoo
    kmikemoo over 1 year ago

    taifur The narrow neck sounds very reasonable.  You may want to try a lid with a small hole on your red bucket to see if that influences the reading.  The open top doesn't reflect any return signal... but the lid might.  Just a thought.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • taifur
    taifur over 1 year ago in reply to kmikemoo

    Good idea, but as I am going to place it in a water tank that has no narrow neck, I don't like to spend more time on it. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • taifur
    taifur over 1 year ago in reply to kmikemoo

    Good idea, but as I am going to place it in a water tank that has no narrow neck, I don't like to spend more time on it.