In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog [AirCare] InTheAir - Week 5: openHAB and MQTT
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
  • Author Author: fvan
  • Date Created: 26 Nov 2014 1:55 PM Date Created
  • Views 1781 views
  • Likes 2 likes
  • Comments 4 comments
  • eclipse_iot
  • mqtt
  • openhab
  • beaglebone_black
  • internet_of_things
  • in_the_air
  • texas_instruments
  • iot_sensor_nodes
  • cc3200
  • launchpad
Related
Recommended

[AirCare] InTheAir - Week 5: openHAB and MQTT

fvan
fvan
26 Nov 2014

Previous posts for this project:

  • [AirCare] InTheAir - Project Description
  • [AirCare] InTheAir - Week 1: Getting a Launchpad to Blink
  • [AirCare] InTheAir - Week 2: Preparing the Beaglebone Black
  • [AirCare] InTheAir - Week 3: Fuel Tank Testing
  • [AirCare] InTheAir - Week 4: Using the CC3200

 

  • Introduction
  • Preparation
  • Java
  • openHAB
  • MQTT

 

Introduction

 

Other competitors in this challenge have already described how they installed openHAB. I did notice however that they used different methods to go the job done.

 

In this post, I describe the method that I've used to deploy the latest version of openHAB (v1.6.0) and how I created a basic configuration to receive MQTT messages.

By the end of the post, I have openHAB subscribing to a broker, receiving MQTT messages sent by the CC3200 containing some statistics on the FuelTank's battery.

 

Preparation

 

First, I updated my system and ensured the "unzip" tool was installed, as I'll be requiring it to install openHAB.

 

debian@beaglebone:~$ sudo apt-get update
debian@beaglebone:~$ sudo apt-get upgrade

 

debian@beaglebone:~$ sudo apt-get install unzip

 

I also configured the proper timezone.

 

debian@beaglebone:~$ sudo dpkg-reconfigure tzdata

Current default time zone: 'Europe/Brussels'
Local time is now:      Wed Nov 26 12:23:46 CET 2014.
Universal Time is now:  Wed Nov 26 11:23:46 UTC 2014.

 

Java

 

To install Java on the BBB, I followed the steps defined by nikil511 in the following post: [Air ex Machina] #04 Beaglebone for dummies - JAVA,OpenHab


I did add "sudo" here and there, as I was running the commands as user "debian" and not "root".


debian@beaglebone:~$ echo "deb http://ppa.launchpad.net/webupd8team/java/ubuntu precise main" | sudo tee /etc/apt/sources.list.d/webupd8team-java.list
debian@beaglebone:~$ echo "deb-src http://ppa.launchpad.net/webupd8team/java/ubuntu precise main" | sudo tee -a /etc/apt/sources.list.d/webupd8team-java.list
debian@beaglebone:~$ sudo apt-key adv --keyserver keyserver.ubuntu.com --recv-keys EEA14886
debian@beaglebone:~$ sudo apt-get update
debian@beaglebone:~$ sudo apt-get install oracle-java8-installer

 

Easy enough, and Java was installed!

 

openHAB

 

I installed openHAB a bit more manually than the other competitors here, but it works just as well.

 

First thing I did, was to download the openHAB runtime and addons for version 1.6.0 directly on the Beaglebone Black.

 

debian@beaglebone:~$ wget https://github.com/openhab/openhab/releases/download/v1.6.0/distribution-1.6.0-runtime.zip
debian@beaglebone:~$ wget https://github.com/openhab/openhab/releases/download/v1.6.0/distribution-1.6.0-addons.zip

 

Next, I prepared the location I would deploy the application to.

 

debian@beaglebone:~$ sudo mkdir /opt/openhab
debian@beaglebone:~$ cd /opt/openhab/ 
debian@beaglebone:/opt/openhab$ sudo unzip /home/debian/distribution-1.6.0-runtime.zip

 

Then, I deployed the addons (bindings, actions, persistence, ...), but I did it in a subfolder called "unused".

That way, openHAB will not load all the addons, but I can easily deploy/activate them by moving the files from the "unused" folder back to the "addons" folder.

 

debian@beaglebone:/opt/openhab$ cd addons/
debian@beaglebone:/opt/openhab/addons$ sudo mkdir unused
debian@beaglebone:/opt/openhab/addons$ cd unused/
debian@beaglebone:/opt/openhab/addons/unused$ sudo unzip /home/debian/distribution-1.6.0-addons.zip

 

openHAB requires a configuration file to be able to work properly, so I created one, based on the default.

 

debian@beaglebone:/opt/openhab/addons/unused$ cd ../../configurations/
debian@beaglebone:/opt/openhab/configurations$ sudo cp openhab_default.cfg openhab.cfg

 

I also created some placeholders for my items, sitemap and rules.

 

debian@beaglebone:/opt/openhab/configurations$ sudo touch items/intheair.items
debian@beaglebone:/opt/openhab/configurations$ sudo touch sitemaps/intheair.sitemap
debian@beaglebone:/opt/openhab/configurations$ sudo touch rules/intheair.rules

 

Finally, I made the startup script executable, edited the HTTP port in it to use port "9090" instead of the default "8080".

 

debian@beaglebone:/opt/openhab$ sudo nano start.sh


...
# set ports for HTTP(S) server
HTTP_PORT=9090
...

 

debian@beaglebone:/opt/openhab$ sudo chmod +x start.sh
debian@beaglebone:/opt/openhab$ sudo ./start.sh

 

openHAB was installed successfully!

 

MQTT

 

Last week, I already explained how I got the CC3200 to publish data to a broker. The next step, was to have openHAB subscribe to that same data and visualise it.

 

Using MQTT with openHAB is made easy by means of a ready-to-use MQTT binding.

 

The first step, is to prepare the MQTT binding addon and define the broker to be used.

To activate the addon, I moved it from the "unused" folder created earlier, to the "addons" folder so that openHAB would be able to use it.

 

debian@beaglebone:/opt/openhab/addons$ sudo mv unused/org.openhab.binding.mqtt-1.6.0.jar .

 

Because I also intend to use persistence, I deployed the required addon for that as well.

I've used MySQL persistence before and thought I'd use RRD4J this time around.

 

debian@beaglebone:/opt/openhab/addons$ sudo mv unused/org.openhab.persistence.rrd4j-1.6.0.jar .

 

Next, I specified the broker information in the general openHAB configuration file "openhab.cfg".

There is a MQTT binding section in the file, which I edited as follows:

 

################################# MQTT Transport ######################################
#
# Define your MQTT broker connections here for use in the MQTT Binding or MQTT
# Persistence bundles. Replace <broker> with a id you choose.
#

# URL to the MQTT broker, e.g. tcp://localhost:1883 or ssl://localhost:8883
mqtt:eclipseIot.url=tcp://iot.eclipse.org:1883

# Optional. Client id (max 23 chars) to use when connecting to the broker.
# If not provided a default one is generated.
mqtt:eclipseIot.clientId=bbb-openhab-fvan

# Optional. User id to authenticate with the broker.
# mqtt:<broker>.user=<user>

# Optional. Password to authenticate with the broker.
#mqtt:<broker>.pwd=<password>

# Optional. Set the quality of service level for sending messages to this broker.
# Possible values are 0 (Deliver at most once),1 (Deliver at least once) or 2
# (Deliver exactly once). Defaults to 0.
#mqtt:<broker>.qos=<qos>

# Optional. True or false. Defines if the broker should retain the messages sent to
# it. Defaults to false.
#mqtt:<broker>.retain=<retain>

# Optional. True or false. Defines if messages are published asynchronously or
# synchronously. Defaults to true.
#mqtt:<broker>.async=<async>

# Optional. Defines the last will and testament that is sent when this client goes offline
# Format: topic:message:qos:retained <br/>
#mqtt:<broker>.lwt=<last will definition>

 

For the parameters you intend to use, it is important to uncomment them and to replace "<broker>" by an alias you can refer to in the items configuration. In this case, I used "eclipseIot" as an alias for testing.<broker>

Then, I started defining my items in the "intheair.items" file.

 

Group All

Number FT_Voltage_Period "Chart Period"
Number FT_TimeToEmpty_Period "Chart Period"
Number FT_StateOfCharge_Period "Chart Period"

Number FT_Voltage "Voltage [%d mV]" (All) {mqtt="<[eclipseIot:cc3200-fvan/voltage:state:default]"}
Number FT_TimeToEmpty "Time to empty [%d min]" (All) {mqtt="<[eclipseIot:cc3200-fvan/tte:state:default]"}
Number FT_StateOfCharge "State of charge [%d %%]" (All) {mqtt="<[eclipseIot:cc3200-fvan/soc:state:default]"}

 

After the items, I defined the sitemap in the "intheair.sitemap" file. Pretty simple so far: three clickable items, leading to a chart visualising the history of that specific item.

 

sitemap intheair label="In The Air" {
     Frame label="Fuel Tank" {
          Text item=FT_Voltage {
               Switch item=FT_Voltage_Period label="Chart Period" mappings=[0="Hour", 1="Day", 2="Week"]
               Chart item=FT_Voltage period=h refresh=6000 visibility=[FT_Voltage_Period==0, FT_Voltage_Period=="Uninitialized"]
               Chart item=FT_Voltage period=D refresh=30000 visibility=[FT_Voltage_Period==1]
               Chart item=FT_Voltage period=W refresh=30000 visibility=[FT_Voltage_Period==2]
          }
          Text item=FT_StateOfCharge {
               Switch item=FT_StateOfCharge_Period label="Chart Period" mappings=[0="Hour", 1="Day", 2="Week"]
               Chart item=FT_StateOfCharge period=h refresh=6000 visibility=[FT_StateOfCharge_Period==0, FT_StateOfCharge_Period=="Uninitialized"]
               Chart item=FT_StateOfCharge period=D refresh=30000 visibility=[FT_StateOfCharge_Period==1]
               Chart item=FT_StateOfCharge period=W refresh=30000 visibility=[FT_StateOfCharge_Period==2]
          }
          Text item=FT_TimeToEmpty {
               Switch item=FT_TimeToEmpty_Period label="Chart Period" mappings=[0="Hour", 1="Day", 2="Week"]
               Chart item=FT_TimeToEmpty period=h refresh=6000 visibility=[FT_TimeToEmpty_Period==0, FT_TimeToEmpty_Period=="Uninitialized"]
               Chart item=FT_TimeToEmpty period=D refresh=30000 visibility=[FT_TimeToEmpty_Period==1]
               Chart item=FT_TimeToEmpty period=W refresh=30000 visibility=[FT_TimeToEmpty_Period==2]
          }
     }
}

 

Finally, I set up the persistence by creating a configuration file for it.

The file should be located in "/opt/openhab/configurations/persistence" and have the name of the persistence service to be used with ".persist" extension. In my case "rrd4j.persist".

 

This is what I put inside the configuration file:

 

Strategies {
  everyMinute : "0 * * * * ?"
  everyHour : "0 0 * * * ?"
  everyDay : "0 0 0 * * ?"

  default = everyChange
}

Items {
  * : strategy = everyChange, everyMinute, restoreOnStartup
}

 

After all the modifications, I restarted openHAB for everything to take effect.

 

To close this week's post, I have some screenshots of openHAB with some Fuel Tank BoosterPack data received from the CC3200 via MQTT:

imageimageimageimage

 

In my next post, I'll be describing in detail how I got the Fuel Tank to work with the CC3200 in order to retrieve battery information, along with longer duration measurements.

  • Sign in to reply
  • DAB
    DAB over 11 years ago

    Good post.

     

    I am looking forward to your fuel tank integration with the CC3200.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to fvan

    Thanks for the writeup of MQTT.

    Do you like how it works?

     

    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 11 years ago in reply to tomaja

    Hi Dragan,

     

    I'm currently using iot.eclipse.org for testing purposes, trying not to combine too many new elements at once (easier for troubleshooting image).

    Now that I know it's working, I can try to switch to AirVantage, knowing that this part is already working as expected.

     

    Frederick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tomaja
    tomaja over 11 years ago

    Hi Frederick,

    I still didn't receive my BBB but I should get it tomorrow. I'm sure this will help me install OpenHAB - your procedure looks straight forward.

    Are you using only iot.eclipse.org MQTT broker instead of using AirVantage or you use both in some way?

     

    Thanks,

    Dragan