In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog AirMobile - 16 - Low power delay
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
  • Author Author: amgalbu
  • Date Created: 7 Jan 2015 10:26 AM Date Created
  • Views 667 views
  • Likes 1 like
  • Comments 0 comments
  • iot_distributed
  • in_the_air
  • in-the-air
  • low-power
  • msp430
Related
Recommended

AirMobile - 16 - Low power delay

amgalbu
amgalbu
7 Jan 2015

Low-power delay

The CCS ULP Advisor tool is a great tool because it provides useful hints to squeeze microampers out of an application.

One of the suggestions was to get rid of delay loops. So I investigated how to implement a delay using timers. Implementation was not as difficult as I would expect.

First of all, the counter the timer has to reach is calculated.

 

uint32_t lcounter = HW_ACLK_FREQUENCY * ms10th;
    lcounter = lcounter / 10000;
    uint16_t counter = (uint16_t)lcounter - 1;

Then, Timer A needs to be initialized

 

/* Configure TimerA in up mode */
 TIMER_A_configureUpMode(TIMER_A1_BASE, 
                            TIMER_A_CLOCKSOURCE_ACLK, 
                            TIMER_A_CLOCKSOURCE_DIVIDER_1,
                            counter, 
                            TIMER_A_TAIE_INTERRUPT_DISABLE, 
                            TIMER_A_CCIE_CCR0_INTERRUPT_ENABLE, 
                            TIMER_A_SKIP_CLEAR);

    /* Start TimerA counter */
    TIMER_A_startCounter(TIMER_A1_BASE, TIMER_A_UP_MODE);

 

Next, the MCU is put in Low power mode 3 (see my previous post for details about different power modes)

 

    /* LPM3, TIMER_A1_ISR will force exit */
    __bis_SR_register(LPM3_bits + GIE);    

 

The interrupt routine is even simpler: just stop the timer and exit Low power mode 3


#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=TIMER1_A0_VECTOR
__interrupt
#elif defined(__GNUC__)
__attribute__((interrupt(TIMER1_A0_VECTOR)))
#endif
void TIMER1_A0_ISR_HOOK(void)
{
    /* USER CODE START (section: TIMER1_A0_ISR_HOOK) */
    TIMER_A_stop(TIMER_A1_BASE);
    LPM3_EXIT;   // Exit active CPU
    /* USER CODE END (section: TIMER1_A0_ISR_HOOK) */
}