In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog AirMobile - 9 - CO sensor
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
  • Author Author: amgalbu
  • Date Created: 27 Nov 2014 12:36 PM Date Created
  • Views 757 views
  • Likes 1 like
  • Comments 2 comments
  • iot_distributed
  • msp-exp430fr5969
  • tgs2442
  • msp_430
  • in_the_air
Related
Recommended

AirMobile - 9 - CO sensor

amgalbu
amgalbu
27 Nov 2014

CO sensor Figaro TGS2442

As CO sensor, I'm going to use the Figaro TGS2442.

 

Hardware considerations

Connecting the Figaro TGS2442 is relatively simple (the difficult part is drive its inputs properly!)

 

   image

 

The sensor requires application of a 1 second heating cycle which is used in connection with a circuit. voltage cycle of 1 second. Each VH cycle is comprised by 4.8V being applied to the heater for the first 14ms, followed by 0V pulse for the remaining 986ms. The Vc cycle consists of 0V applied for 995ms, followed by 5.0V for 5ms. For achieving optimal sensing characteristics, the sensor's signal should be measured after the midpoint of the 5ms Vc pulse of 5.0V.

The only component to dimension is the load resistance RL. Datasheet states that RL needs to be greater than 10k. I think a 39k resistor is a good trade-off

As usual, I added a buffer and a voltage divider to get a voltage between 0 and 2.0 V


  image

 

Software implementation

Using the same functions I already talked about in my previous post, I can write a the function to read out the output value provided by the TGS2442 sensor

 

#define SENSORS_NO2_HEATHER_PORT   3

#define SENSORS_NO2_HEATHER_PIN    0

#define SENSORS_NO2_OUTPUT_PORT    3

#define SENSORS_NO2_OUTPUT_PIN     1

 

void SENSORS_ReadCO()

{

      GPIO_setOutputLowOnPin(SENSORS_NO2_OUTPUT_PORT,

                  SENSORS_NO2_OUTPUT_PIN);

 

      // generate pulse on heather pin

      GPIO_setOutputHighOnPin(SENSORS_NO2_HEATHER_PORT,

                  SENSORS_NO2_HEATHER_PIN);

 

      delay(14);

 

      GPIO_setOutputLowOnPin(SENSORS_NO2_HEATHER_PORT,

                  SENSORS_NO2_HEATHER_PIN);

 

      delay(981);

 

      // generate output to measure NO2 level

      GPIO_setOutputHighOnPin(SENSORS_NO2_OUTPUT_PORT,

                  SENSORS_NO2_OUTPUT_PIN);

 

      delay(3);

 

      float val = SENSORS_AnalogRead(ADC12_B_MEMORY_3);

      SENSORS_Data.CO = SENSORS_Map(val, 0 , 1023, 0, 100);

}

 

Currently the delay function is implemented as a simple loop. I'm trying to devise a more energy-efficient implementation

  • Sign in to reply

Top Comments

  • amgalbu
    amgalbu over 11 years ago in reply to ipv1 +1
    Hi I got the Figaro and the MiCS from RS components. On RS I also bought a sharp dust sensor I didn't buy the MiCS sensor because I found a sample at work, but I think it comes from cdiweb.com (it was…
Parents
  • ipv1
    ipv1 over 11 years ago

    May I ask where you got the sensors from? Both the figrao and the mics?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amgalbu
    amgalbu over 11 years ago in reply to ipv1

    Hi

    I got the Figaro and the MiCS from RS components. On RS I also bought a sharp dust sensor

    I didn't buy  the MiCS sensor because I found a sample at work, but I think it comes from cdiweb.com (it was in a box with that logo)

     

    Hope it helps!

    Ambrogio

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • amgalbu
    amgalbu over 11 years ago in reply to ipv1

    Hi

    I got the Figaro and the MiCS from RS components. On RS I also bought a sharp dust sensor

    I didn't buy  the MiCS sensor because I found a sample at work, but I think it comes from cdiweb.com (it was in a box with that logo)

     

    Hope it helps!

    Ambrogio