In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog CC3200 Development in Visual Studio
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
  • Author Author: xever
  • Date Created: 21 Nov 2014 1:35 PM Date Created
  • Views 1930 views
  • Likes 4 likes
  • Comments 7 comments
  • cc3200-launchxl
  • iot_footprint
  • in_the_air
  • cc3200_launchpad
  • cc3200
Related
Recommended

CC3200 Development in Visual Studio

xever
xever
21 Nov 2014

In my last post, I have walked you through on how to write firmware for the MSP430 using Visual Studio and VisualGDB.  This post however is now focused on developing for the CC3200 using Visual Studio.

 

TI's CC3200 was not officially supported by VisualGDB, and so will have to follow their legacy tutorial on how to setup the development environment.  This tutorial however is a bit cumbersome and you will have to extract the GCC flags from the example make files.  Below are the VisualGDB (GCC) settings used for this approach.  Ensure that the CC3200 SDK has been installed in the default directory.

 

Argument

Value

Include Directories

C:\ti\CC3200SDK_1.0.0\cc3200-sdk\inc

C:\ti\CC3200SDK_1.0.0\cc3200-sdk\driverlib

${ProjectDir}

PreProcessor macros

gcc

Entry Point Argument

 

Linker Script

C:\ti\CC3200SDK_1.0.0\cc3200-sdk\tools\gcc_scripts\cc3200.ld

Additional Libraries

"add path as required."

C:\ti\CC3200SDK_1.0.0\cc3200-sdk\driverlib\gcc\exe\libdriver

CPU type flag

-mcpu=cortex-m4

There is one big hurdle with this approach, and that is debugging.  Setting up the environment to debug the firmware was a bit tricky such that it requires changes to OpenOCD, one needs to configure the connection interface with LaunchpadXL, etc. which I had serious struggle getting that up and running.  So I contacted SysProgs support team and ask them to lend me a hand on how to get debugging work on the CC3200.  Kudos to the support team, that not only they helped me out on how to configure the debugger, they actually made updates and patches to OpenOCD and officially support the CC3200.  My contribution to them was really about testing the update and providing feedback.  The tutorial can be found here.


I have tried the TI's sample applications by following the tutorials and they do work as expected.  Then I tried creating another project based on the tcpSocket example from which I will build my firmware for the sensor nodes.  My current VS solution now looks like the image below.



image



Some important stuff:


  • If you have setup VisualGDB before and have OpenOCD already installed, you will have to manually delete the folder C:\Users\<CurrentUser>\AppData\Local\VisualGDB\EmbeddedDebugPackage\com.sysprogs.arm.openocd.  If this folder has not been deleted, VisualGDB will throw an error in Step 5 of the tutorial.
  • When selecting the CC3200 MCU variant, if your CC3200 LaunchpadXL board is rev 3.2, choose XCC3200HZ (170Kb RAM variant).  Better yet, check the chip marking.
  • Possibly the most important part.  Microsoft has released Visual Studio Community Edition which has all the capabilities of the VS Professional variant but FREE.  You can download Visual Studio Community Edition here.

 

Now that the development environment has been setup for my sensor nodes, my next posts will be more design-focused and will go through the guts of the CFMS (Carbon Footprint Monitoring System).

  • Sign in to reply

Top Comments

  • clem57
    clem57 over 11 years ago +2
    @ Christever del Rosario Great write up. Thanks for pointing out link for microsoft download. Clem
  • shabaz
    shabaz over 11 years ago +1
    It would be cool if there was a tool to convert back-and-forth between the settings in VS and a GNU Makefile. Otherwise, it gets difficult for people to replicate on non-Windows platforms : ( (assuming…
Parents
  • amgalbu
    amgalbu over 11 years ago

    It's pity it only works with Professional+ versions of Visual Studio... should it work with Express version this would be a great free alternaitve!

     

    Great post!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • xever
    xever over 11 years ago in reply to amgalbu

    Microsoft has released Visual Studio Community Edition which has the same features as the Professional.  You can find out more here.  So you can stop using Express editions and move to the Community Edition.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • xever
    xever over 11 years ago in reply to amgalbu

    Microsoft has released Visual Studio Community Edition which has the same features as the Professional.  You can find out more here.  So you can stop using Express editions and move to the Community Edition.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • amgalbu
    amgalbu over 11 years ago in reply to xever

    Great news!

    Thanks!!