In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog Dust, Temperature and Humidity Monitor Chapter 1
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
  • Author Author: engswee
  • Date Created: 30 Oct 2014 4:21 AM Date Created
  • Views 857 views
  • Likes 2 likes
  • Comments 1 comment
  • haze_monitor
  • in_the_air
Related
Recommended

Dust, Temperature and Humidity Monitor Chapter 1

engswee
engswee
30 Oct 2014

Project code     : Nanoimp.

Objective          : Monitor and eliminate dust and particle in the air.

Location           : Singapore (1.2971342,103.7777567,17).

Time                 : 2160 hour.

Target               : Complete system, low cost, & better life

 

 

Idea 101:


image

Now the air quality become worse and worse especially in town area. This idea is to solve air issue for critical need like asthma patient, laser laboratory and baby or elderly.

 

The main Idea is build monitor system and air filter system.

Monitor device is for monitor dust, temperature and humidity in the air.

Air filter device is to filter air and cool the area(optional).

This two device will work together via IoT.

 

All the device can be link and manage to work together or individual.

For example, user can setup 3 monitor system with just one filter system. The information from 3 monitor system can be use to control the filter system in a require setting.

On the other way round, user also can only use one monitor system to control multiple filter system.

 

Monitor System:

 

This is planning monitor system and not the end prototype. It will be different in part and program development.

My plan is try to use the given device before going to other.

This is the main system to be done. I hope can complete all but for now just concentrate on the main.

 

Monitor System 1:

image

 

Monitor System 2:

 

image

 

 

Filter System:

 

For filter system the main idea is simple. Force dust and particle (nanoimp) to water and trap them in the water.

If this still not enough then trap them in HEPA filter after the water trap.

Not sure what sensor will be included at this moment, maybe water level. Let see how.



image


Some testing:


Filter test:

image

It look simple, build simple and it simply work image

 

Try using the big fan with no speed drive it blow hard to water and water splash every where.

End up running 12V blower for few hour and the result quite good but those big fan work great he..he..

 

Simple check using 10W LED  touch light to check the dust and look like this method working very well.

The big dust & particle even can seen in the water trapped image

 

Sorry no waterproof camera to show the dust & particle in the water.

Maybe next time update you guys with the picture.

 

 

 

 

 

 

Show time but it a bit boring.image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Sierra Wireless system Testing:

I have starting to play around with Sierra wireless cloud system to more understanding their system.

image

 

Starting with registering and it was easy (http://developer.sierrawireless.com/Cloud%20Platform.aspx).

First view around for example as many as I can get to boost up the development time.

When searching around the system look very serious, They plan for BIG, I mean is their system is design so that can support thousand or even million device and all around the world.

Don't worry, with this ability then for small quantity it should not be an issue he..he..

 

I found this and it look easy (http://airvantage.github.io/tutorials/2013/07/05/rest-for-devices/)

 

Have try for few time to upload my apps but just get error for not supported file. Maybe there are something wrong or stupid thing done by me.

I just hope they have a working downloadable file for user to try out.

Will try again when have free time image

 

 

 

 

Sharing:

SKEDD it coolimage

Be patience for the video image

http://www.we-online.de/web/en/intelligente_systeme/neu__skedd/startseite.php

 

Other Support link:

Würth Elektronik tool:

http://www.we-online.de/web/en/electronic_components/toolbox_pbs/Toolbox.php

 

Air Design Challenge TI support:

http://www.element14.com/community/message/129415/l/have-a-question-for-ti-ask-it-here#129415

 

Sierra Wireless support:

https://signup.airvantage.net/public/avep/

 

More for Sierra Wireless and look like I need more time to digest the given information

Ger started

https://na.airvantage.net/

More example

http://airvantage.github.io/tutorials/eclo/

http://airvantage.github.io/devkit/app/#/data/b814c0981882494cb09830d93aeb0aaf

https://doc.airvantage.net/display/USERGUIDE/Tutorial+videos

User guide

https://doc.airvantage.net/display/USERGUIDE/User+Guide

Example for BBB ( look simple, but have a try to fell the burn)

https://github.com/crystallam/beagleboneblack-mqtt-greenhouse

 

Please use the support wisely image

 

Previous

Dust, Temperature and Humidity Monitor                  

 

Next

Dust, Temperature and Humidity Monitor Chapter 2

  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Nice post.

     

    I like the fan blowing into the water.

    It would be an interesting side product to put some of the water drops onto a microscope slide to see what all you are cleaning from the air.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    Nice post.

     

    I like the fan blowing into the water.

    It would be an interesting side product to put some of the water drops onto a microscope slide to see what all you are cleaning from the air.

     

    DAB