In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog IOT - In the Air Design Challenge - Portable Field Tester #3
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
  • Author Author: dwinhold
  • Date Created: 23 Nov 2014 7:07 PM Date Created
  • Views 1236 views
  • Likes 4 likes
  • Comments 4 comments
  • in_the_air
Related
Recommended

IOT - In the Air Design Challenge - Portable Field Tester #3

dwinhold
dwinhold
23 Nov 2014

Portable Field Tester part 3, making a solar power supply:

 

This part will be written by my daughter Chrystal, she is looking after making the power supply for our field tester (With my guidance).

 

Hi everyone, my name is Chrystal and I am 14 years old. My dad has helped me with this part by explaining diodes, resistors and how electricity works. I will explain each picture in detail as they are posted.

 

Diodes:

They allow electricity to pass only one way. So the power coming from our solar panel to the chargeable batteries have a diode soldered in (Silver ring end of diode towards the batteries). This stops the charged batteries from forcing electricity back up the wire to the solar panels.

 

image

 

The power supply I made is only for testing as my solar panel I have is not strong enough to power the project. As shown below we are only getting 2V from our small panel. We added a volt meter (I, with Dad's help, built it from a kit) with a push button to display the voltage. The volt meter is powered by a 9 volt battery (This is a waste of energy and won't be battery run in the final project), the push button only displays the volts for the length of time pressed (Saves some energy from being wasted).

 

 

 

image

 

The 150 Ohm resistor is to being the 9 volt battery down to the 5 volts required to run the volt meter. The resistor isn't exactly what we should have used as it drops us down to 4.6 volts but still works good (I should have used a 130 OHM resistor).

 

Recharger Wires:

So the picture above (Mess of wires) I will explain how this works. The green panel behind the battery is the backside of the solar panel. There are 2 red wires and 2 black wires attached, 1 red and black to the battery charger and the other 2 go to the volt meter. The positive red wire that goes to the charger has the diode. It is attached to the positive side of the charger. The negative wire is attached to the negative on the charger.

 

Volt Meter Wires:

The other red and black wires go to the volt meter test end. I wired it wrong the first 3 times, I hooked it up to the power side which didn't work, then reverse to the test side (Dad finally explained what I did wrong... I learned a lot from this mistake). The positive rom the battery with the resistor attached went to the positive on the volt meter and negative to negative. Oh, I almost forgot to say I put a push button on/off switch in the positive wire of the volt meter.

 

image

 

Working solar energy:

After it was all together I tested it. The panel was put in the light and I pressed the button...... It worked, 2 volts shown!!! I did it, except..... I require around 9 volts to run everything (Beaglebone, TI's, sensors.... image) My solar panel is to small for the energy I require to collect.

 

image

 

Conclusion:

The power supply worked great but I require a bigger or more panels to reach the required volts. Dad just informed me he had ordered the panels we required so when they arrive I will make this run our Field Tester.

 

More to come,

 

Chrystal W.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +1
    Good job Crystal. It takes a while to learn and remember all of the things you need to build electronics. Luckily your dad has the right attitude to let you try and then explain what went wrong. Keep on…
  • amgalbu
    amgalbu over 11 years ago +1
    Great job Crystal! Keep on experimenting Ambrogio
  • jw0752
    jw0752 over 11 years ago +1
    Hi Crystal, You did a great job and your dad is lucky to have such a smart partner for this project. Keep making those mistakes! I have learned that I seldom really learn things as well as I do when they…
Parents
  • jw0752
    jw0752 over 11 years ago

    Hi Crystal, You did a great job and your dad is lucky to have such a smart partner for this project. Keep making those mistakes! I have learned that I seldom really learn things as well as I do when they are learned from mistakes. You indicated that you felt it was a waste to have to use 9 volts in order to read the 2 volts of the Solar Panel. Don't loose sight of the fact that the voltage is only one dimension of the real quantity of importance called POWER (Volts times Amps). Despite the difference in the numbers 9 volts and 2 volts the amount of actual power being used by the meter is probably very small compared to the power generated by a solar panel in direct sunlight. I look forward to reading more about your project.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 11 years ago

    Hi Crystal, You did a great job and your dad is lucky to have such a smart partner for this project. Keep making those mistakes! I have learned that I seldom really learn things as well as I do when they are learned from mistakes. You indicated that you felt it was a waste to have to use 9 volts in order to read the 2 volts of the Solar Panel. Don't loose sight of the fact that the voltage is only one dimension of the real quantity of importance called POWER (Volts times Amps). Despite the difference in the numbers 9 volts and 2 volts the amount of actual power being used by the meter is probably very small compared to the power generated by a solar panel in direct sunlight. I look forward to reading more about your project.

    John