In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog Pollution Effect Minimiser (Post 4)
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
  • Author Author: e14 Contributor
  • Date Created: 29 Nov 2014 8:44 AM Date Created
  • Views 635 views
  • Likes 1 like
  • Comments 0 comments
  • iot_pollution_effect
  • in_the_air
Related
Recommended

Pollution Effect Minimiser (Post 4)

e14 Contributor
e14 Contributor
29 Nov 2014

Setting up Beaglebone Black

This is my post for setting beaglebone for connecting to airvantage. For this beaglebone needs to be setup. For windows machine follow the following steps :

  1. Connect beaglebone to USB port of pc using usb cable.
  2. Install drivers for beaglebone from http://beagleboard.org/getting-started. It may take a while to install the drivers.
  3. Launch : http://192.168.7.2 to log into the board.

Next connect the beaglebone black to internet using Ethernet or Wifi.

Open Cloud9 IDE by going to the address http://192.168.7.2:3000/ .

Then i noticed an article on the element14 site to update the image of debian. The factory installed version has many problems. I tried to login from the user debian to root but it asks for a password which is not there. You will always notice a authorization failure in this case.

So to avoid these problem update your image. This can be done in two ways :

  1. By Flashing the image to emmc:
  2. Download the latest image from http://beagleboard.org/latest-images.
  3. The downloaded image is a .img.xz file. Then download 7zip to decompress the archive.
  4. Use 7-zip to decompress the SD card .img file. In my case 7zip was not able to open the archive.I had the following error saying “cannot open file as archive.”
  5. So i used my ubuntu pc to flash the sd card with the image.
  6. In ubuntu just click on the link and restore the image on the sd card.
  7. Now power down the beaglebone insert the sd card and press down the BOOT button and power up the board.
  8. If using BeagleBone Black and the image is meant to program your on-board eMMC, you'll need to wait while the programming occurs. When the flashing is complete, all 4 USRx LEDs will be steady on or off. The latest Debian flasher images automatically power down the board upon completion. This can take up to 45 minutes. Power-down your board, remove the SD card and apply power again to be complete.
  9. In my case i had errors in this case, the board started with the emmc flashing and the user leds started blinking in a sequence. But after 5 minutes this stopped and all of them started to glow. I powered the board down to see if the process is over but i noticed that the board wasn’t booting. I was not able to ssh into the board. So i used the other method of using an sd card to boot the board.
  10. By using sd card :
  11. Download the latest image from http://beagleboard.org/latest-images (bootable sd card image)
  12. Decompress the image using 7zip and flash it to the sd card using win32disk imager on windows or restore it in ubuntu.
  13. Now power down the beaglebone insert the sd card and press down the BOOT button and power up the board.
  14. For booting with sd card this is all you have to do. The board will boot from the card.