In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Documents In the Air Challenge Competitors
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: doctorcdf
  • Date Created: 24 Oct 2014 10:27 AM Date Created
  • Last Updated Last Updated: 8 Oct 2021 7:56 AM
  • Views 1445 views
  • Likes 3 likes
  • Comments 3 comments
Related
Recommended

In the Air Challenge Competitors

Janis Alnis | Dominic Amann | Ravi Butani | Christever del Rosario | Ambrogio Galbusera | Dragan Knezevic | Crystal Knodel | Ryan Longlong M. Labutap | Manolis Nikiforakis | Inderpreet Singh | Gan Eng Swee | Anshul Thakur | Frederick Vandenbosch |  Dale Winhold | Michael Wylie

imageJanis Alnis
Latvia
Project: Air Quality Monitoring In School Classes
Synopsis:

Carbon dioxide in air makes people feel tired: ventilation in Latvian schools is a problem, especially in winter as there is no active ventilation.

There are 8-9 classes per day and students get very tired in the afternoon. One could monitor how air changes throughout the day.

One could analyse if classes requiring active thinking (during math test) use more oxygen and produce more CO2.

Read Janis's project blogs (tag school_air)

imageDominic Amann
Canada
Project: Automated Greenhouse Climate Control
Synopsis:

I will create an automated climate control system for a greenhouse. The glass house would be heated by solar, augmented by geothermal, with computer control of the circulation system. The greenhouse would use the Beaglebone as the primary controller to bring together sensing information about temperature, humidity, soil moisture, soil chemistry etc. This information can be used to drive sprinkler systems and control temperatures to provide an ideal growing environment for chosen food crops. Actuators could open and close air vents, and draw over shades as necessary.

Read Dominic's project blogs (tag auto_greenhouse)

imageRavi Butani
India
Project: Healthier Living with IoT
Synopsis:

I am designing an IoT based system using Beaglebone Black and CC3200 Launchpad as main processing part for sensing and controlling Air quality and water quality for Breath Easily and Healthier Living by means of controlling Air-condition, Ventilators and Exhaust Fan using real time Air Quality data of indoor and outdoor environment. The system also monitors TDS level of drinking water in home.

All the real time data will be available online from AirVantage M2M cloud by mihini running on Beaglebone Black.

Read Ravi's project blogs (tag iot_healthy)

imageChristever del Rosario
New Zealand
Project: Carbon Footprint Monitoring System
Synopsis:

I will build a realtime carbon footprint monitoring system using IoT technology. Using this system, the user will be informed of the current carbon footprint on a daily basis, provide suggestion on how to reduce this footprint and trigger warnings should "daily allowances" are reaching pre-defined thresholds.  Along with this goal, the system is to keep a healthier and safer dwelling.

Read Christever's project blogs (tag iot_footprint)

imageAmbrogio Galbusera
Italy
Project: Distributed Network of Air Quality Sensors
Synopsis:

I will make a sensor that can be installed on cars, but in the future handlebar-mounted and armband versions of the sensor can be designed.

The sensor is battery-free and harvest energy from car radiator heat by means of a Peltier cell. Data is transferred to a smartphone through a Bluetooth Low Energy link. The smartphone internet connectivity is leveraged to push data to a cloud service.

Data from all the installed sensors can be analyzed at home thanks to a plugin that will be developed as part of this project.

Read Ambrogio's project blogs (tag iot_distributed)

imageDragan Knezevic
Serbia
Project: Pollen & Allergen Sensor
Synopsis:

My idea is to make a system that would enable users with allergies to be aware of pollen, dust and other allergen levels in the outside air and to isolate living space from the outside. This could be done by alerting users to close all windows (or to even close windows automatically if supported - like with Velux windows) and turn ventilation with pollen filters on or automatically start the indoor air-purifier device. This system would be extendable with possibility to detect other kinds of outside air pollution and providing alerts.

Read Dragan's project blogs (tag iot_pollen)

imageCrystal Knodel
United States
Project: Portable Air Quality Monitor
Synopsis:

The goal is to design a small, portable, battery operated device that could be deployed by the user in any space office or home space. IoT connectivity to the cloud will allow for room by room tracking of environmental parameters and data logging. Indoor air quality will then be compared outdoor air quality in the cloud.

Read Crystal's project blogs (tag iot_portable_air)

imageRyan Longlong M. Labutap
Philippines
Project: Low Cost Harmful Algal Bloom Monitoring
Synopsis:

Harmful Algal Bloom describes coastal phenomenon where high algal biomass or concentration of algae is detected with effects including depleted dissolved oxygen and discoloration in bodies of water. Numerous HAB monitoring methodology have already been established from traditional method of water sampling then conducting test on water samples in the laboratory, to modern sophisticated method such as satellite imaging. In the Philippines, the common method is still water sampling and testing in laboratory which wastes so much time for information/advisories to be accessible to public. Modern methods are not considered due to very high cost that can range up to millions of dollars. This project aims to address these problems.

Read Ryan's project blogs (tag iot_algal)

imageManolis Nikiforakis
Greece
Project: Air ex Machina
Synopsis:

My project is to create a compact, solid, battery powered weather & air quality station based on CC3200 with the following sensors :

  • Rain drops sensor (basic accuracy for low/high precipitation)
  • Temperature/Humidity Sensor (DHT22)
  • Grove - Air quality sensor
  • NO2/CO Sensor (MICS-4514)
  • Particle sensor (for dust or pollen)
  • Ozone (O3) Sensor
  • Volatile Organics (VoC) Sensor

The above system will be power by batteries, and will require a cleverly designed box to keep the electronics dry, but expose the sensors to the elements, as this box will be placed on my flat’s balcony.

Read Manolis' project blogs (tag air_ex_machina)

imageInderpreet Singh
India
Project: Firecracker Aftermath Analyzer
Synopsis:

An air pollution analyzer will be designed. It will have sensors for the following:

  1. Air Temperature
  2. NO2 Levels
  3. Single Sensor for carbon monixide, alcohol, acetone, thinner, formaldehyde
  4. Particulate levels in the air
  5. Humidity
  6. Carbon Monoxide
  7. O2
  8. Sulphur based gases
Read Inderpreet's project blogs (tag iot_firecracker)

imageGan Eng Swee
Singapore
Project: Dust, Temperature And Humidity Monitor
Synopsis:

In Singapore there is a yearly haze: this smoke comes from burning plantations. It will be very useful for the user and public to have a monitor of the dust, temperature and humidity to monitor its effects.

Read Gan Eng's project blogs (tag haze_monitor)

imageAnshul Thakur
India
Project: Pollution Effect Minimiser
Synopsis:

In my project I will be monitoring and controlling a lot of sensors and actuators to minimise the effect of pollution: noise, water, light, & air.

Read Anshul's project blogs (tag iot_pollution_effect)

imageFrederick Vandenbosch
Belgium
Project: Self Powered Sensor Nodes
Synopsis:

My project idea for this challenge is one of wireless, self-powered sensor nodes reporting to a central unit which can, if needed, trigger air filtering systems in specific rooms/areas.

Read Frederick's project blogs (tag iot_sensor_nodes)

imageDale Winhold
Canada
Project: Portable Environment Field Tester
Synopsis:

I will create a Portable Environment Field Tester. This can be used by outdoor enthusiasts, researchers, campers, hunters or anyone who spends time outdoors. The chances of getting lost is not very great, but running out of water, getting bad weather, being in an area with bad air quality or falling in contaminated mud or dirt is greater.

Read Dale's project blogs (tag iot_field_tester)

imageMichael Wylie
United States
Project: Particle Counting System
Synopsis:

I will design a particle counting system that can be embedded into HVAC units. This sensor can be interfaced through an IoT enabled device and the resulting particle counts can be used to control how a smart home responds to airborne particulates. More importantly, the particle counter can be used as a Particulate Matter (PM) sensor. The PM10 and PM2.5 levels are globally used as the Air Quality Index (AQI).

Read Michael's project blogs (tag iot_particle_counter)
  • eclipse_iot
  • cisco
  • keysight
  • sierra_wireless
  • beaglebone_black
  • internet_of_things
  • in_the_air
  • texas_instruments
  • iot
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 12 years ago +2
    All the projects here look extremely interesting. Looking forward to seeing these develop!
  • shabaz
    shabaz over 12 years ago in reply to kas.lewis

    It wasn't that long ago (maybe a year ago?) that the average home project used a single microcontroller or RPI board. Now, nobody here is shy to use multiple different platforms, wireless and tons of sensors, multiple energy sources and cloud platforms, to realise solutions within a couple of months!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kas.lewis
    kas.lewis over 12 years ago

    Definitely looking to see how some of these turn out, they sound very interesting and well thought out. Can't wait to hear more about each project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago

    All the projects here look extremely interesting. Looking forward to seeing these develop!