Inductive Sensing
  • Challenges & Projects
  • Design Challenges
  • Inductive Sensing
  • More
  • Cancel
Inductive Sensing
Blog Inductive Sensing Design Challenge: USB Microphone based on the LDC1000 Inductance to Digital Converter (week 1)
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 26 Apr 2014 6:40 PM Date Created
  • Views 3734 views
  • Likes 1 like
  • Comments 9 comments
  • inductive_sensing
  • eagle
  • inductive_sensing_challenge
  • microphone
  • farnell
  • usb
  • ldc1000
  • texas_instruments
  • road_test
Related
Recommended

Inductive Sensing Design Challenge: USB Microphone based on the LDC1000 Inductance to Digital Converter (week 1)

e14 Contributor
e14 Contributor
26 Apr 2014

Hi everyone, my name is Sammy Peiren. This is the first blog post for my entry in the inductive sensing design challenge. The basic idea is to build a USB microphone based on the inductance to digital principle. Since the LDC1000 provides a digital output, it should be possible to get a USB connection.

 

image

 

To understand how I plan to detect sound with the LDC1000 I will give a short overview of the basic idea:

Imagine a point source that emits sound waves. As the waves are produced from the source, they propagate by vibration of particles in a medium (for example open air).

 

If a sound wave strikes a flexible object, a portion of the total energy will be reflected and another part will be transferred into a vibration of the object (absorption).

Some energy (heat) will be lost as the wave travels through the object and encounters friction from the material. Sound waves travel faster in a dense medium, thus the sound will be refracted by its encounter with a solid object. This is illustrated in the following figure:

image

 

Imagine we take a flexible plate and apply a sound wave to it. As the sound wave travels through the plate it will vibrate resulting in a slight flexing. The next figure shows an exaggerated example of this. Imagine we observe the position of the plate (by position we mean the nearest point on any part of the plate) from a certain point. If no sound wave is applied, the distance between the plate and the observation point is equal to A. In the second situation a sound wave strikes the plate and the plate flexes slightly inward. From our observation point, the distance of the plate is now equal to C. The difference between the original idle position of the plate and the flexed position is exactly B. In the third situation, the plate flexes back to the other side. This results in a new relative position which is equal to D. This is exactly equal to the original idle position plus B or C plus two times B.

 

image

 

 

The relative position of the plate can be plotted versus time as shown on the following figure:

image

 

The LDC1000 is capable of detecting the movement of a conductive surface so if we were to use a conductive plate and the plate were sufficiently flexible, it should be possible to measure the movement of the plate by using inductive sensing.

 

But how does the vibration of a piece of metal translate into something we can hear? If we look at this in terms of sound there are two factors that will determine the character of the sound:

-the amplitude of the vibrations will correspond to the loudness of the sound

-the frequency of the vibrations will correspond to the pitch of the sound

 

We can plot the response of the microphone to various frequencies. The frequency response, determined by the material and the surrounding structures tells us how much of the vibration is transferred at a certain frequency. In our case the frequency response is also determined by the sensor frequency (to get a decent response time and output data rate the sensor frequency needs to be high enough). As shown in the next figure it is very common to use a logarithmic frequency axis and a logarithmic value for the amplitude (the decibel).

http://www.shure.co.uk/dms/shure/products/microphones/frequency-curves/sm/frequency-response_sm58/frequency-response_sm58.gif?1255946787

source: SM58 The legendary vocal microphone

 

There are other parameters that will determine how good the microphone works:

The dynamic range of the microphone tells us what the minimum and maximum amplitude of the vibration is we can detect. There are also various parameters that will determine what the dynamic range of the LDC1000 <-> transducer combination will be including the distance of the transducer, the construction of the coil, RP_min and RP_max.

 

The main advantages of using the LDC1000 are the high sensitivity and dynamic range and the fact that it has a digital output. Since the LDC1000 only requires a coil and a conductive target, there are also no rare-earth magnets required. I do expect some difficulties as the basic setup shows that the LDC output is not linear for a basic position measurement (see figure).

 

image

 

I hope to learn a lot from this project and I'm sure it will be a very interesting project. Be sure to follow my blog if you are interested in inductive sensing and/or sound. This will be a rather experimental project, but you can expect a thorough explanation of all the steps, backed up by measurements and calculations.

 

The first few weeks will consist of getting to know the capabilities of the LDC1000 and its limitations. Once I receive the LDC1000EVM I hope to get started with my basic experiments, so stay tuned!

  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Hi Sammy,

     

    Good idea.  I thought of something similar using a mounted sheet of plastic with a thin metal plate or magnet.

    If you draw the plastic tight like a drum head, then you can pickup the vibrations using the LDC detector.

    It will be very interesting to see how sensitive your microphone can be given the micron detection capability of the device.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to DAB

    Hi,

     

    That might be a good option for the transducer. I don't really have any experience with the mechanics of flexing plates/foils. Theoretically it should work very well given the LDC1000's specs. I think it will be a matter of getting all the parameters just right to get the maximum dynamic range and sensitivity.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to DAB

    Hi,

     

    That might be a good option for the transducer. I don't really have any experience with the mechanics of flexing plates/foils. Theoretically it should work very well given the LDC1000's specs. I think it will be a matter of getting all the parameters just right to get the maximum dynamic range and sensitivity.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • DAB
    DAB over 12 years ago in reply to e14 Contributor

    Just keep it simple, take a sheet of plastic food wrap and then attack a small piece of metal tape.

    Use an old plastic bowl and drill some holes in one end and attach the plastic wrap to the opening with some tape.

    Then you adjust the LDC detector until you can see detection as you blow into the other side of the bowl.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to DAB

    That is a good idea. My initial idea was quite similar: to use a cardboard tube with some stretched aluminum foil at one end. Like you say it'll be a matter of adjusting the LDC and the distance between the coil and metal to get a good detection.