Internet of the Backyard
  • Challenges & Projects
  • Design Challenges
  • Internet of the Backyard
  • More
  • Cancel
Internet of the Backyard
Blog Backyard Challenge: Week One
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 25 Aug 2014 11:26 PM Date Created
  • Views 883 views
  • Likes 0 likes
  • Comments 1 comment
  • iot_backyard
  • internet_of_things
  • cc3200_launchpad
  • ti
  • iot_water
Related
Recommended

Backyard Challenge: Week One

e14 Contributor
e14 Contributor
25 Aug 2014

First I would like to thank element14 and TI for choosing me as one of the RoadTesters for the Internet of the Backyard Challenge.

 

For my project I will design a watering system for a backyard garden which will not only keep track of the moisture of the soil to determine how much water is needed, but also keep small animals like squirrels away from the plants by spraying water if it senses their presence.

 

The basic layout of the project will include electrically controlled (solenoid) water valves, a water flow sensor, moisture sensor, a passive infrared sensor (PIR), and possibly other sensors for weather data. The flow sensor will be connected to a y-connector (or multi-connector) and then to one or more solenoid valves which will control flow to the garden. I will most likely be using a perforated hose laying on the soil for the main water supply and a sprinkler to fend off small animals. The water flow sensor will help me gauge water usage and determine how much water is needed for the desired moisture level. The system will be controlled by the TI CC3200 controller board and Fuel Tank Boosterpack. If my budget allows I may use solar power to keep the Fuel Tank Boosterpack powered.

 

I have already looked at the initial parts I would like to use, and now just have to check what additional parts I will need to put all of this together.

 

Till next week!

  • Sign in to reply
Parents
  • mcb1
    mcb1 over 12 years ago

    I will most likely be using a perforated hose laying on the soil for the main water supply

    The other option is drippers.

    The advantage is you can place them relative to the plant or attach a small hose to extend the range.

    Most have a set rate for pressure v time which may remove the need for the flow sensor.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 12 years ago

    I will most likely be using a perforated hose laying on the soil for the main water supply

    The other option is drippers.

    The advantage is you can place them relative to the plant or attach a small hose to extend the range.

    Most have a set rate for pressure v time which may remove the need for the flow sensor.

     

    Mark