Internet of the Backyard
  • Challenges & Projects
  • Design Challenges
  • Internet of the Backyard
  • More
  • Cancel
Internet of the Backyard
Forum Have a question for TI re: The Internet of the Backyard Challenge? Ask here!
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 39 replies
  • Subscribers 8 subscribers
  • Views 5889 views
  • Users 0 members are here
  • iot_backyard
Related

Have a question for TI re: The Internet of the Backyard Challenge? Ask here!

doctorcdf
doctorcdf over 12 years ago

This thread is dedicated to questions for the Internet of the Backyard challenge; Texas Instruments' staff will be monitoring it regularly.

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to BigG +1
    It looks like the is a FET switch configured to protect against reverse voltage and should also protect the batteries from harm if the USB or other supply is also connected (Q2 bottom right)
  • bwelsby
    bwelsby over 12 years ago in reply to DAB +1
    DAB wrote: What is the APP needed to open the CCS 6 download? I got the same message on Windows 8.1 and 7. The TI message indicated that they were .exe files, but when I tried to change the name…
  • janisalnis
    janisalnis over 12 years ago in reply to e14 Contributor +1
    Registering at Plotly is free of charge for everyone. Limitation, I read somewhere, is that it would allow to store 50 plots. Is there an simple HTTP POST example for CC3200? There is a GET function used…
Parents
  • janisalnis
    janisalnis over 12 years ago

    Hi!

     

    I have a question about energy saving mode.

    In my application the board could sleep for 5 min and then wake up to send data.


    I am trying to put CC3200 in hibernate mode (Examples Sensor_Profile and Hib) to reach the advertisized 1 year running time from 2xAA.

    If I measure current across jumper J12 it is 0.2 mA (decreases to 20uA with extra 100k pull resistors soldered to the serial flash chip).

    However the current drawn from 2xAA battery connector in hibernate mode is 0.64 mA with J13 removed (and unsoldered PWR and RESET LEDs).

     

    There is boost regulator 3.3V chip U8. I suspect it consuming this extra current. (Or I2C chips?)

    What is the purpose of boost DC/DC 3V3 U8? Is it supplied with a preproduction CHIP having a bug on the LAUNCHXL needing external DC/DC.

    Coil L4 belonging to ANA_2 pins on the demo board is not populated.


    With 0.6 mA could expect ca 3 months from AA cells but 20 uA would be great to have if possible.


    Greetings,

    Janis.




     



     


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • janisalnis
    janisalnis over 12 years ago

    Hi!

     

    I have a question about energy saving mode.

    In my application the board could sleep for 5 min and then wake up to send data.


    I am trying to put CC3200 in hibernate mode (Examples Sensor_Profile and Hib) to reach the advertisized 1 year running time from 2xAA.

    If I measure current across jumper J12 it is 0.2 mA (decreases to 20uA with extra 100k pull resistors soldered to the serial flash chip).

    However the current drawn from 2xAA battery connector in hibernate mode is 0.64 mA with J13 removed (and unsoldered PWR and RESET LEDs).

     

    There is boost regulator 3.3V chip U8. I suspect it consuming this extra current. (Or I2C chips?)

    What is the purpose of boost DC/DC 3V3 U8? Is it supplied with a preproduction CHIP having a bug on the LAUNCHXL needing external DC/DC.

    Coil L4 belonging to ANA_2 pins on the demo board is not populated.


    With 0.6 mA could expect ca 3 months from AA cells but 20 uA would be great to have if possible.


    Greetings,

    Janis.