Internet of the Backyard
  • Challenges & Projects
  • Design Challenges
  • Internet of the Backyard
  • More
  • Cancel
Internet of the Backyard
Forum Have a question for TI re: The Internet of the Backyard Challenge? Ask here!
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 39 replies
  • Subscribers 8 subscribers
  • Views 5889 views
  • Users 0 members are here
  • iot_backyard
Related

Have a question for TI re: The Internet of the Backyard Challenge? Ask here!

doctorcdf
doctorcdf over 12 years ago

This thread is dedicated to questions for the Internet of the Backyard challenge; Texas Instruments' staff will be monitoring it regularly.

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to BigG +1
    It looks like the is a FET switch configured to protect against reverse voltage and should also protect the batteries from harm if the USB or other supply is also connected (Q2 bottom right)
  • bwelsby
    bwelsby over 12 years ago in reply to DAB +1
    DAB wrote: What is the APP needed to open the CCS 6 download? I got the same message on Windows 8.1 and 7. The TI message indicated that they were .exe files, but when I tried to change the name…
  • janisalnis
    janisalnis over 12 years ago in reply to e14 Contributor +1
    Registering at Plotly is free of charge for everyone. Limitation, I read somewhere, is that it would allow to store 50 plots. Is there an simple HTTP POST example for CC3200? There is a GET function used…
Parents
  • janisalnis
    janisalnis over 12 years ago

    Hello!

     

    I was struglling with CC3200 analog input ADC example. It was not working. Sometimes giving only erratic values, sometimes only zero ADC values. Only the timer bits increased as they should. Found a forum topic about this bug:

    http://e2e.ti.com/support/wireless_connectivity/f/968/t/365450.aspx

    http://e2e.ti.com/support/wireless_connectivity/f/968/p/354092/1243186.aspx#1243186

    Need a line in while (forewer) loop uiIndex=0;

     

     

    ADC on PIN_57 is not allowed by example. Why? It giving value around 1090 regardless if connected to GND or not.

    ADC on pins PIN_58 and PIN_59 do not have resistors "dnp" on P3 header. (Actually resistors are on P1 header so one can connect signals there).

     

     

    There is another strange thing. It ADC input is floating the voltage on it is 0.5 V. If pin_60 is tied to GND via 100k then voltage is 0.4 V.

    Is there some pull-up on the pin that has to be additionally disabled?

    I made a voltage divider using 100k and 1Meg. 0.1 uF cap at ADC input was necessary to prevent pickup.

     

     

    I have changed example to a function that returns just 1 value read from CC3200 ADC. A delay was added between enabling ADC and readout allowing the input voltage to settle down. Without such delay the value was erratic.

    ----------------------------------------------------------------

    float readADC(unsigned long uiAdcInputPin)

        {   unsigned int  uiChannel;

            unsigned long ulSample;

     

            //uiAdcInputPin=PIN_60;

            PinTypeADC(uiAdcInputPin, 0xFF);

     

            switch(uiAdcInputPin)

            {

                case PIN_58: {uiChannel = ADC_CH_1;}break;

                case PIN_59: {uiChannel = ADC_CH_2;}break;

                case PIN_60: {uiChannel = ADC_CH_3;}break;

                default: break;

            }

            MAP_ADCChannelEnable(ADC_BASE, uiChannel);

            MAP_ADCEnable(ADC_BASE);

            MAP_UtilsDelay(800000);

                if(MAP_ADCFIFOLvlGet(ADC_BASE, uiChannel))

                {

                ulSample = MAP_ADCFIFORead(ADC_BASE, uiChannel);

                ulSample = (ulSample & 0x3ffc)>>2;

                }

            //   UART_PRINT(" %d \n\r", ulSample);

            return ulSample;

        }

    ----------------------------------------------------------------

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • janisalnis
    janisalnis over 12 years ago

    Hello!

     

    I was struglling with CC3200 analog input ADC example. It was not working. Sometimes giving only erratic values, sometimes only zero ADC values. Only the timer bits increased as they should. Found a forum topic about this bug:

    http://e2e.ti.com/support/wireless_connectivity/f/968/t/365450.aspx

    http://e2e.ti.com/support/wireless_connectivity/f/968/p/354092/1243186.aspx#1243186

    Need a line in while (forewer) loop uiIndex=0;

     

     

    ADC on PIN_57 is not allowed by example. Why? It giving value around 1090 regardless if connected to GND or not.

    ADC on pins PIN_58 and PIN_59 do not have resistors "dnp" on P3 header. (Actually resistors are on P1 header so one can connect signals there).

     

     

    There is another strange thing. It ADC input is floating the voltage on it is 0.5 V. If pin_60 is tied to GND via 100k then voltage is 0.4 V.

    Is there some pull-up on the pin that has to be additionally disabled?

    I made a voltage divider using 100k and 1Meg. 0.1 uF cap at ADC input was necessary to prevent pickup.

     

     

    I have changed example to a function that returns just 1 value read from CC3200 ADC. A delay was added between enabling ADC and readout allowing the input voltage to settle down. Without such delay the value was erratic.

    ----------------------------------------------------------------

    float readADC(unsigned long uiAdcInputPin)

        {   unsigned int  uiChannel;

            unsigned long ulSample;

     

            //uiAdcInputPin=PIN_60;

            PinTypeADC(uiAdcInputPin, 0xFF);

     

            switch(uiAdcInputPin)

            {

                case PIN_58: {uiChannel = ADC_CH_1;}break;

                case PIN_59: {uiChannel = ADC_CH_2;}break;

                case PIN_60: {uiChannel = ADC_CH_3;}break;

                default: break;

            }

            MAP_ADCChannelEnable(ADC_BASE, uiChannel);

            MAP_ADCEnable(ADC_BASE);

            MAP_UtilsDelay(800000);

                if(MAP_ADCFIFOLvlGet(ADC_BASE, uiChannel))

                {

                ulSample = MAP_ADCFIFORead(ADC_BASE, uiChannel);

                ulSample = (ulSample & 0x3ffc)>>2;

                }

            //   UART_PRINT(" %d \n\r", ulSample);

            return ulSample;

        }

    ----------------------------------------------------------------