IoT on Wheels Design Challenge
  • Challenges & Projects
  • Design Challenges
  • IoT on Wheels Design Challenge
  • More
  • Cancel
IoT on Wheels Design Challenge
Blog IOT on Wheels Design Challenge - Fatigue Alert System Blog #2
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
  • Author Author: dwinhold
  • Date Created: 1 Oct 2017 12:17 AM Date Created
  • Views 871 views
  • Likes 4 likes
  • Comments 5 comments
  • dwinhold
  • fatigue
  • fatiguealert
Related
Recommended

IOT on Wheels Design Challenge - Fatigue Alert System Blog #2

dwinhold
dwinhold
1 Oct 2017

Hello everyone,

 

This weeks update is a flow chart on how the computer will work with the sensors and how I plan the programming. I am also going to blog about the software I plan to use to program the Nucleo.

 

First the flow chart:

 

image

 

I hope this is fairly easy to follow (it makes sense to me anyway image) The Nucleo is at the heart of my design and everything branches off from there. I will have the WiFi module and the sensor board attached. I will be making a sensor for the steering wheel to make sure your hands are on the wheel. There is also going to be a heart rate monitor a vibration sensor and a confirmation light and button. With this all put together and the programming done right it will sense how tired you are and let you know when to stop driving.

 

As for  programming the Nucleo I will first use Mbed OS 5 https://os.mbed.com/  This looks to be what I need to use and I will also review the ease of this.

 

A quick note on the Nucleo-64 and the expansion boards. They came nicely packaged and with a card of info on each one. The Nucleo-64 and expansion boards are very impressive and will more then do the job I am set out to do. The only thing missing is a USB type A to mini B cable. Luckily I have a lot laying around but it could have been awkward if I didn't.

 

That is it for this blog, next one will be on the programming and making of some sensors.

 

Thank you

Dale W

  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +2
    Hi Dale, Have you considered putting a 3-axis accelerometer strapped to the head? You could use it to see if the head is starting to droop, which is an indication of fatigue and sleep deprivation. DAB
  • dwinhold
    dwinhold over 8 years ago in reply to DAB +1
    Hi DAB I was thinking of doing this originally but wasn't sure and left it off. With you mentioning it, I will now put it into my project. Thank you for the advice, it's always appreciated!! Dale
  • dwinhold
    dwinhold over 8 years ago in reply to mcb1 +1
    Hi Mark Very good point mcb1 . My original thought is that you have 3 seconds to press the acknowledge button (reaction time) before more drastic measures. You are absolutely correct in that 3 seconds…
Parents
  • mcb1
    mcb1 over 8 years ago

    Dale

    I'm curious about the 3 second timer used in your flowcharts.

    On the right side you've already detected excess vibrations which may indicate the vehicle has strayed off to the right.

    By my calculation at 100kmph the vehicle will travel 27.77m/sec and therefore after 3 secs has quite likely travelled 83m.

     

    IMO doing something much more drastic at 1 or 1.5 second after the wrist vibrations might be more useful.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 8 years ago

    Dale

    I'm curious about the 3 second timer used in your flowcharts.

    On the right side you've already detected excess vibrations which may indicate the vehicle has strayed off to the right.

    By my calculation at 100kmph the vehicle will travel 27.77m/sec and therefore after 3 secs has quite likely travelled 83m.

     

    IMO doing something much more drastic at 1 or 1.5 second after the wrist vibrations might be more useful.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dwinhold
    dwinhold over 8 years ago in reply to mcb1

    Hi Mark

     

    Very good point mcb1 . My original thought is that you have 3 seconds to press the acknowledge button (reaction time) before more drastic measures. You are absolutely correct in that 3 seconds is way to much time, I will definitely change this. If you aren't dozing off when this alert happens, the computer will still calculate your reaction time. I also plan that if the vibration doesn't stop and you keep pressing the acknowledge button the computer will ignore the vibration until it stops (eg. You may be on a dirt road), then it will start to monitor again.

     

    Thank you for the comment and help!!

     

    Dale