IoT on Wheels Design Challenge
  • Challenges & Projects
  • Design Challenges
  • IoT on Wheels Design Challenge
  • More
  • Cancel
IoT on Wheels Design Challenge
Blog IOT on Wheels Design Challenge - Smart Drive - Connecting GPS - Blog #5
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
  • Author Author: vlasov01
  • Date Created: 1 Nov 2017 2:00 AM Date Created
  • Views 1194 views
  • Likes 2 likes
  • Comments 3 comments
  • iot on wheels design challenge
  • assistnow
  • u-blox
  • gps receiver
Related
Recommended

IOT on Wheels Design Challenge - Smart Drive - Connecting GPS - Blog #5

vlasov01
vlasov01
1 Nov 2017

GPS Module

I've purchased a GPS module VK2828U7G5LF. It is based on UBX-M8030-KT chip, antenna and UART interface.

 

Testing GPS

I've used USB TTL serial converter to connect my GPS module to PC. The manufacturer of UBX-M8030-KT chip provides free software u-blox u-center to test and configure GPS module. It is very useful tool to start working with GPS module and debug protocol and controller behavior..

image

u-blox provides AssistNow feature for better precision. It is quite important for ant road related application. I've registered on u-blox site and got the token to use this technology. I've entered the token in the application and got data from the server. But my attempts to load this data into GPS Module failed. I suspect it may be a limitation of my GPS module.

image

Connecting GPS Module to Arduino

There is a lot of code samples for this GPS module built for Arduino platform.

I've looked at several of them:

Tiny GPS ( TinyGPS | Arduiniana  )

Tiny GPS Plus ( TinyGPS++ | Arduiniana  )

UBX GPS MultipleMessages ( https://www.youtube.com/watch?v=ylxwOg2pXrc  )

I've selected the last one as it focus on performance and small code footprint. As well code includes configuration sequence for GPS module, which simplifies configuration process,

image

The small code size was especially important as it simplified the process of porting the code from Arduino to Nucleo development environment.

It was pretty simple to connect the module to UART interface on Arduino board and run tests.

 

Summary

It was my first experience working with GPS module. I'm generally happy with results so far.

The next steps is to explore STM32L47RG serial interface and connect it to GPS module.

  • Sign in to reply

Top Comments

  • vlasov01
    vlasov01 over 9 years ago in reply to mcb1 +2
    Thank you! I was thinking to use I2C, but my GPS module doesn't expose it. I was able to connect it with Nucleo using UART instead. I'll publish details in the next blog.
  • e14phil
    e14phil over 9 years ago +1
    There is something very exciting with communicating with something that is in orbit. :-D
Parents
  • mcb1
    mcb1 over 9 years ago

    The guys and gals at Wyolum did this using an Arduino

    https://docs.google.com/document/pub?id=1wtgUoS4d7RWNOscLEQqgQcdmxl_rW34bLy4mNCantpQ

     

    I believe the code is in their repository.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vlasov01
    vlasov01 over 9 years ago in reply to mcb1

    Thank you! I was thinking to use I2C, but my GPS module doesn't expose it.

    image

    I was able to connect it with Nucleo using UART instead. I'll publish details in the next blog.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vlasov01
    vlasov01 over 9 years ago in reply to mcb1

    Thank you! I was thinking to use I2C, but my GPS module doesn't expose it.

    image

    I was able to connect it with Nucleo using UART instead. I'll publish details in the next blog.