IoT on Wheels Design Challenge
  • Challenges & Projects
  • Design Challenges
  • IoT on Wheels Design Challenge
  • More
  • Cancel
IoT on Wheels Design Challenge
Blog Walking-Wheel on Water  #1 Outline of the Design
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
  • Author Author: fyaocn
  • Date Created: 7 Sep 2017 3:09 AM Date Created
  • Views 852 views
  • Likes 3 likes
  • Comments 4 comments
  • walkingwheels
Related
Recommended

Walking-Wheel on Water  #1 Outline of the Design

fyaocn
fyaocn
7 Sep 2017

1. Introduction of the design

Design a kind of Glider with wheels to roll on road and floating barrel to float on water.

The glider is driven by propellers and Wheels are passive.

So the glider can not fly in this challenge, but it is ready to be thrown by hand landed on road or lake, if not crashed.

2. Schedule

- Evaluation blog to STM32-L476 and BlueNRG board.(1 blog)

- Demo design on mbed.org..(1 blog)

- MBED program for L476+BlueNRG to link mobile via evothings..(2 blog)

- Making of structure of glider .(1 blog)

- Make of propeller and motor for the glider .(1 blog)

- Mounting the Boards one the clumsy Glider .(1 blog)

- Test and run the glider .(1~3 blog)

- Final Show of the design

3. Hard ware and software

Nucleo-L476RG and extension board of BlueNRG shall be used for remote control by mobile

Two motors shall be controlled by ST-STM32L476-nucleo to move forward or turn left or right.

Software of CubeMX for ST shall be used.

4. Challenge and Afterward

The plane can not fly on air, but can float on water and move on road. Driven by propeller.

I would design PCB board integrating L476 and BLE chip to make the glider self-pilot.

image

This picture is a toy, I would make it sizable for Nucleo board and batteries.

  • Sign in to reply
Parents
  • janousv@stm
    janousv@stm over 9 years ago

    Do you plan to use rechargeable batteries ? In other words, will be battery charger (USB 5V powered) part of your design? This would be smart rechargeable toy then. If not, you could also power up the system from a commercially available power bank connected to the STM32Nucleo USB port  .... 5V should be also ok for your motor control circuit. Curious to see the fully sized plane with all the Nucleo boards integrated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • janousv@stm
    janousv@stm over 9 years ago

    Do you plan to use rechargeable batteries ? In other words, will be battery charger (USB 5V powered) part of your design? This would be smart rechargeable toy then. If not, you could also power up the system from a commercially available power bank connected to the STM32Nucleo USB port  .... 5V should be also ok for your motor control circuit. Curious to see the fully sized plane with all the Nucleo boards integrated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fyaocn
    fyaocn over 9 years ago in reply to janousv@stm

    Yes.

    Rechargeable batteries shall be used. Optional 4xAAA batteries can  be used. I have tested the power supply with L298N in walkingwheels on Water  #12 Motor Driver L298N for N30 DC motor

    The

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fyaocn
    fyaocn over 9 years ago in reply to fyaocn

    The L298N by ST has been widely used.

    This idea comes from toy-plane. But it can be of real life applicable in un-manned air delivery. Glider can carry more goods with much slower speed and lower power consumption than prevailing quad-rotor-drone.