Just Encase
  • Challenges & Projects
  • Design Challenges
  • Just Encase
  • More
  • Cancel
Just Encase
Blog Blog 4: Landslide monitoring for the Himalayan region- Putting it all together and testing
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Just Encase to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rsjawale24
  • Date Created: 27 Feb 2022 6:38 PM Date Created
  • Views 987 views
  • Likes 2 likes
  • Comments 0 comments
  • Arduino MKR WAN 1300
  • just encase design challenge
  • vibration sensor
  • landslide_monitoring
  • just_encase
  • just encase
Related
Recommended

Blog 4: Landslide monitoring for the Himalayan region- Putting it all together and testing

rsjawale24
rsjawale24
27 Feb 2022

Assembling all the parts together

In this blog, I will put together all the components of the landslide monitoring system - The vibration sensor, the buzzer and the Arduino inside the enclosure box. I chose the non-transparent 1554UGY water-tight enclosure box to prevent the electronics from any rainwater or any possible collapse of the box into a nearby river or valley due to a landslide.

The complete system looks like this  -

image

Here's the code for triggering the alarm and reading the signal from the vibration sensor.

int a;    //variable to store the vibration sensor signal
void setup() {
  // put your setup code here, to run once:
pinMode(5,INPUT); //pin for vibration sensor
pinMode(6,OUTPUT); // pin for buzzer
digitalWrite(6,LOW); //initialise buzzer to off state
}

void loop() {
  // put your main code here, to run repeatedly:
  a = digitalRead(5);
  if(a==0)
  {
    a = 0;  //latch the state of the vibration sensor
    while(1){   //keep the buzzer on infinitely
     digitalWrite(6,HIGH);   //sound the buzzer
    }
    }
    
  }

The Arduino continuously monitors the status of the vibration sensor and as soon as the sensor is triggered, the arduino sounds the buzzer alarm and the LEDs to indicate a landslide. If the audio alarm is loud enough, this can be heard at a long distance and hence accidents can be prevented. The entire electronics is powered using a power bank. In the future, I plan to make a solar version of this so that the power bank can be charged from the solar panel and it won't require an external power source.

In the next blog, I will test the system in the field.